Data Structures | |
| struct | zb_zcl_scene_table_record_fixed_s |
| Fixed-size part of the Scene table. More... | |
| struct | zb_zcl_scenes_fieldset_common_s |
| Common part of the field set definition. More... | |
| struct | zb_zcl_scenes_add_scene_req_s |
| struct | zb_zcl_scenes_view_scene_req_s |
| View scene command payload structure. More... | |
| struct | zb_zcl_scenes_remove_scene_req_s |
| Remove scene command payload structure. More... | |
| struct | zb_zcl_scenes_remove_all_scenes_req_s |
| Remove all scenes command payload structure. More... | |
| struct | zb_zcl_scenes_store_scene_req_s |
| Store scene command payload structure. More... | |
| struct | zb_zcl_scenes_recall_scene_req_s |
| Recall scene command payload structure. More... | |
| struct | zb_zcl_scenes_recall_scene_transition_time_req_s |
| Recall scene command transition_time payload structure. More... | |
| struct | zb_zcl_scenes_get_scene_membership_req_s |
| Get scene membership command payload structure. More... | |
| struct | zb_zcl_scenes_copy_scene_mode_s |
| Scene copying mode bitfield. More... | |
| struct | zb_zcl_scenes_copy_scene_req_s |
| Copy scene command payload structure. More... | |
| struct | zb_zcl_scenes_add_scene_res_s |
| Add scene response payload structure. More... | |
| struct | zb_zcl_scenes_view_scene_res_fixed_size_s |
| Mandatory part of the Scenes.ViewSceneResponse payload. More... | |
| struct | zb_zcl_scenes_remove_scene_res_s |
| Remove scene response payload structure. More... | |
| struct | zb_zcl_scenes_remove_all_scenes_res_s |
| Remove all scenes response payload structure. More... | |
| struct | zb_zcl_scenes_store_scene_res_s |
| Store scene response payload structure. More... | |
| struct | zb_zcl_scenes_get_scene_membership_res_mandatory_s |
| Get scene membership response fixed-structure payload part representation. More... | |
| struct | zb_zcl_scenes_get_scene_membership_res_optional_s |
| Get scene membership response optional payload part representation. More... | |
| struct | zb_zcl_scenes_get_scene_membership_res_s |
| Get scene membership response. More... | |
Scenes cluster attributes | |
| enum | zb_zcl_scene_attr_e { ZB_ZCL_ATTR_SCENES_SCENE_COUNT_ID = 0x0000, ZB_ZCL_ATTR_SCENES_CURRENT_SCENE_ID = 0x001, ZB_ZCL_ATTR_SCENES_CURRENT_GROUP_ID = 0x002, ZB_ZCL_ATTR_SCENES_SCENE_VALID_ID = 0x003, ZB_ZCL_ATTR_SCENES_NAME_SUPPORT_ID = 0x004, ZB_ZCL_ATTR_SCENES_LAST_CONFIGURED_BY_ID = 0x005 } |
| Scene cluster attribute identifiers. More... | |
| typedef struct zb_zcl_scene_table_record_fixed_s | zb_zcl_scene_table_record_fixed_t |
| Fixed-size part of the Scene table. More... | |
| typedef struct zb_zcl_scenes_fieldset_common_s | zb_zcl_scenes_fieldset_common_t |
| Common part of the field set definition. More... | |
| #define | ZB_ZCL_SCENES_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0003u) |
| Default value for Scenes cluster revision global attribute. More... | |
| #define | ZB_ZCL_SCENES_CLUSTER_REVISION_MAX ZB_ZCL_SCENES_CLUSTER_REVISION_DEFAULT |
| Maximal value for implemented Scenes cluster revision global attribute. More... | |
| #define | ZB_ZCL_SCENES_NAME_SUPPORT_BIT_MASK 0x80 |
| Mask to extract Name support bit. More... | |
| #define | ZB_ZCL_ATTR_SCENES_CURRENT_GROUP_MIN_VALUE 0x0001 |
| #define | ZB_ZCL_ATTR_SCENES_CURRENT_GROUP_MAX_VALUE 0xfff7 |
| #define | ZB_ZCL_MAX_SCENE_TABLE_RECORDS 16 |
| #define | ZB_ZCL_SCENES_SCENE_COUNT_DEFAULT_VALUE 0 |
| Default value for Scene count attribute. More... | |
| #define | ZB_ZCL_SCENES_CURRENT_SCENE_DEFAULT_VALUE 0 |
| Default value for Current scene attribute. More... | |
| #define | ZB_ZCL_SCENES_CURRENT_GROUP_DEFAULT_VALUE 0 |
| Default value for Current group attribute. More... | |
| #define | ZB_ZCL_SCENES_SCENE_VALID_DEFAULT_VALUE 0 |
| Default value for Scene valid attribute. More... | |
| #define | ZB_ZCL_RECALL_SCENES_TRANSITION_TIME_NOT_USED_VALUE 0xffff |
| "Not used" value for Recall scene transition time More... | |
| #define | ZB_ZCL_SCENES_NAME_SUPPORT_DEFAULT_VALUE 0 |
| Default value for Name support attribute The Stack does not support scene names, the default value for the attribute can be declared until name support will be added. More... | |
| #define | ZB_ZCL_SCENE_GLOBAL_SCENE_GROUP_ID 0x00 |
| Global Scene - group identifier see ZLL spec 6.5.1.3.1. More... | |
| #define | ZB_ZCL_SCENE_GLOBAL_SCENE_ID 0x00 |
| Global Scene - scene identifier see ZLL spec 6.5.1.3.1. More... | |
| #define | ZB_ZCL_SCENES_FREE_SCENE_TABLE_RECORD 0xffff |
| Declares a "free record" marker for a scene table Used as a value of a group_id field in a corresponding table record. More... | |
| #define | ZB_ZCL_SCENES_TRANSITION_TIME_DEFAULT_VALUE 0 |
| Default value for scene transition time. More... | |
| #define | ZB_ZCL_DECLARE_SCENES_ATTRIB_LIST( attr_list, scene_count, current_scene, current_group, scene_valid, name_support) |
| Declares Scenes attribute list. More... | |
Scenes cluster commands | |
| enum | zb_zcl_scenes_cmd_e { ZB_ZCL_CMD_SCENES_ADD_SCENE = 0x00, ZB_ZCL_CMD_SCENES_VIEW_SCENE = 0x01, ZB_ZCL_CMD_SCENES_REMOVE_SCENE = 0x02, ZB_ZCL_CMD_SCENES_REMOVE_ALL_SCENES = 0x03, ZB_ZCL_CMD_SCENES_STORE_SCENE = 0x04, ZB_ZCL_CMD_SCENES_RECALL_SCENE = 0x05, ZB_ZCL_CMD_SCENES_GET_SCENE_MEMBERSHIP = 0x06, ZB_ZCL_CMD_SCENES_ENHANCED_ADD_SCENE = 0x40, ZB_ZCL_CMD_SCENES_ENHANCED_VIEW_SCENE = 0x41, ZB_ZCL_CMD_SCENES_COPY_SCENE = 0x42 } |
| Command identifiers for Scenes Cluster. More... | |
| enum | zb_zcl_scenes_cmd_resp_e { ZB_ZCL_CMD_SCENES_ADD_SCENE_RESPONSE = 0x00, ZB_ZCL_CMD_SCENES_VIEW_SCENE_RESPONSE = 0x01, ZB_ZCL_CMD_SCENES_REMOVE_SCENE_RESPONSE = 0x02, ZB_ZCL_CMD_SCENES_REMOVE_ALL_SCENES_RESPONSE = 0x03, ZB_ZCL_CMD_SCENES_STORE_SCENE_RESPONSE = 0x04, ZB_ZCL_CMD_SCENES_GET_SCENE_MEMBERSHIP_RESPONSE = 0x06, ZB_ZCL_CMD_SCENES_ENHANCED_ADD_SCENE_RESPONSE = 0x40, ZB_ZCL_CMD_SCENES_ENHANCED_VIEW_SCENE_RESPONSE = 0x41, ZB_ZCL_CMD_SCENES_COPY_SCENE_RESPONSE = 0x42 } |
| Command response identifiers for Scenes Cluster. More... | |
| typedef struct zb_zcl_scenes_add_scene_req_s | zb_zcl_scenes_add_scene_req_t |
| typedef struct zb_zcl_scenes_view_scene_req_s | zb_zcl_scenes_view_scene_req_t |
| View scene command payload structure. More... | |
| typedef struct zb_zcl_scenes_remove_scene_req_s | zb_zcl_scenes_remove_scene_req_t |
| Remove scene command payload structure. More... | |
| typedef struct zb_zcl_scenes_remove_all_scenes_req_s | zb_zcl_scenes_remove_all_scenes_req_t |
| Remove all scenes command payload structure. More... | |
| typedef struct zb_zcl_scenes_store_scene_req_s | zb_zcl_scenes_store_scene_req_t |
| Store scene command payload structure. More... | |
| typedef struct zb_zcl_scenes_recall_scene_req_s | zb_zcl_scenes_recall_scene_req_t |
| Recall scene command payload structure. More... | |
| typedef struct zb_zcl_scenes_recall_scene_transition_time_req_s | zb_zcl_scenes_recall_scene_transition_time_req_t |
| Recall scene command transition_time payload structure. More... | |
| typedef struct zb_zcl_scenes_get_scene_membership_req_s | zb_zcl_scenes_get_scene_membership_req_t |
| Get scene membership command payload structure. More... | |
| typedef struct zb_zcl_scenes_copy_scene_mode_s | zb_zcl_scenes_copy_scene_mode_t |
| Scene copying mode bitfield. More... | |
| typedef struct zb_zcl_scenes_copy_scene_req_s | zb_zcl_scenes_copy_scene_req_t |
| Copy scene command payload structure. More... | |
| typedef struct zb_zcl_scenes_add_scene_res_s | zb_zcl_scenes_add_scene_res_t |
| Add scene response payload structure. More... | |
| typedef struct zb_zcl_scenes_view_scene_res_fixed_size_s | zb_zcl_scenes_view_scene_res_fixed_size_t |
| Mandatory part of the Scenes.ViewSceneResponse payload. More... | |
| typedef struct zb_zcl_scenes_remove_scene_res_s | zb_zcl_scenes_remove_scene_res_t |
| Remove scene response payload structure. More... | |
| typedef struct zb_zcl_scenes_remove_all_scenes_res_s | zb_zcl_scenes_remove_all_scenes_res_t |
| Remove all scenes response payload structure. More... | |
| typedef struct zb_zcl_scenes_store_scene_res_s | zb_zcl_scenes_store_scene_res_t |
| Store scene response payload structure. More... | |
| typedef struct zb_zcl_scenes_get_scene_membership_res_mandatory_s | zb_zcl_scenes_get_scene_membership_res_mandatory_t |
| Get scene membership response fixed-structure payload part representation. More... | |
| typedef struct zb_zcl_scenes_get_scene_membership_res_optional_s | zb_zcl_scenes_get_scene_membership_res_optional_t |
| Get scene membership response optional payload part representation. More... | |
| typedef struct zb_zcl_scenes_get_scene_membership_res_s | zb_zcl_scenes_get_scene_membership_res_t |
| Get scene membership response. More... | |
| void | zb_zcl_scenes_send_recall_scene_req_zcl8 (zb_bufid_t buffer, const zb_addr_u *dst_addr, zb_uint8_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t ep, zb_uint16_t prof_id, zb_uint8_t dis_default_resp, zb_callback_t callback, zb_uint16_t group_id, zb_uint8_t scene_id, zb_uint16_t transition_time) |
| Send Recall scene command The command can be sent to device or group of devices either. More... | |
| void | zb_zcl_scenes_send_recall_scene_req (zb_bufid_t buffer, const zb_addr_u *dst_addr, zb_uint8_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t ep, zb_uint16_t prof_id, zb_uint8_t dis_default_resp, zb_callback_t callback, zb_uint16_t group_id, zb_uint8_t scene_id) |
| Send Recall scene command (pre-ZCL8) Use zb_zcl_scenes_send_recall_scene_req_zcl8 for ZCL8 revision call. The command can be sent to device or group of devices either. More... | |
| #define | ZB_ZCL_SCENES_INIT_ADD_SCENE_REQ_COMMON( buffer, cmd_struct_ptr, dis_default_resp, group_id, scene_id, transition_time, add_scene_cmd_id) |
| Common macro to start filling Add scene command frame. More... | |
| #define | ZB_ZCL_SCENES_INIT_ADD_SCENE_REQ( buffer, cmd_struct_ptr, dis_default_resp, group_id, scene_id, transition_time) |
| Start filling Add scene command frame. More... | |
| #define | ZB_ZCL_SCENES_INIT_ENHANCED_ADD_SCENE_REQ( buffer, cmd_struct_ptr, dis_default_resp, group_id, scene_id, transition_time) |
| Start filling Enhanced Add scene command frame. More... | |
| #define | ZB_ZCL_SCENES_SEND_ADD_SCENE_REQ( buffer, cmd_struct_ptr, dst_addr, dst_ep, ep, prof_id, callback) |
| Sends Add scene command. More... | |
| #define | ZB_ZCL_SCENES_INIT_FIELDSET(cmd_struct_ptr, cluster, fs_length) |
| Adds fieldset into the buffer for sending command. More... | |
| #define | ZB_ZCL_SCENES_GET_ADD_SCENE_REQ_COMMON(buffer, cmd_struct_ptr) |
| Parse common part of Add Scene command. More... | |
| #define | ZB_ZCL_SCENES_GET_ADD_SCENE_REQ_NEXT_FIELDSET_DESC( buffer, cmd_struct_ptr, content_length) |
| Parses fieldset description. More... | |
| #define | ZB_ZCL_SCENES_GET_ADD_SCENE_REQ_STORE_FIELDSET_COMMON( src_data_ptr, dst_data_ptr, content_length) |
| Copies parsed fieldset description into designated memory area. More... | |
| #define | ZB_ZCL_SCENES_SEND_VIEW_SCENE_REQ_COMMON( buffer, dst_addr, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id, view_scene_cmd_id) |
| Common macro to send View Scene commands. More... | |
| #define | ZB_ZCL_SCENES_SEND_VIEW_SCENE_REQ( buffer, dst_addr, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id) |
| Send View Scene commands. More... | |
| #define | ZB_ZCL_SCENES_SEND_ENHANCED_VIEW_SCENE_REQ( buffer, dst_addr, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id) |
| Send Enhanced View Scene command. More... | |
| #define | ZB_ZCL_SCENES_GET_VIEW_SCENE_REQ(buffer, cmd_struct_ptr) |
| Parses Scenes.ViewScene command payload. More... | |
| #define | ZB_ZCL_SCENES_SEND_REMOVE_SCENE_REQ( buffer, dst_addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id) |
| Send Remove scene command. More... | |
| #define | ZB_ZCL_SCENES_GET_REMOVE_SCENE_REQ(buffer, cmd_struct_ptr) |
| Parses Scenes.RemoveScene command payload. More... | |
| #define | ZB_ZCL_SCENES_SEND_REMOVE_ALL_SCENES_REQ( buffer, dst_addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, callback, group_id) |
| Send Remove all scenes command. More... | |
| #define | ZB_ZCL_SCENES_GET_REMOVE_ALL_SCENES_REQ(buffer, cmd_struct_ptr) |
| Parses Scenes.RemoveScene command payload. More... | |
| #define | ZB_ZCL_SCENES_SEND_STORE_SCENE_REQ( buffer, dst_addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id) |
| Send Store Scene command. More... | |
| #define | ZB_ZCL_SCENES_GET_STORE_SCENE_REQ(buffer, cmd_struct_ptr) |
| Parse Store Scene command. More... | |
| #define | ZB_ZCL_SCENES_SEND_RECALL_SCENE_REQ_ZCL8(buffer, dst_addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id, transition_time) |
| #define | ZB_ZCL_SCENES_SEND_RECALL_SCENE_REQ(buffer, dst_addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, callback, group_id, scene_id) |
| #define | ZB_ZCL_SCENES_RECALL_SCENE_REQ_PAYLOAD_LEN sizeof(zb_zcl_scenes_recall_scene_req_t) |
| Recall scene payload length macro. More... | |
| #define | ZB_ZCL_SCENES_RECALL_SCENE_REQ_TRANSITION_TIME_PAYLOAD_LEN sizeof(zb_uint16_t) |
| Transition Time field of Recall scene payload length macro. More... | |
| #define | ZB_ZCL_SCENES_RECALL_SCENE_REQ_TRANSITION_TIME_INVALID_VALUE (zb_uint16_t)0xFFFF |
| Transition Time field invalid value. More... | |
| #define | ZB_ZCL_SCENES_GET_RECALL_SCENE_REQ(buffer, cmd_struct_ptr, req_len) |
| Parse Recall Scene command. More... | |
| #define | ZB_ZCL_SCENES_SEND_GET_SCENE_MEMBERSHIP_REQ( buffer, dst_addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, callback, group_id) |
| Send Remove all scenes command. More... | |
| #define | ZB_ZCL_SCENES_SEND_COPY_SCENE_REQ( buffer, dst_addr, dst_ep, ep, prof_id, dis_default_resp, callback, mode, group_id_from, scene_id_from, group_id_to, scene_id_to) |
| Send Copy scene command. More... | |
| #define | ZB_ZCL_SCENES_SEND_COPY_SCENE_RES( buffer, cmd_struct_ptr, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id_from, scene_id_from) |
| Send Copy scene Response command. More... | |
| #define | ZB_ZCL_SCENES_GET_GET_SCENE_MEMBERSHIP_REQ(buffer, cmd_struct_ptr) |
| Parses Scenes.GetSceneMembership command payload. More... | |
| #define | ZB_ZCL_COPY_ALL_SCENES_ENABLED 0x01U |
| #define | ZB_ZCL_COPY_ALL_SCENES_DISABLED 0x00U |
| #define | ZB_ZCL_SCENES_GET_COPY_SCENE_REQ(buffer, cmd_struct_ptr) |
| #define | ZB_ZCL_SCENES_SEND_ADD_SCENE_RES_COMMON( buffer, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id, scene_id, cmd_id) |
| Common macro to send Add Scene response. More... | |
| #define | ZB_ZCL_SCENES_SEND_ADD_SCENE_RES( buffer, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id, scene_id) |
| Send Add Scene response. More... | |
| #define | ZB_ZCL_SCENES_SEND_ENHANCED_ADD_SCENE_RES( buffer, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id, scene_id) |
| Send Enhanced Add Scene response. More... | |
| #define | ZB_ZCL_SCENES_GET_ADD_SCENE_RES(buffer, cmd_struct_ptr) |
| Parses Scenes.AddSceneResponse command payload. More... | |
| #define | ZB_ZCL_SCENES_INIT_VIEW_SCENE_RES_COMMON( buffer, cmd_struct_ptr, seq_num, status, group_id, scene_id, view_res_cmd_id) |
| Common macro to start filling View scene response frame. More... | |
| #define | ZB_ZCL_SCENES_INIT_VIEW_SCENE_RES( buffer, cmd_struct_ptr, seq_num, status, group_id, scene_id) |
| Start filling View scene response frame. More... | |
| #define | ZB_ZCL_SCENES_INIT_ENHANCED_VIEW_SCENE_RES( buffer, cmd_struct_ptr, seq_num, status, group_id, scene_id) |
| Start filling Enhanced View scene response frame. More... | |
| #define | ZB_ZCL_SCENES_SEND_VIEW_SCENE_RES( buffer, cmd_struct_ptr, dst_addr, dst_ep, ep, prof_id, callback) |
| Sends View scene response. More... | |
| #define | ZB_ZCL_SCENES_ADD_TRANSITION_TIME_VIEW_SCENE_RES( cmd_struct_ptr, trans_time) ZB_ZCL_PACKET_PUT_DATA16((cmd_struct_ptr), &(trans_time)) |
| Adds transition time into Scenes.ViewSceneResponse payload. More... | |
| #define | ZB_ZCL_SCENES_ADD_SCENE_NAME_VIEW_SCENE_RES(cmd_struct_ptr, scene_name) ZB_ZCL_PACKET_PUT_DATA8((cmd_struct_ptr), 0) |
| Adds scene name into Scenes.ViewSceneResponse payload. More... | |
| #define | ZB_ZCL_SCENES_GET_VIEW_SCENE_RES_COMMON(buffer, response_ptr) |
| Parses common part of the Scenes.ViewSceneResponse. More... | |
| #define | ZB_ZCL_SCENES_SEND_REMOVE_SCENE_RES( buffer, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id, scene_id) |
| Send Remove Scene response. More... | |
| #define | ZB_ZCL_SCENES_GET_REMOVE_SCENE_RES(buffer, cmd_struct_ptr) |
| Parses Scenes.RemoveSceneResponse command payload. More... | |
| #define | ZB_ZCL_SCENES_SEND_REMOVE_ALL_SCENES_RES( buffer, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id) |
| Send Remove all scenes response. More... | |
| #define | ZB_ZCL_SCENES_GET_REMOVE_ALL_SCENES_RES(buffer, cmd_struct_ptr) |
| Parses Scenes.RemoveAllScenesResponse command payload. More... | |
| #define | ZB_ZCL_SCENES_SEND_STORE_SCENE_RES( buffer, seq_num, dst_addr, dst_ep, ep, prof_id, callback, status, group_id, scene_id) |
| Send Store scene response. More... | |
| #define | ZB_ZCL_SCENES_GET_STORE_SCENE_RES(buffer, cmd_struct_ptr) |
| Parses Scenes.StoreScene command payload. More... | |
| #define | ZB_ZCL_SCENES_CAPACITY_ONE_MORE ((zb_uint8_t)0xfe) |
| Scene table capacity: at least one scene can be added. More... | |
| #define | ZB_ZCL_SCENES_CAPACITY_UNKNOWN ((zb_uint8_t)0xff) |
| Scene table capacity unknown. More... | |
| #define | ZB_ZCL_SCENES_INIT_GET_SCENE_MEMBERSHIP_RES( buffer, cmd_struct_ptr, seq_num, cap_ptr, status, capacity, group_id) |
| Start filling Get scene membership response frame. More... | |
| #define | ZB_ZCL_SCENES_ADD_SCENE_COUNT_GET_SCENE_MEMBERSHIP_RES(cmd_struct_ptr, scene_count) ZB_ZCL_PACKET_PUT_DATA8(cmd_struct_ptr, (scene_count)) |
| Appends Scene count value to Get scene membership response constant-structure payload part. More... | |
| #define | ZB_ZCL_SCENES_ADD_SCENE_ID_GET_SCENE_MEMBERSHIP_RES(cmd_struct_ptr, scene_id) ZB_ZCL_PACKET_PUT_DATA8(cmd_struct_ptr, (scene_id)) |
| Appends a scene identifier to the Scene list in Get scene membership response payload. More... | |
| #define | ZB_ZCL_SCENES_SEND_GET_SCENE_MEMBERSHIP_RES(buffer, cmd_struct_ptr, dst_addr, dst_ep, ep, prof_id, callback) |
| Sends Get scene membership response. More... | |
| #define | ZB_ZCL_SCENES_GET_GET_SCENE_MEMBERSHIP_RES(buffer, cmd_struct_ptr) |
| Parses Scenes.RemoveAllScenesResponse command payload. More... | |
ZCL Scenes cluster definitions
| #define ZB_ZCL_ATTR_SCENES_CURRENT_GROUP_MAX_VALUE 0xfff7 |
Maximal permissible value for Current group attribute
| #define ZB_ZCL_ATTR_SCENES_CURRENT_GROUP_MIN_VALUE 0x0001 |
Minimal permissible value for Current group attribute
| #define ZB_ZCL_COPY_ALL_SCENES_DISABLED 0x00U |
| #define ZB_ZCL_COPY_ALL_SCENES_ENABLED 0x01U |
| #define ZB_ZCL_DECLARE_SCENES_ATTRIB_LIST | ( | attr_list, | |
| scene_count, | |||
| current_scene, | |||
| current_group, | |||
| scene_valid, | |||
| name_support | |||
| ) |
Declares Scenes attribute list.
| attr_list | Attribute list name |
| scene_count | ZB_ZCL_ATTR_SCENES_SCENE_COUNT_ID placeholder |
| current_scene | ZB_ZCL_ATTR_SCENES_CURRENT_SCENE_ID placeholder |
| current_group | ZB_ZCL_ATTR_SCENES_CURRENT_GROUP_ID placeholder |
| scene_valid | ZB_ZCL_ATTR_SCENES_SCENE_VALID_ID placeholder |
| name_support | ZB_ZCL_ATTR_SCENES_NAME_SUPPORT_ID placeholder |
| #define ZB_ZCL_MAX_SCENE_TABLE_RECORDS 16 |
Maximal number of scene table records
| #define ZB_ZCL_RECALL_SCENES_TRANSITION_TIME_NOT_USED_VALUE 0xffff |
"Not used" value for Recall scene transition time
| #define ZB_ZCL_SCENE_GLOBAL_SCENE_GROUP_ID 0x00 |
Global Scene - group identifier see ZLL spec 6.5.1.3.1.
| #define ZB_ZCL_SCENE_GLOBAL_SCENE_ID 0x00 |
Global Scene - scene identifier see ZLL spec 6.5.1.3.1.
| #define ZB_ZCL_SCENES_ADD_SCENE_COUNT_GET_SCENE_MEMBERSHIP_RES | ( | cmd_struct_ptr, | |
| scene_count | |||
| ) | ZB_ZCL_PACKET_PUT_DATA8(cmd_struct_ptr, (scene_count)) |
Appends Scene count value to Get scene membership response constant-structure payload part.
| cmd_struct_ptr | - pointer to the memory area SceneCount value should be put to |
| scene_count | - number of scenes in the scene list |
| #define ZB_ZCL_SCENES_ADD_SCENE_ID_GET_SCENE_MEMBERSHIP_RES | ( | cmd_struct_ptr, | |
| scene_id | |||
| ) | ZB_ZCL_PACKET_PUT_DATA8(cmd_struct_ptr, (scene_id)) |
Appends a scene identifier to the Scene list in Get scene membership response payload.
| cmd_struct_ptr | - pointer to the memory area scene identifier should be put to |
| scene_id | - scene identifier |
| #define ZB_ZCL_SCENES_ADD_SCENE_NAME_VIEW_SCENE_RES | ( | cmd_struct_ptr, | |
| scene_name | |||
| ) | ZB_ZCL_PACKET_PUT_DATA8((cmd_struct_ptr), 0) |
Adds scene name into Scenes.ViewSceneResponse payload.
Since the Stack does not support scene names, the define puts only zero scene name length byte to preserve payload format.
| cmd_struct_ptr | - pointer to the place in buffer to put data to |
| scene_name | - scene name to put (currently ignored) |
| #define ZB_ZCL_SCENES_ADD_TRANSITION_TIME_VIEW_SCENE_RES | ( | cmd_struct_ptr, | |
| trans_time | |||
| ) | ZB_ZCL_PACKET_PUT_DATA16((cmd_struct_ptr), &(trans_time)) |
Adds transition time into Scenes.ViewSceneResponse payload.
| cmd_struct_ptr | - pointer to the place in buffer to put data to |
| trans_time | - transition time to put |
| #define ZB_ZCL_SCENES_CAPACITY_ONE_MORE ((zb_uint8_t)0xfe) |
Scene table capacity: at least one scene can be added.
Exact number is unknown
| #define ZB_ZCL_SCENES_CAPACITY_UNKNOWN ((zb_uint8_t)0xff) |
Scene table capacity unknown.
| #define ZB_ZCL_SCENES_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0003u) |
Default value for Scenes cluster revision global attribute.
| #define ZB_ZCL_SCENES_CLUSTER_REVISION_MAX ZB_ZCL_SCENES_CLUSTER_REVISION_DEFAULT |
Maximal value for implemented Scenes cluster revision global attribute.
| #define ZB_ZCL_SCENES_CURRENT_GROUP_DEFAULT_VALUE 0 |
Default value for Current group attribute.
| #define ZB_ZCL_SCENES_CURRENT_SCENE_DEFAULT_VALUE 0 |
Default value for Current scene attribute.
| #define ZB_ZCL_SCENES_FREE_SCENE_TABLE_RECORD 0xffff |
Declares a "free record" marker for a scene table Used as a value of a group_id field in a corresponding table record.
| #define ZB_ZCL_SCENES_GET_ADD_SCENE_REQ_COMMON | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parse common part of Add Scene command.
| buffer | containing Store scene command payload |
| cmd_struct_ptr | - pointer to the request representation structure of type zb_zcl_scenes_add_scene_req_t or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_ADD_SCENE_REQ_NEXT_FIELDSET_DESC | ( | buffer, | |
| cmd_struct_ptr, | |||
| content_length | |||
| ) |
Parses fieldset description.
| buffer | containing fieldset |
| cmd_struct_ptr | - pointer to the fieldset description representation structure (of type zb_zcl_scenes_fieldset_common_s) or NULL pointer if payload size is too small |
| content_length | - variable to contain size of the fieldset content left unprocessed |
| #define ZB_ZCL_SCENES_GET_ADD_SCENE_REQ_STORE_FIELDSET_COMMON | ( | src_data_ptr, | |
| dst_data_ptr, | |||
| content_length | |||
| ) |
Copies parsed fieldset description into designated memory area.
| src_data_ptr | - pointer to the memory area containing parsed fieldset description |
| dst_data_ptr | - pointer to the memory area to put fieldset description to |
| content_length | - remaining length of the unprocessed fieldset content |
| #define ZB_ZCL_SCENES_GET_ADD_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.AddSceneResponse command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_add_scene_res_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_COPY_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
| #define ZB_ZCL_SCENES_GET_GET_SCENE_MEMBERSHIP_REQ | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.GetSceneMembership command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_get_scene_membership_req_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_GET_SCENE_MEMBERSHIP_RES | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.RemoveAllScenesResponse command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_get_scene_membership_res_s) or NULL pointer if payload size is too small to contain mandatory part |
| #define ZB_ZCL_SCENES_GET_RECALL_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr, | |||
| req_len | |||
| ) |
Parse Recall Scene command.
| buffer | containing Store scene command payload |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_recall_scene_req_s) or NULL pointer if payload size is too small |
| req_len | - length of ZCL command |
| #define ZB_ZCL_SCENES_GET_REMOVE_ALL_SCENES_REQ | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.RemoveScene command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_remove_scene_req_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_REMOVE_ALL_SCENES_RES | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.RemoveAllScenesResponse command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_remove_all_scenes_res_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_REMOVE_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.RemoveScene command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_remove_scene_req_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_REMOVE_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.RemoveSceneResponse command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_remove_scene_res_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_STORE_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parse Store Scene command.
| buffer | containing Store scene command payload |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_store_scene_req_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_STORE_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.StoreScene command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_store_scene_res_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_VIEW_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr | |||
| ) |
Parses Scenes.ViewScene command payload.
| buffer | to get data from |
| cmd_struct_ptr | - pointer to the request representation structure (of type zb_zcl_scenes_view_scene_req_s) or NULL pointer if payload size is too small |
| #define ZB_ZCL_SCENES_GET_VIEW_SCENE_RES_COMMON | ( | buffer, | |
| response_ptr | |||
| ) |
Parses common part of the Scenes.ViewSceneResponse.
| buffer | containing data |
| response_ptr | - pointer to the extracted data |
| #define ZB_ZCL_SCENES_INIT_ADD_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr, | |||
| dis_default_resp, | |||
| group_id, | |||
| scene_id, | |||
| transition_time | |||
| ) |
Start filling Add scene command frame.
Fills the constant-structure part of the command payload only.
Command can contain no fieldsets defining empty scene. The new scene can be used, for example, for storing fieldsets with Store scene command.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| dis_default_resp | - enable/disable default response |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| transition_time | - scene transition time (in seconds) |
| #define ZB_ZCL_SCENES_INIT_ADD_SCENE_REQ_COMMON | ( | buffer, | |
| cmd_struct_ptr, | |||
| dis_default_resp, | |||
| group_id, | |||
| scene_id, | |||
| transition_time, | |||
| add_scene_cmd_id | |||
| ) |
Common macro to start filling Add scene command frame.
Fills the constant-structure part of the command payload only.
Command can contain no fieldsets defining empty scene. The new scene can be used, for example, for storing fieldsets with Store scene command.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| dis_default_resp | - enable/disable default response |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| transition_time | - scene transition time |
| add_scene_cmd_id | - a scene cmd ID (Add Scene or Enh Add Scene) |
| #define ZB_ZCL_SCENES_INIT_ENHANCED_ADD_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr, | |||
| dis_default_resp, | |||
| group_id, | |||
| scene_id, | |||
| transition_time | |||
| ) |
Start filling Enhanced Add scene command frame.
Fills the constant-structure part of the command payload only.
Command can contain no fieldsets defining empty scene. The new scene can be used, for example, for storing fieldsets with Store scene command.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| dis_default_resp | - enable/disable default response |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| transition_time | - scene transition time (in tenths of a second) |
| #define ZB_ZCL_SCENES_INIT_ENHANCED_VIEW_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr, | |||
| seq_num, | |||
| status, | |||
| group_id, | |||
| scene_id | |||
| ) |
Start filling Enhanced View scene response frame.
Fills the mandatory part of the View scene response payload.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| seq_num | - ZCL sequence number |
| status | of the command execution. Appropriate values (defined in zcl_status enumeration) are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_INIT_FIELDSET | ( | cmd_struct_ptr, | |
| cluster, | |||
| fs_length | |||
| ) |
Adds fieldset into the buffer for sending command.
| cmd_struct_ptr | - pointer to the place in the buffer to put data to |
| cluster | identifier the fieldset under consideration belongs to |
| fs_length | - summary length of the attributes in the fieldset |
| #define ZB_ZCL_SCENES_INIT_GET_SCENE_MEMBERSHIP_RES | ( | buffer, | |
| cmd_struct_ptr, | |||
| seq_num, | |||
| cap_ptr, | |||
| status, | |||
| capacity, | |||
| group_id | |||
| ) |
Start filling Get scene membership response frame.
Fills the mandatory part of the Get scene membership scene response payload.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| seq_num | - ZCL sequence number |
| cap_ptr | - pointer to the capacity fields of the response |
| status | of the command execution. Appropriate values (defined in zcl_status enumeration) are:
|
| capacity | of the scene table |
| group_id | - group identifier for the scene to store |
| #define ZB_ZCL_SCENES_INIT_VIEW_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr, | |||
| seq_num, | |||
| status, | |||
| group_id, | |||
| scene_id | |||
| ) |
Start filling View scene response frame.
Fills the mandatory part of the View scene response payload.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| seq_num | - ZCL sequence number |
| status | of the command execution. Appropriate values (defined in zcl_status enumeration) are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_INIT_VIEW_SCENE_RES_COMMON | ( | buffer, | |
| cmd_struct_ptr, | |||
| seq_num, | |||
| status, | |||
| group_id, | |||
| scene_id, | |||
| view_res_cmd_id | |||
| ) |
Common macro to start filling View scene response frame.
Fills the mandatory part of the View scene response payload.
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| seq_num | - ZCL sequence number |
| status | of the command execution. Appropriate values (defined in zcl_status enumeration) are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| view_res_cmd_id | - a command ID (View Response or Enh View Response) |
| #define ZB_ZCL_SCENES_NAME_SUPPORT_BIT_MASK 0x80 |
Mask to extract Name support bit.
| #define ZB_ZCL_SCENES_NAME_SUPPORT_DEFAULT_VALUE 0 |
Default value for Name support attribute The Stack does not support scene names, the default value for the attribute can be declared until name support will be added.
| #define ZB_ZCL_SCENES_RECALL_SCENE_REQ_PAYLOAD_LEN sizeof(zb_zcl_scenes_recall_scene_req_t) |
Recall scene payload length macro.
| #define ZB_ZCL_SCENES_RECALL_SCENE_REQ_TRANSITION_TIME_INVALID_VALUE (zb_uint16_t)0xFFFF |
Transition Time field invalid value.
| #define ZB_ZCL_SCENES_RECALL_SCENE_REQ_TRANSITION_TIME_PAYLOAD_LEN sizeof(zb_uint16_t) |
Transition Time field of Recall scene payload length macro.
| #define ZB_ZCL_SCENES_SCENE_COUNT_DEFAULT_VALUE 0 |
Default value for Scene count attribute.
| #define ZB_ZCL_SCENES_SCENE_VALID_DEFAULT_VALUE 0 |
Default value for Scene valid attribute.
| #define ZB_ZCL_SCENES_SEND_ADD_SCENE_REQ | ( | buffer, | |
| cmd_struct_ptr, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback | |||
| ) |
Sends Add scene command.
| buffer | - with prepared command payload |
| cmd_struct_ptr | - pointer to the place variable-structure part of the |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| #define ZB_ZCL_SCENES_SEND_ADD_SCENE_RES | ( | buffer, | |
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Add Scene response.
| buffer | to put packet to |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| status | of the corresponding Add scene command execution. Appropriate values (defined in zcl_status enumeration)are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_ADD_SCENE_RES_COMMON | ( | buffer, | |
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id, | |||
| scene_id, | |||
| cmd_id | |||
| ) |
Common macro to send Add Scene response.
| buffer | to put packet to |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| status | of the corresponding Add scene command execution. Appropriate values (defined in zcl_status enumeration)are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| cmd_id | - a response cmd ID (Add Scene or Enh Add Scene) |
| #define ZB_ZCL_SCENES_SEND_COPY_SCENE_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| mode, | |||
| group_id_from, | |||
| scene_id_from, | |||
| group_id_to, | |||
| scene_id_to | |||
| ) |
Send Copy scene command.
The command can be sent to device or group of devices either
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| mode | - a scene copying mode |
| group_id_from | - group identifier for the scene to copy from |
| scene_id_from | - scene identifier to copy from |
| group_id_to | - group identifier for the scene to copy to |
| scene_id_to | - scene identifier to copy to |
| #define ZB_ZCL_SCENES_SEND_COPY_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr, | |||
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id_from, | |||
| scene_id_from | |||
| ) |
Send Copy scene Response command.
The command can be sent to device or group of devices either
| buffer | to put packet to |
| cmd_struct_ptr | - pointer to the place variable-structure part of the command payload (fieldsets) should be placed. |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | - for getting command send status |
| status | - copying status |
| group_id_from | - a group ID to copy from |
| scene_id_from | - a scene ID to copy from |
| #define ZB_ZCL_SCENES_SEND_ENHANCED_ADD_SCENE_RES | ( | buffer, | |
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Enhanced Add Scene response.
| buffer | to put packet to |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| status | of the corresponding Add scene command execution. Appropriate values (defined in zcl_status enumeration)are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_ENHANCED_VIEW_SCENE_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Enhanced View Scene command.
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_GET_SCENE_MEMBERSHIP_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id | |||
| ) |
Send Remove all scenes command.
The command can be sent to device or group of devices either
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_addr_mode | - addressing mode. Either ZB_APS_ADDR_MODE_16_ENDP_PRESENT or ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT will fit |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_GET_SCENE_MEMBERSHIP_RES | ( | buffer, | |
| cmd_struct_ptr, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback | |||
| ) |
Sends Get scene membership response.
| buffer | with prepared command payload |
| cmd_struct_ptr | - pointer to the place directly after the payload |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| #define ZB_ZCL_SCENES_SEND_RECALL_SCENE_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id | |||
| ) |
Macro for calling zb_zcl_scenes_send_recall_scene_req function
| #define ZB_ZCL_SCENES_SEND_RECALL_SCENE_REQ_ZCL8 | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id, | |||
| transition_time | |||
| ) |
Macro for call zb_zcl_scenes_send_recall_scene_req_zcl8 function
| #define ZB_ZCL_SCENES_SEND_REMOVE_ALL_SCENES_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id | |||
| ) |
Send Remove all scenes command.
The command can be sent to device or group of devices either
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_addr_mode | - addressing mode. Either ZB_APS_ADDR_MODE_16_ENDP_PRESENT or ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT will fit |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_REMOVE_ALL_SCENES_RES | ( | buffer, | |
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id | |||
| ) |
Send Remove all scenes response.
| buffer | to put packet to |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| status | of the corresponding Add scene command execution. Appropriate values (defined in zcl_status enumeration)are:
|
| group_id | - group identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_REMOVE_SCENE_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Remove scene command.
The command can be sent to device or group of devices either
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_addr_mode | - addressing mode. Either ZB_APS_ADDR_MODE_16_ENDP_PRESENT or ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT will fit |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_REMOVE_SCENE_RES | ( | buffer, | |
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Remove Scene response.
| buffer | to put packet to |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| status | of the corresponding Add scene command execution. Appropriate values (defined in zcl_status enumeration)are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_STORE_SCENE_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Store Scene command.
The command can be sent to device or group of devices either
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_addr_mode | - addressing mode. Either ZB_APS_ADDR_MODE_16_ENDP_PRESENT or ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT will fit |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_STORE_SCENE_RES | ( | buffer, | |
| seq_num, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback, | |||
| status, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send Store scene response.
| buffer | to put packet to |
| seq_num | - ZCL sequence number |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| status | of the corresponding Add scene command execution. Appropriate values (defined in zcl_status enumeration)are:
|
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_VIEW_SCENE_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id | |||
| ) |
Send View Scene commands.
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| #define ZB_ZCL_SCENES_SEND_VIEW_SCENE_REQ_COMMON | ( | buffer, | |
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| dis_default_resp, | |||
| callback, | |||
| group_id, | |||
| scene_id, | |||
| view_scene_cmd_id | |||
| ) |
Common macro to send View Scene commands.
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| view_scene_cmd_id | - command ID (View Scene or Enhanced View Scene) |
| #define ZB_ZCL_SCENES_SEND_VIEW_SCENE_RES | ( | buffer, | |
| cmd_struct_ptr, | |||
| dst_addr, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| callback | |||
| ) |
Sends View scene response.
| buffer | with prepared command payload |
| cmd_struct_ptr | - pointer to the place variable-structure part of the |
| dst_addr | - address to send packet to |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| callback | for getting command send status |
| #define ZB_ZCL_SCENES_TRANSITION_TIME_DEFAULT_VALUE 0 |
Default value for scene transition time.
Fixed-size part of the Scene table.
| typedef struct zb_zcl_scenes_add_scene_req_s zb_zcl_scenes_add_scene_req_t |
Inform User App about Scene cluster Add Scene command.
| typedef struct zb_zcl_scenes_add_scene_res_s zb_zcl_scenes_add_scene_res_t |
Add scene response payload structure.
| typedef struct zb_zcl_scenes_copy_scene_mode_s zb_zcl_scenes_copy_scene_mode_t |
Scene copying mode bitfield.
| typedef struct zb_zcl_scenes_copy_scene_req_s zb_zcl_scenes_copy_scene_req_t |
Copy scene command payload structure.
| typedef struct zb_zcl_scenes_fieldset_common_s zb_zcl_scenes_fieldset_common_t |
Common part of the field set definition.
Get scene membership command payload structure.
| typedef struct zb_zcl_scenes_get_scene_membership_res_mandatory_s zb_zcl_scenes_get_scene_membership_res_mandatory_t |
Get scene membership response fixed-structure payload part representation.
| typedef struct zb_zcl_scenes_get_scene_membership_res_optional_s zb_zcl_scenes_get_scene_membership_res_optional_t |
Get scene membership response optional payload part representation.
Get scene membership response.
| typedef struct zb_zcl_scenes_recall_scene_req_s zb_zcl_scenes_recall_scene_req_t |
Recall scene command payload structure.
| typedef struct zb_zcl_scenes_recall_scene_transition_time_req_s zb_zcl_scenes_recall_scene_transition_time_req_t |
Recall scene command transition_time payload structure.
Remove all scenes command payload structure.
Remove all scenes response payload structure.
| typedef struct zb_zcl_scenes_remove_scene_req_s zb_zcl_scenes_remove_scene_req_t |
Remove scene command payload structure.
| typedef struct zb_zcl_scenes_remove_scene_res_s zb_zcl_scenes_remove_scene_res_t |
Remove scene response payload structure.
| typedef struct zb_zcl_scenes_store_scene_req_s zb_zcl_scenes_store_scene_req_t |
Store scene command payload structure.
| typedef struct zb_zcl_scenes_store_scene_res_s zb_zcl_scenes_store_scene_res_t |
Store scene response payload structure.
| typedef struct zb_zcl_scenes_view_scene_req_s zb_zcl_scenes_view_scene_req_t |
View scene command payload structure.
Mandatory part of the Scenes.ViewSceneResponse payload.
| enum zb_zcl_scene_attr_e |
Scene cluster attribute identifiers.
| enum zb_zcl_scenes_cmd_e |
Command identifiers for Scenes Cluster.
Command response identifiers for Scenes Cluster.
| void zb_zcl_scenes_send_recall_scene_req | ( | zb_bufid_t | buffer, |
| const zb_addr_u * | dst_addr, | ||
| zb_uint8_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | ep, | ||
| zb_uint16_t | prof_id, | ||
| zb_uint8_t | dis_default_resp, | ||
| zb_callback_t | callback, | ||
| zb_uint16_t | group_id, | ||
| zb_uint8_t | scene_id | ||
| ) |
Send Recall scene command (pre-ZCL8) Use zb_zcl_scenes_send_recall_scene_req_zcl8 for ZCL8 revision call. The command can be sent to device or group of devices either.
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_addr_mode | - addressing mode. Either ZB_APS_ADDR_MODE_16_ENDP_PRESENT or ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT will fit |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| void zb_zcl_scenes_send_recall_scene_req_zcl8 | ( | zb_bufid_t | buffer, |
| const zb_addr_u * | dst_addr, | ||
| zb_uint8_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | ep, | ||
| zb_uint16_t | prof_id, | ||
| zb_uint8_t | dis_default_resp, | ||
| zb_callback_t | callback, | ||
| zb_uint16_t | group_id, | ||
| zb_uint8_t | scene_id, | ||
| zb_uint16_t | transition_time | ||
| ) |
Send Recall scene command The command can be sent to device or group of devices either.
| buffer | to put packet to |
| dst_addr | - address to send packet to |
| dst_addr_mode | - addressing mode. Either ZB_APS_ADDR_MODE_16_ENDP_PRESENT or ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT will fit |
| dst_ep | - destination endpoint (if sendting to a particular device) |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| dis_default_resp | - enable/disable default response |
| callback | for getting command send status |
| group_id | - group identifier for the scene to store |
| scene_id | - scene identifier for the scene to store |
| transition_time | - determines how long the transition takes from the old cluster state to the new cluster state |