|
| enum | zb_zcl_price_set_received_block_threshold_e {
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK1_THRESHOLD = ZB_ZCL_ATTR_SET_WITH_ATTR_ID(ZB_ZCL_PRICE_SET_RECEIVED_BLOCK_THRESHOLD, 0x00),
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK2_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK3_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK4_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK5_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK6_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK7_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK8_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK9_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK10_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK11_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK12_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK13_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK14_THRESHOLD,
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK15_THRESHOLD
} |
| | Received Block Threshold Attributes Set. More...
|
| |
This set of attributes provides remote access to the Price server ReceivedBlockThresholds. The number of block thresholds is indicated by the NumberOfBlockThresholds field in the associated PublishTariffInformation command. The number of blocks is one greater than the number of thresholds.
§ zb_zcl_price_set_received_block_threshold_e
#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_price.h>
Received Block Threshold Attributes Set.
- See also
- SE spec, D.4.2.2.11
| Enumerator |
|---|
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK1_THRESHOLD | The format of these attributes is the same as for the 'Delivered' Block Thresholds
|
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK2_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK3_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK4_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK5_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK6_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK7_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK8_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK9_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK10_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK11_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK12_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK13_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK14_THRESHOLD | |
| ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK15_THRESHOLD | |