This set of attributes provides remote access to the Price server Billing information.
§ zb_zcl_price_set_billing_information_e
#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_price.h>
Billing Information (Delivered) Attributes Set.
- See also
- SE spec, D.4.2.2.8
| Enumerator |
|---|
| ZB_ZCL_ATTR_PRICE_SRV_CURRENT_BILLING_PERIOD_START | The CurrentBillingPeriodStart attribute represents the start time of the current billing period.
|
| ZB_ZCL_ATTR_PRICE_SRV_CURRENT_BILLING_PERIOD_DURATION | The CurrentBillingPeriodDuration attribute represents the current billing period duration in minutes.
|
| ZB_ZCL_ATTR_PRICE_SRV_LAST_BILLING_PERIOD_START | The LastBillingPeriodStart attribute represents the start time of the last billing period.
|
| ZB_ZCL_ATTR_PRICE_SRV_LAST_BILLING_PERIOD_DURATION | The LastBillingPeriodDuration attribute is the duration of the last billing period in minutes (start to end of last billing period).
|
| ZB_ZCL_ATTR_PRICE_SRV_LAST_BILLING_PERIOD_CONSOLIDATED_BILL | The LastBillingPeriodConsolidatedBill attribute is an amount for the cost of the energy supplied from the date of the LastBillingPeriodStart attribute and until the duration of the LastBillingPeriodDuration attribute expires, measured in base unit of Currency with the decimal point located as indicated by the Trailing Digits attribute.
|