Logo
Developing with ZBOSS for Zigbee
ZCL Illuminance Measurement cluster

Illuminance Measurement cluster attributes

enum  zb_zcl_illuminance_measurement_attr_e {
  ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_ID = 0x0000, ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_ID = 0x0001, ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_ID = 0x0002, ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_TOLERANCE_ID = 0x0003,
  ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_LIGHT_SENSOR_TYPE_ID = 0x0004
}
 Illuminance Measurement cluster attribute identifiers. More...
 
#define ZB_ZCL_ILLUMINANCE_MEASUREMENT_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)
 Default value for Illuminance Measurement cluster revision global attribute. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_TOO_LOW   0
 MeasuredValue attribute too-low value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_INVALID   0xFFFF
 MeasuredValue attribute invalid value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_DEFAULT   ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_TOO_LOW
 MeasuredValue attribute default value. More...
 
#define ZB_ZCL_ILLUMINANCE_MEASUREMENT_LIGHT_SENSOR_TYPE_DEFAULT_VALUE   ((zb_uint8_t)0xFF)
 Default value for LightSensorType attribute. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_MIN_VALUE   0x0001
 MinMeasuredValue attribute minimum value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_MAX_VALUE   0xFFFD
 MinMeasuredValue attribute maximum value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_UNDEFINED   0xFFFF
 MinMeasuredValue attribute not-defined value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_MIN_VALUE   0x0002
 MaxMeasuredValue attribute minimum value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_MAX_VALUE   0xFFFE
 MaxMeasuredValue attribute maximum value. More...
 
#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_UNDEFINED   0xFFFF
 MaxMeasuredValue attribute not-defined value. More...
 
#define ZB_ZCL_DECLARE_ILLUMINANCE_MEASUREMENT_ATTRIB_LIST(attr_list, value, min_value, max_value)
 Declare attribute list for Illuminance Measurement cluster - server side. More...
 

Detailed Description

Macro Definition Documentation

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_MAX_VALUE

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_MAX_VALUE   0xFFFE

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_MIN_VALUE

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_MIN_VALUE   0x0002

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_UNDEFINED

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_UNDEFINED   0xFFFF

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_DEFAULT

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_INVALID

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_INVALID   0xFFFF

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_TOO_LOW

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_TOO_LOW   0

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_MAX_VALUE

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_MAX_VALUE   0xFFFD

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_MIN_VALUE

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_MIN_VALUE   0x0001

§ ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_UNDEFINED

#define ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_UNDEFINED   0xFFFF

§ ZB_ZCL_DECLARE_ILLUMINANCE_MEASUREMENT_ATTRIB_LIST

#define ZB_ZCL_DECLARE_ILLUMINANCE_MEASUREMENT_ATTRIB_LIST (   attr_list,
  value,
  min_value,
  max_value 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_illuminance_measurement.h>

Value:
ZB_ZCL_START_DECLARE_ATTRIB_LIST_CLUSTER_REVISION(attr_list, ZB_ZCL_ILLUMINANCE_MEASUREMENT) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_ID, (min_value)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_ID, (max_value)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
MeasuredValue, ZCL spec 4.2.2.2.1.1.
Definition: zb_zcl_illuminance_measurement.h:50
MinMeasuredValue, ZCL spec 4.2.2.2.1.2.
Definition: zb_zcl_illuminance_measurement.h:52
MaxMeasuredValue, ZCL spec 4.2.2.2.1.3.
Definition: zb_zcl_illuminance_measurement.h:54

Declare attribute list for Illuminance Measurement cluster - server side.

Parameters
attr_list- attribute list name
value- pointer to variable to store MeasuredValue attribute
min_value- pointer to variable to store MinMeasuredValue attribute
max_value- pointer to variable to store MAxMeasuredValue attribute

§ ZB_ZCL_ILLUMINANCE_MEASUREMENT_CLUSTER_REVISION_DEFAULT

#define ZB_ZCL_ILLUMINANCE_MEASUREMENT_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)

§ ZB_ZCL_ILLUMINANCE_MEASUREMENT_LIGHT_SENSOR_TYPE_DEFAULT_VALUE

#define ZB_ZCL_ILLUMINANCE_MEASUREMENT_LIGHT_SENSOR_TYPE_DEFAULT_VALUE   ((zb_uint8_t)0xFF)

Enumeration Type Documentation

§ zb_zcl_illuminance_measurement_attr_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_illuminance_measurement.h>

Illuminance Measurement cluster attribute identifiers.

See also
ZCL spec, Illuminance Measurement Cluster 4.2.2.2.1
Enumerator
ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MEASURED_VALUE_ID 

MeasuredValue, ZCL spec 4.2.2.2.1.1.

ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MIN_MEASURED_VALUE_ID 

MinMeasuredValue, ZCL spec 4.2.2.2.1.2.

ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_MAX_MEASURED_VALUE_ID 

MaxMeasuredValue, ZCL spec 4.2.2.2.1.3.

ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_TOLERANCE_ID 

The Tolerance attribute SHALL indicate the magnitude of the possible error that is associated with MeasuredValue, using the same units and resolution.

ZB_ZCL_ATTR_ILLUMINANCE_MEASUREMENT_LIGHT_SENSOR_TYPE_ID 

The LightSensorType attribute specifies the electronic type of the light sensor.