Logo
Developing with ZBOSS for Zigbee
ZCL DoorLock cluster

Data Structures

struct  zb_zcl_door_lock_read_lock_door_res_payload_s
 
struct  zb_zcl_door_lock_read_unlock_door_res_payload_s
 

Door Lock cluster attributes

enum  zb_zcl_door_lock_attr_e {
  ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_ID = 0x0000, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_ID = 0x0001, ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ID = 0x0002, ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ID = 0x0003,
  ZB_ZCL_ATTR_DOOR_LOCK_NUM_OF_DOOR_OPEN_EVENTS_ID = 0x0004, ZB_ZCL_ATTR_DOOR_LOCK_NUM_OF_DOOR_CLOSED_EVENTS_ID = 0x0005, ZB_ZCL_ATTR_DOOR_LOCK_OPEN_PERIOD_ID = 0x0006, ZB_ZCL_ATTR_DOOR_LOCK_NUMBER_OF_LOG_RECORDS_SUPPORTED_ID = 0x0010,
  ZB_ZCL_ATTR_DOOR_LOCK_NUM_TOTAL_USERS_ID = 0x0011, ZB_ZCL_ATTR_DOOR_LOCK_NUM_PIN_USERS_ID = 0x0012, ZB_ZCL_ATTR_DOOR_LOCK_NUMBER_OF_RFID_USERS_SUPPORTED_ID = 0x0013, ZB_ZCL_ATTR_DOOR_LOCK_NUM_WEEK_DAY_SCHEDULE_PER_USER_ID = 0x0014,
  ZB_ZCL_ATTR_DOOR_LOCK_NUM_YEAR_DAY_SCHEDULE_PER_USER_ID = 0x0015, ZB_ZCL_ATTR_DOOR_LOCK_NUM_HOLIDAY_SCHEDULE_ID = 0x0016, ZB_ZCL_ATTR_DOOR_LOCK_MAX_PIN_LEN_ID = 0x0017, ZB_ZCL_ATTR_DOOR_LOCK_MIN_PIN_LEN_ID = 0x0018,
  ZB_ZCL_ATTR_DOOR_LOCK_MAX_RFID_CODE_LENGTH_ID = 0x0019, ZB_ZCL_ATTR_DOOR_LOCK_MIN_RFID_CODE_LENGTH_ID = 0x001A, ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_LOGGING_ID = 0x0020, ZB_ZCL_ATTR_DOOR_LOCK_LANGUAGE_ID = 0x0021,
  ZB_ZCL_ATTR_DOOR_LOCK_LED_SETTINGS_ID = 0x0022, ZB_ZCL_ATTR_DOOR_LOCK_AUTO_RELOCK_TIME_ID = 0x0023, ZB_ZCL_ATTR_DOOR_LOCK_SOUND_VOLUME_ID = 0x0024, ZB_ZCL_ATTR_DOOR_LOCK_OPERATING_MODE_ID = 0x0025,
  ZB_ZCL_ATTR_DOOR_LOCK_OPERATION_MODES_SUPPORTED_ID = 0x0026, ZB_ZCL_ATTR_DOOR_LOCK_DEFAULT_CONFIGURATION_REGISTER_ID = 0x0027, ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_LOCAL_PROGRAMMING_ID = 0x0028, ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_ONE_TOUCH_LOCKING_ID = 0x0029,
  ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_INSIDE_STATUS_LED_ID = 0x002A, ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_PRIVACY_MODE_BUTTON_ID = 0x002B, ZB_ZCL_ATTR_DOOR_LOCK_WRONG_CODE_ENTRY_LIMIT_ID = 0x0030, ZB_ZCL_ATTR_DOOR_LOCK_USER_CODE_TEMPORARY_DISABLE_TIME_ID = 0x0031,
  ZB_ZCL_ATTR_DOOR_LOCK_SEND_PIN_OVER_THE_AIR_ID = 0x0032, ZB_ZCL_ATTR_DOOR_LOCK_REQUIRE_PIN_RF_ID = 0x0033, ZB_ZCL_ATTR_DOOR_LOCK_SECURITY_LEVEL_ID = 0x0034, ZB_ZCL_ATTR_DOOR_LOCK_ALARM_MASK_ID = 0x0040,
  ZB_ZCL_ATTR_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_ID = 0x0041, ZB_ZCL_ATTR_DOOR_LOCK_RF_OPERATION_EVENT_MASK_ID = 0x0042, ZB_ZCL_ATTR_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_ID = 0x0043, ZB_ZCL_ATTR_DOOR_LOCK_RFID_OPERATION_EVENT_MASK_ID = 0x0044,
  ZB_ZCL_ATTR_DOOR_LOCK_KEYPAD_PROGRAMMING_EVENT_MASK_ID = 0x0045, ZB_ZCL_ATTR_DOOR_LOCK_RF_PROGRAMMING_EVENT_MASK_ID = 0x0046, ZB_ZCL_ATTR_DOOR_LOCK_RFID_PROGRAMMING_EVENT_MASK_ID = 0x0047
}
 Door Lock cluster attribute identifiers. More...
 
enum  zb_zcl_door_lock_lock_state_e { ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_NOT_FULLY_LOCKED = 0x00, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_LOCKED = 0x01, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNLOCKED = 0x02, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNDEFINED = 0xff }
 Values for LockState attribute. More...
 
enum  zb_zcl_door_lock_lock_type_e { ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_DEADBOLT = 0x00, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_MAGNETIC = 0x01, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_OTHER = 0x02, ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_UNDEFINED = 0xff }
 Values for LockType attribute. More...
 
enum  zb_zcl_door_lock_actuator_enabled_e { ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_DISABLED = 0x0b0, ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ENABLED = 0x0b1 }
 Values for ActuatorEnabled attribute. More...
 
enum  zb_zcl_door_lock_door_state_e {
  ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_OPEN = 0x00, ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_CLOSED = 0x01, ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ERROR_JAMMED = 0x02, ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ERROR_FORCED_OPEN = 0x03,
  ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ERROR_UNSPECIFIED = 0x04
}
 Values for DoorState attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0003u)
 Default value for Door Lock cluster revision global attribute. More...
 
#define ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_DEFAULT_VALUE   ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNDEFINED
 Default value for Lock State attribute. More...
 
#define ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_DEFAULT_VALUE   ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_UNDEFINED
 Default value for Lock Type attribute. More...
 
#define ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_DEFAULT_VALUE   ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ENABLED
 Default value for Actuator Enabled attribute. More...
 
#define ZB_ZCL_DECLARE_DOOR_LOCK_ATTRIB_LIST(attr_list, lock_state, lock_type, actuator_enabled)
 Declare attribute list for Door Lock cluster. More...
 

Door Lock cluster commands

enum  zb_zcl_door_lock_cmd_e {
  ZB_ZCL_CMD_DOOR_LOCK_LOCK_DOOR = 0x00, ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_DOOR = 0x01, ZB_ZCL_CMD_DOOR_LOCK_TOGGLE = 0x02, ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_WITH_TIMEOUT = 0x03,
  ZB_ZCL_CMD_DOOR_LOCK_GET_LOG_RECORD = 0x04, ZB_ZCL_CMD_DOOR_LOCK_SET_PIN_CODE = 0x05, ZB_ZCL_CMD_DOOR_LOCK_GET_PIN_CODE = 0x06, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_PIN_CODE = 0x07,
  ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_PIN_CODES = 0x08, ZB_ZCL_CMD_DOOR_LOCK_SET_USER_STATUS = 0x09, ZB_ZCL_CMD_DOOR_LOCK_GET_USER_STATUS = 0x0A, ZB_ZCL_CMD_DOOR_LOCK_SET_WEEKDAY_SCHEDULE = 0x0B,
  ZB_ZCL_CMD_DOOR_LOCK_GET_WEEKDAY_SCHEDULE = 0x0C, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_WEEKDAY_SCHEDULE = 0x0D, ZB_ZCL_CMD_DOOR_LOCK_SET_YEAR_DAY_SCHEDULE = 0x0E, ZB_ZCL_CMD_DOOR_LOCK_GET_YEAR_DAY_SCHEDULE = 0x0F,
  ZB_ZCL_CMD_DOOR_LOCK_CLEAR_YEAR_DAY_SCHEDULE = 0x10, ZB_ZCL_CMD_DOOR_LOCK_SET_HOLIDAY_SCHEDULE = 0x11, ZB_ZCL_CMD_DOOR_LOCK_GET_HOLIDAY_SCHEDULE = 0x12, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_HOLIDAY_SCHEDULE = 0x13,
  ZB_ZCL_CMD_DOOR_LOCK_SET_USER_TYPE = 0x14, ZB_ZCL_CMD_DOOR_LOCK_GET_USER_TYPE = 0x15, ZB_ZCL_CMD_DOOR_LOCK_SET_RFID_CODE = 0x16, ZB_ZCL_CMD_DOOR_LOCK_GET_RFID_CODE = 0x17,
  ZB_ZCL_CMD_DOOR_LOCK_CLEAR_RFID_CODE = 0x18, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_RFID_CODES = 0x19
}
 Door Lock cluster commands. More...
 
enum  zb_zcl_door_lock_cmd_resp_e {
  ZB_ZCL_CMD_DOOR_LOCK_LOCK_DOOR_RES = 0x00, ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_DOOR_RES = 0x01, ZB_ZCL_CMD_DOOR_LOCK_TOGGLE_RESPONSE = 0x02, ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_WITH_TIMEOUT_RESPONSE = 0x03,
  ZB_ZCL_CMD_DOOR_LOCK_GET_LOG_RECORD_RESPONSE = 0x04, ZB_ZCL_CMD_DOOR_LOCK_SET_PIN_CODE_RESPONSE = 0x05, ZB_ZCL_CMD_DOOR_LOCK_GET_PIN_CODE_RESPONSE = 0x06, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_PIN_CODE_RESPONSE = 0x07,
  ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_PIN_CODES_RESPONSE = 0x08, ZB_ZCL_CMD_DOOR_LOCK_SET_USER_STATUS_RESPONSE = 0x09, ZB_ZCL_CMD_DOOR_LOCK_GET_USER_STATUS_RESPONSE = 0x0A, ZB_ZCL_CMD_DOOR_LOCK_SET_WEEKDAY_SCHEDULE_RESPONSE = 0x0B,
  ZB_ZCL_CMD_DOOR_LOCK_GET_WEEKDAY_SCHEDULE_RESPONSE = 0x0C, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_WEEKDAY_SCHEDULE_RESPONSE = 0x0D, ZB_ZCL_CMD_DOOR_LOCK_SET_YEAR_DAY_SCHEDULE_RESPONSE = 0x0E, ZB_ZCL_CMD_DOOR_LOCK_GET_YEAR_DAY_SCHEDULE_RESPONSE = 0x0F,
  ZB_ZCL_CMD_DOOR_LOCK_CLEAR_YEAR_DAY_SCHEDULE_RESPONSE = 0x10, ZB_ZCL_CMD_DOOR_LOCK_SET_HOLIDAY_SCHEDULE_RESPONSE = 0x11, ZB_ZCL_CMD_DOOR_LOCK_GET_HOLIDAY_SCHEDULE_RESPONSE = 0x12, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_HOLIDAY_SCHEDULE_RESPONSE = 0x13,
  ZB_ZCL_CMD_DOOR_LOCK_SET_USER_TYPE_RESPONSE = 0x14, ZB_ZCL_CMD_DOOR_LOCK_GET_USER_TYPE_RESPONSE = 0x15, ZB_ZCL_CMD_DOOR_LOCK_SET_RFID_CODE_RESPONSE = 0x16, ZB_ZCL_CMD_DOOR_LOCK_GET_RFID_CODE_RESPONSE = 0x17,
  ZB_ZCL_CMD_DOOR_LOCK_CLEAR_RFID_CODE_RESPONSE = 0x18, ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_RFID_CODES_RESPONSE = 0x19, ZB_ZCL_CMD_DOOR_LOCK_OPERATION_EVENT_NOTIFICATION_ID = 0x20, ZB_ZCL_CMD_DOOR_LOCK_PROGRAMMING_EVENT_NOTIFICATION = 0x21
}
 Door Lock cluster commands response. More...
 
enum  zb_zcl_door_lock_operation_event_source_e {
  ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_KEYPAD = 0x00, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_RF = 0x01, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_MANUAL = 0x02, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_RFID = 0x03,
  ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_INDETERMINATE = 0xFF
}
 
enum  zb_zcl_door_lock_operation_event_code_e {
  ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_UNKNOWN = 0x00, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_LOCK = 0x01, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_UNLOCK = 0x02, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_KEY_LOCK = 0x08,
  ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_KEY_UNLOCK = 0x09, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_MANUAL_LOCK = 0x0D, ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_MANUAL_UNLOCK = 0x0E
}
 
enum  zb_zcl_door_lock_keypad_operation_event_mask_e { ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_UNKNOWN = (1l << 0), ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_LOCK = (1l << 1), ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_UNLOCK = (1l << 2) }
 
enum  zb_zcl_door_lock_rf_operation_event_mask_e { ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_UNKNOWN = (1l << 0), ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_LOCK = (1l << 1), ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_UNLOCK = (1l << 2) }
 
enum  zb_zcl_door_lock_manual_operation_event_mask_e {
  ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_UNKNOWN = (1l << 0), ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_THUMBTURN_LOCK = (1l << 1), ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_THUMBTURN_UNLOCK = (1l << 2), ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_KEY_LOCK = (1l << 4),
  ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_KEY_UNLOCK = (1l << 5), ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_MANUAL_LOCK = (1l << 9), ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_MANUAL_UNLOCK = (1l << 10)
}
 
typedef struct zb_zcl_door_lock_read_lock_door_res_payload_s zb_zcl_door_lock_read_lock_door_res_payload_t
 
typedef struct zb_zcl_door_lock_read_unlock_door_res_payload_s zb_zcl_door_lock_read_unlock_door_res_payload_t
 
#define ZB_ZCL_DOOR_LOCK_NUMBER_OF_LOG_RECORDS_SUPPORTED_DEFAULT_VALUE   ((zb_uint16_t)0)
 Default value for NumberOfLogRecordsSupported attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_NUM_TOTAL_USERS_DEFAULT_VALUE   ((zb_uint16_t)0)
 Default value for NumTotalUsers attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_NUM_PIN_USERS_DEFAULT_VALUE   ((zb_uint16_t)0)
 Default value for NumPINUsers attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_NUMBER_OF_RFID_USERS_SUPPORTED_DEFAULT_VALUE   ((zb_uint16_t)0)
 Default value for NumberOfRFIDUsersSupported attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_NUM_WEEK_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for NumWeekDaySchedulePerUser attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_NUM_YEAR_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for NumYearDaySchedulePerUser attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_NUM_HOLIDAY_SCHEDULE_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for NumHolidaySchedule attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_MAX_PIN_LEN_DEFAULT_VALUE   ((zb_uint8_t)0x08)
 Default value for MaxPINLen attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_MIN_PIN_LEN_DEFAULT_VALUE   ((zb_uint8_t)0x04)
 Default value for MinPINLen attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_MAX_RFID_CODE_LENGTH_DEFAULT_VALUE   ((zb_uint8_t)0x14)
 Default value for MaxRFIDCodeLength attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_MIN_RFID_CODE_LENGTH_DEFAULT_VALUE   ((zb_uint8_t)0x08)
 Default value for MinRFIDCodeLength attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_ENABLE_LOGGING_DEFAULT_VALUE   ((zb_bool_t)0)
 Default value for EnableLogging attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_LANGUAGE_DEFAULT_VALUE   {0}
 Default value for Language attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_LED_SETTINGS_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for LEDSettings attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_AUTO_RELOCK_TIME_DEFAULT_VALUE   ((zb_uint32_t)0)
 Default value for AutoRelockTime attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_SOUND_VOLUME_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for SoundVolume attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_OPERATING_MODE_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for OperatingMode attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_OPERATION_MODES_SUPPORTED_DEFAULT_VALUE   ((zb_uint16_t)0x0001)
 Default value for OperationModesSupported attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_DEFAULT_CONFIGURATION_REGISTER_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for DefaultConfigurationRegister attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_ENABLE_LOCAL_PROGRAMMING_DEFAULT_VALUE   ((zb_bool_t)0x01)
 Default value for EnableLocalProgramming attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_ENABLE_ONE_TOUCH_LOCKING_DEFAULT_VALUE   ((zb_bool_t)0)
 Default value for EnableOneTouchLocking attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_ENABLE_INSIDE_STATUS_LED_DEFAULT_VALUE   ((zb_bool_t)0)
 Default value for EnableInsideStatusLED attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_ENABLE_PRIVACY_MODE_BUTTON_DEFAULT_VALUE   ((zb_bool_t)0)
 Default value for EnablePrivacyModeButton attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_WRONG_CODE_ENTRY_LIMIT_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for WrongCodeEntryLimit attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_USER_CODE_TEMPORARY_DISABLE_TIME_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for UserCodeTemporaryDisableTime attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_SEND_PIN_OVER_THE_AIR_DEFAULT_VALUE   ((zb_bool_t)0)
 Default value for SendPINOverTheAir attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_REQUIRE_PIN_RF_ID_DEFAULT_VALUE   ((zb_bool_t)0)
 Default value for RequirePIN_RF_ID attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_SECURITY_LEVEL_DEFAULT_VALUE   ((zb_uint8_t)0)
 Default value for SecurityLevel attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_ALARM_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for AlarmMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for KeypadOperationEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for RFOperationEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for ManualOperationEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_RFID_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for RFIDOperationEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_KEYPAD_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for KeypadProgrammingEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_RF_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for RFProgrammingEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_RFID_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)
 Default value for RFIDProgrammingEventMask attribute. More...
 
#define ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_REQ(buffer, dst_addr, dst_addr_mode, dst_ep, ep, dis_default_resp, cb)
 General macro for sending a "Door Lock" cluster command. More...
 
#define ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_REQ(buffer, dst_addr, dst_addr_mode, dst_ep, ep, dis_default_resp, cb)
 General macro for sending a "Door Unlock" cluster command. More...
 
#define ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_RES(buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq_num, status, aps_secured)
 Door Lock command send response macro. More...
 
#define ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_RES(buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq_num, status, aps_secured)
 Door Unlock command send response macro. More...
 
#define ZB_ZCL_DOOR_LOCK_READ_LOCK_DOOR_RES(buffer)
 Door Lock response structured reading. More...
 
#define ZB_ZCL_DOOR_LOCK_READ_UNLOCK_DOOR_RES(buffer)
 Door unLock response structured reading. More...
 

Detailed Description

Door Lock cluster defined in ZCL spec, clause 7.3.

The cluster contains 2 command sets:

Both requests have no payload and could be scheduled for sending with corresponding macros. Both responses have simple payload, and their sending and parsing with corresponding macros is almost trivial.

Examples:

Send Door Lock command:

Send Door Unlock command:

Macro Definition Documentation

§ ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_DEFAULT_VALUE

#define ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_DEFAULT_VALUE   ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ENABLED

§ ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_DEFAULT_VALUE

§ ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_DEFAULT_VALUE

§ ZB_ZCL_DECLARE_DOOR_LOCK_ATTRIB_LIST

#define ZB_ZCL_DECLARE_DOOR_LOCK_ATTRIB_LIST (   attr_list,
  lock_state,
  lock_type,
  actuator_enabled 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
ZB_ZCL_START_DECLARE_ATTRIB_LIST_CLUSTER_REVISION(attr_list, ZB_ZCL_DOOR_LOCK) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_ID, (lock_state)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_ID, (lock_type)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ID, (actuator_enabled)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
LockType attribute.
Definition: zb_zcl_door_lock.h:68
LockState attribute.
Definition: zb_zcl_door_lock.h:66
ActuatorEnabled attribute.
Definition: zb_zcl_door_lock.h:70

Declare attribute list for Door Lock cluster.

Parameters
attr_list- attribute list name
lock_state
lock_type
actuator_enabled

§ ZB_ZCL_DOOR_LOCK_ALARM_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_ALARM_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_AUTO_RELOCK_TIME_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_AUTO_RELOCK_TIME_DEFAULT_VALUE   ((zb_uint32_t)0)

§ ZB_ZCL_DOOR_LOCK_CLUSTER_REVISION_DEFAULT

#define ZB_ZCL_DOOR_LOCK_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0003u)

§ ZB_ZCL_DOOR_LOCK_DEFAULT_CONFIGURATION_REGISTER_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_DEFAULT_CONFIGURATION_REGISTER_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_ENABLE_INSIDE_STATUS_LED_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_ENABLE_INSIDE_STATUS_LED_DEFAULT_VALUE   ((zb_bool_t)0)

§ ZB_ZCL_DOOR_LOCK_ENABLE_LOCAL_PROGRAMMING_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_ENABLE_LOCAL_PROGRAMMING_DEFAULT_VALUE   ((zb_bool_t)0x01)

§ ZB_ZCL_DOOR_LOCK_ENABLE_LOGGING_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_ENABLE_LOGGING_DEFAULT_VALUE   ((zb_bool_t)0)

§ ZB_ZCL_DOOR_LOCK_ENABLE_ONE_TOUCH_LOCKING_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_ENABLE_ONE_TOUCH_LOCKING_DEFAULT_VALUE   ((zb_bool_t)0)

§ ZB_ZCL_DOOR_LOCK_ENABLE_PRIVACY_MODE_BUTTON_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_ENABLE_PRIVACY_MODE_BUTTON_DEFAULT_VALUE   ((zb_bool_t)0)

§ ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_KEYPAD_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_KEYPAD_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_LANGUAGE_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_LANGUAGE_DEFAULT_VALUE   {0}

§ ZB_ZCL_DOOR_LOCK_LED_SETTINGS_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_LED_SETTINGS_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_MAX_PIN_LEN_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_MAX_PIN_LEN_DEFAULT_VALUE   ((zb_uint8_t)0x08)

§ ZB_ZCL_DOOR_LOCK_MAX_RFID_CODE_LENGTH_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_MAX_RFID_CODE_LENGTH_DEFAULT_VALUE   ((zb_uint8_t)0x14)

§ ZB_ZCL_DOOR_LOCK_MIN_PIN_LEN_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_MIN_PIN_LEN_DEFAULT_VALUE   ((zb_uint8_t)0x04)

§ ZB_ZCL_DOOR_LOCK_MIN_RFID_CODE_LENGTH_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_MIN_RFID_CODE_LENGTH_DEFAULT_VALUE   ((zb_uint8_t)0x08)

§ ZB_ZCL_DOOR_LOCK_NUM_HOLIDAY_SCHEDULE_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUM_HOLIDAY_SCHEDULE_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_NUM_PIN_USERS_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUM_PIN_USERS_DEFAULT_VALUE   ((zb_uint16_t)0)

§ ZB_ZCL_DOOR_LOCK_NUM_TOTAL_USERS_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUM_TOTAL_USERS_DEFAULT_VALUE   ((zb_uint16_t)0)

§ ZB_ZCL_DOOR_LOCK_NUM_WEEK_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUM_WEEK_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_NUM_YEAR_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUM_YEAR_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_NUMBER_OF_LOG_RECORDS_SUPPORTED_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUMBER_OF_LOG_RECORDS_SUPPORTED_DEFAULT_VALUE   ((zb_uint16_t)0)

§ ZB_ZCL_DOOR_LOCK_NUMBER_OF_RFID_USERS_SUPPORTED_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_NUMBER_OF_RFID_USERS_SUPPORTED_DEFAULT_VALUE   ((zb_uint16_t)0)

§ ZB_ZCL_DOOR_LOCK_OPERATING_MODE_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_OPERATING_MODE_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_OPERATION_MODES_SUPPORTED_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_OPERATION_MODES_SUPPORTED_DEFAULT_VALUE   ((zb_uint16_t)0x0001)

§ ZB_ZCL_DOOR_LOCK_READ_LOCK_DOOR_RES

#define ZB_ZCL_DOOR_LOCK_READ_LOCK_DOOR_RES (   buffer)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
? NULL \
Definition: zb_zcl_door_lock.h:690
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
struct zb_zcl_door_lock_read_lock_door_res_payload_s zb_zcl_door_lock_read_lock_door_res_payload_t
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Door Lock response structured reading.

Parameters
buffer- ID of the message buffer (of type zb_bufid_t) containing payload
Returns
pointer to zb_zcl_door_lock_read_lock_door_res_payload_s structure
Attention
returned pointer will point to the same data in the buffer thus being valid until buffer data will be overwritten.

§ ZB_ZCL_DOOR_LOCK_READ_UNLOCK_DOOR_RES

#define ZB_ZCL_DOOR_LOCK_READ_UNLOCK_DOOR_RES (   buffer)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
? NULL \
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
struct zb_zcl_door_lock_read_unlock_door_res_payload_s zb_zcl_door_lock_read_unlock_door_res_payload_t
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372
Definition: zb_zcl_door_lock.h:707

Door unLock response structured reading.

Parameters
buffer- ID of the message buffer (of type zb_buf_t) containing payload
Returns
pointer to zb_zcl_door_lock_read_unlock_door_res_payload_s structure
Attention
returned pointer will point to the same data in the buffer thus being valid until buffer data will be overwritten.

§ ZB_ZCL_DOOR_LOCK_REQUIRE_PIN_RF_ID_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_REQUIRE_PIN_RF_ID_DEFAULT_VALUE   ((zb_bool_t)0)

§ ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_RF_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_RF_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_RFID_OPERATION_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_RFID_OPERATION_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_RFID_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_RFID_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE   ((zb_uint16_t)0x0000)

§ ZB_ZCL_DOOR_LOCK_SECURITY_LEVEL_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_SECURITY_LEVEL_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_REQ

#define ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_REQ (   buffer,
  dst_addr,
  dst_addr_mode,
  dst_ep,
  ep,
  dis_default_resp,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
ZB_ZCL_SEND_CMD( buffer, \
dst_addr, \
dst_addr_mode, \
dst_ep, \
ep, \
dis_default_resp, \
cb)
#define ZB_AF_HA_PROFILE_ID
Definition: zboss_api_af.h:287
Definition: zb_zcl_door_lock.h:268
#define ZB_ZCL_SEND_CMD( buffer, addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, cluster_id, command_id, cb)
General macro for sending a command with empty payload.
Definition: zb_zcl_common.h:1515
#define ZB_ZCL_CLUSTER_ID_DOOR_LOCK
Definition: zb_zcl_common.h:240

General macro for sending a "Door Lock" cluster command.

Parameters
bufferto put command payload and headers to
dst_addraddress to send to
dst_addr_modedestination address mode
dst_epdestination endpoint
epsource endpoint
dis_default_resp"Disable default response" flag
cbcommand send status callback

§ ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_RES

#define ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_RES (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  seq_num,
  status,
  aps_secured 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_RES_FRAME_CONTROL(ptr); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, seq_num, ZB_ZCL_CMD_DOOR_LOCK_LOCK_DOOR_RES); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, status); \
ZB_ZCL_FINISH_N_SEND_PACKET_NEW(buffer, \
ptr, \
addr, \
dst_addr_mode, \
dst_ep, \
ep, \
prfl_id, \
NULL, \
aps_secured, \
0); \
}
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_CLUSTER_ID_DOOR_LOCK
Definition: zb_zcl_common.h:240
#define ZB_FALSE
Definition: zb_types.h:349
Definition: zb_zcl_door_lock.h:328

Door Lock command send response macro.

Parameters
bufferto put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
seq_num- sequence number
status- result of command execute
aps_secured- APS security mode

§ ZB_ZCL_DOOR_LOCK_SEND_PIN_OVER_THE_AIR_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_SEND_PIN_OVER_THE_AIR_DEFAULT_VALUE   ((zb_bool_t)0)

§ ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_REQ

#define ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_REQ (   buffer,
  dst_addr,
  dst_addr_mode,
  dst_ep,
  ep,
  dis_default_resp,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
ZB_ZCL_SEND_CMD(buffer, \
dst_addr, \
dst_addr_mode, \
dst_ep, \
ep, \
dis_default_resp, \
Definition: zb_zcl_door_lock.h:270
#define ZB_AF_HA_PROFILE_ID
Definition: zboss_api_af.h:287
#define ZB_ZCL_SEND_CMD( buffer, addr, dst_addr_mode, dst_ep, ep, prof_id, dis_default_resp, cluster_id, command_id, cb)
General macro for sending a command with empty payload.
Definition: zb_zcl_common.h:1515
#define ZB_ZCL_CLUSTER_ID_DOOR_LOCK
Definition: zb_zcl_common.h:240

General macro for sending a "Door Unlock" cluster command.

Parameters
bufferto put command payload and headers to
dst_addraddress to send to
dst_addr_modedestination address mode
dst_epdestination endpoint
epsource endpoint
dis_default_resp"Disable default response" flag
cbcommand send status callback

§ ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_RES

#define ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_RES (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  seq_num,
  status,
  aps_secured 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_RES_FRAME_CONTROL(ptr); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, seq_num, ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_DOOR_RES); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, status); \
ZB_ZCL_FINISH_N_SEND_PACKET_NEW(buffer, \
ptr, \
addr, \
dst_addr_mode, \
dst_ep, \
ep, \
prfl_id, \
NULL, \
aps_secured, \
0); \
}
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_CLUSTER_ID_DOOR_LOCK
Definition: zb_zcl_common.h:240
#define ZB_FALSE
Definition: zb_types.h:349
Definition: zb_zcl_door_lock.h:330

Door Unlock command send response macro.

Parameters
bufferto put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
seq_num- sequence number
status- result of command execute
aps_secured- APS security mode

§ ZB_ZCL_DOOR_LOCK_SOUND_VOLUME_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_SOUND_VOLUME_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_USER_CODE_TEMPORARY_DISABLE_TIME_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_USER_CODE_TEMPORARY_DISABLE_TIME_DEFAULT_VALUE   ((zb_uint8_t)0)

§ ZB_ZCL_DOOR_LOCK_WRONG_CODE_ENTRY_LIMIT_DEFAULT_VALUE

#define ZB_ZCL_DOOR_LOCK_WRONG_CODE_ENTRY_LIMIT_DEFAULT_VALUE   ((zb_uint8_t)0)

Typedef Documentation

§ zb_zcl_door_lock_read_lock_door_res_payload_t

§ zb_zcl_door_lock_read_unlock_door_res_payload_t

Enumeration Type Documentation

§ zb_zcl_door_lock_actuator_enabled_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Values for ActuatorEnabled attribute.

See also
ZCL spec, subclause 7.3.2.2.3
Enumerator
ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_DISABLED 

"Disabled" value

ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ENABLED 

"Enabled" value

§ zb_zcl_door_lock_attr_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Door Lock cluster attribute identifiers.

See also
ZCL spec, subclause 7.3.2.2
Enumerator
ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_ID 

LockState attribute.

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_ID 

LockType attribute.

ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ID 

ActuatorEnabled attribute.

ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ID 

DoorState attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_OF_DOOR_OPEN_EVENTS_ID 

DoorOpenEvents attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_OF_DOOR_CLOSED_EVENTS_ID 

DoorClosedEvents attribute.

ZB_ZCL_ATTR_DOOR_LOCK_OPEN_PERIOD_ID 

OpenPeriod attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUMBER_OF_LOG_RECORDS_SUPPORTED_ID 

The number of available log records.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_TOTAL_USERS_ID 

NumberOfTotalUsersSupported attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_PIN_USERS_ID 

NumberOfPINUsersSupported attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUMBER_OF_RFID_USERS_SUPPORTED_ID 

The number of RFID users supported.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_WEEK_DAY_SCHEDULE_PER_USER_ID 

NumberOfWeekDaySchedulesSupportedPerUser attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_YEAR_DAY_SCHEDULE_PER_USER_ID 

NumberOfYearDaySchedulesSupportedPerUser attribute.

ZB_ZCL_ATTR_DOOR_LOCK_NUM_HOLIDAY_SCHEDULE_ID 

NumberOfHolidaySchedulesSupported attribute.

ZB_ZCL_ATTR_DOOR_LOCK_MAX_PIN_LEN_ID 

Max PIN code length attribute.

ZB_ZCL_ATTR_DOOR_LOCK_MIN_PIN_LEN_ID 

Min PIN code length attribute.

ZB_ZCL_ATTR_DOOR_LOCK_MAX_RFID_CODE_LENGTH_ID 

An 8-bit value indicates the maximum length in bytes of a RFID Code on this device.

ZB_ZCL_ATTR_DOOR_LOCK_MIN_RFID_CODE_LENGTH_ID 

An 8-bit value indicates the minimum length in bytes of a RFID Code on this device.

ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_LOGGING_ID 

Enable/disable event logging.

ZB_ZCL_ATTR_DOOR_LOCK_LANGUAGE_ID 

Modifies the language for the on-screen or audible user interface using three bytes from ISO-639-1.

ZB_ZCL_ATTR_DOOR_LOCK_LED_SETTINGS_ID 

The settings for the LED support three different modes.

ZB_ZCL_ATTR_DOOR_LOCK_AUTO_RELOCK_TIME_ID 

The number of seconds to wait after unlocking a lock before it automatically locks again.

ZB_ZCL_ATTR_DOOR_LOCK_SOUND_VOLUME_ID 

The sound volume on a door lock has three possible settings: silent, low and high volumes.

ZB_ZCL_ATTR_DOOR_LOCK_OPERATING_MODE_ID 

OperatingMode attribute.

ZB_ZCL_ATTR_DOOR_LOCK_OPERATION_MODES_SUPPORTED_ID 

SupportedOperatingModes attribute.

ZB_ZCL_ATTR_DOOR_LOCK_DEFAULT_CONFIGURATION_REGISTER_ID 

This attribute represents the default configurations as they are physically set on the device (example: hardware dip switch setting, etc) and represents the default setting for some of the attributes within this Operational Setting Attribute Set (for example: LED, Auto Lock, Sound Volume, and Operating Mode attributes).

ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_LOCAL_PROGRAMMING_ID 

EnableLocalProgramming attribute.

ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_ONE_TOUCH_LOCKING_ID 

Enable/disable the ability to lock the door lock with a single touch on the door lock.

ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_INSIDE_STATUS_LED_ID 

Enable/disable an inside LED that allows the user to see at a glance if the door is locked.

ZB_ZCL_ATTR_DOOR_LOCK_ENABLE_PRIVACY_MODE_BUTTON_ID 

Enable/disable a button inside the door that is used to put the lock into privacy mode.

ZB_ZCL_ATTR_DOOR_LOCK_WRONG_CODE_ENTRY_LIMIT_ID 

The number of incorrect codes or RFID presentment attempts a user is allowed to enter before the door will enter a lockout state.

ZB_ZCL_ATTR_DOOR_LOCK_USER_CODE_TEMPORARY_DISABLE_TIME_ID 

The number of seconds that the lock shuts down following wrong code entry.

ZB_ZCL_ATTR_DOOR_LOCK_SEND_PIN_OVER_THE_AIR_ID 

Boolean set to True if it is ok for the door lock server to send PINs over the air.

ZB_ZCL_ATTR_DOOR_LOCK_REQUIRE_PIN_RF_ID 

Require PIN for RF operation attribute.

ZB_ZCL_ATTR_DOOR_LOCK_SECURITY_LEVEL_ID 

The Security Level attribute allows the door lock manufacturer to indicate what level of security the door lock requires.

ZB_ZCL_ATTR_DOOR_LOCK_ALARM_MASK_ID 

The alarm mask is used to turn on/off alarms for particular functions

ZB_ZCL_ATTR_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_ID 

Event mask used to turn on and off the transmission of keypad operation events.

ZB_ZCL_ATTR_DOOR_LOCK_RF_OPERATION_EVENT_MASK_ID 

Event mask used to turn on and off the transmission of RF operation events.

ZB_ZCL_ATTR_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_ID 

Event mask used to turn on and off manual operation events.

ZB_ZCL_ATTR_DOOR_LOCK_RFID_OPERATION_EVENT_MASK_ID 

Event mask used to turn on and off RFID operation events.

ZB_ZCL_ATTR_DOOR_LOCK_KEYPAD_PROGRAMMING_EVENT_MASK_ID 

Event mask used to turn on and off keypad programming events.

ZB_ZCL_ATTR_DOOR_LOCK_RF_PROGRAMMING_EVENT_MASK_ID 

Event mask used to turn on and off RF programming events.

ZB_ZCL_ATTR_DOOR_LOCK_RFID_PROGRAMMING_EVENT_MASK_ID 

Event mask used to turn on and off RFID programming events.

§ zb_zcl_door_lock_cmd_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Door Lock cluster commands.

See also
ZCL spec, subclause 7.3.2.3 Commands Received
Enumerator
ZB_ZCL_CMD_DOOR_LOCK_LOCK_DOOR 

This command causes the lock device to lock the door.

ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_DOOR 

This command causes the lock device to unlock the door.

ZB_ZCL_CMD_DOOR_LOCK_TOGGLE 

Request the status of the lock.

ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_WITH_TIMEOUT 

This command causes the lock device to unlock the door with a timeout parameter.

ZB_ZCL_CMD_DOOR_LOCK_GET_LOG_RECORD 

Request a log record.

ZB_ZCL_CMD_DOOR_LOCK_SET_PIN_CODE 

Set a PIN into the lock.

ZB_ZCL_CMD_DOOR_LOCK_GET_PIN_CODE 

Retrieve a PIN Code.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_PIN_CODE 

Delete a PIN.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_PIN_CODES 

Clear out all PINs on the lock.

ZB_ZCL_CMD_DOOR_LOCK_SET_USER_STATUS 

Set the status of a user ID.

ZB_ZCL_CMD_DOOR_LOCK_GET_USER_STATUS 

Get the status of a user.

ZB_ZCL_CMD_DOOR_LOCK_SET_WEEKDAY_SCHEDULE 

Set a weekly repeating schedule for a specified user.

ZB_ZCL_CMD_DOOR_LOCK_GET_WEEKDAY_SCHEDULE 

Retrieve the specific weekly schedule for the specific user.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_WEEKDAY_SCHEDULE 

Clear the specific weekly schedule for the specific user.

ZB_ZCL_CMD_DOOR_LOCK_SET_YEAR_DAY_SCHEDULE 

Set a time-specific schedule ID for a specified user.

ZB_ZCL_CMD_DOOR_LOCK_GET_YEAR_DAY_SCHEDULE 

Retrieve the specific year day schedule for the specific user.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_YEAR_DAY_SCHEDULE 

Clears the specific year day schedule for the specific user.

ZB_ZCL_CMD_DOOR_LOCK_SET_HOLIDAY_SCHEDULE 

Set the holiday Schedule by specifying local start time and local end time with respect to any Lock Operating Mode.

ZB_ZCL_CMD_DOOR_LOCK_GET_HOLIDAY_SCHEDULE 

Get the holiday Schedule by specifying Holiday ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_HOLIDAY_SCHEDULE 

Clear the holiday Schedule by specifying Holiday ID.

ZB_ZCL_CMD_DOOR_LOCK_SET_USER_TYPE 

Set the type byte for a specified user.

ZB_ZCL_CMD_DOOR_LOCK_GET_USER_TYPE 

Retrieve the type byte for a specific user.

ZB_ZCL_CMD_DOOR_LOCK_SET_RFID_CODE 

Set an ID for RFID access into the lock.

ZB_ZCL_CMD_DOOR_LOCK_GET_RFID_CODE 

Retrieve an ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_RFID_CODE 

Delete an ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_RFID_CODES 

Clear out all RFIDs on the lock.

§ zb_zcl_door_lock_cmd_resp_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Door Lock cluster commands response.

See also
ZCL spec, subclause 7.3.2.4 Commands Generated
Enumerator
ZB_ZCL_CMD_DOOR_LOCK_LOCK_DOOR_RES 

This command is sent in response to a Lock command with one status byte payload.

ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_DOOR_RES 

This command is sent in response to a Unlock command with one status byte payload.

ZB_ZCL_CMD_DOOR_LOCK_TOGGLE_RESPONSE 

This command is sent in response to a Toggle command with one status byte payload.

ZB_ZCL_CMD_DOOR_LOCK_UNLOCK_WITH_TIMEOUT_RESPONSE 

This command is sent in response to an Unlock with Timeout command with one status byte payload.

ZB_ZCL_CMD_DOOR_LOCK_GET_LOG_RECORD_RESPONSE 

Returns the specified log record.

ZB_ZCL_CMD_DOOR_LOCK_SET_PIN_CODE_RESPONSE 

Returns status of the PIN set command.

ZB_ZCL_CMD_DOOR_LOCK_GET_PIN_CODE_RESPONSE 

Returns the PIN for the specified user ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_PIN_CODE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_PIN_CODES_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_SET_USER_STATUS_RESPONSE 

Returns the pass or fail value for the setting of the user status.

ZB_ZCL_CMD_DOOR_LOCK_GET_USER_STATUS_RESPONSE 

Returns the user status for the specified user ID.

ZB_ZCL_CMD_DOOR_LOCK_SET_WEEKDAY_SCHEDULE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_GET_WEEKDAY_SCHEDULE_RESPONSE 

Returns the weekly repeating schedule data for the specified schedule ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_WEEKDAY_SCHEDULE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_SET_YEAR_DAY_SCHEDULE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_GET_YEAR_DAY_SCHEDULE_RESPONSE 

Returns the weekly repeating schedule data for the specified schedule ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_YEAR_DAY_SCHEDULE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_SET_HOLIDAY_SCHEDULE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_GET_HOLIDAY_SCHEDULE_RESPONSE 

Returns the Holiday Schedule Entry for the specified Holiday ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_HOLIDAY_SCHEDULE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_SET_USER_TYPE_RESPONSE 

Returns the pass or fail value for the setting of the user type.

ZB_ZCL_CMD_DOOR_LOCK_GET_USER_TYPE_RESPONSE 

Returns the user type for the specified user ID.

ZB_ZCL_CMD_DOOR_LOCK_SET_RFID_CODE_RESPONSE 

Returns status of the Set RFID Code command.

ZB_ZCL_CMD_DOOR_LOCK_GET_RFID_CODE_RESPONSE 

Returns the RFID code for the specified user ID.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_RFID_CODE_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_CLEAR_ALL_RFID_CODES_RESPONSE 

Returns pass/fail of the command.

ZB_ZCL_CMD_DOOR_LOCK_OPERATION_EVENT_NOTIFICATION_ID 

The door lock server sends out operation event notification when the event is triggered by the various event sources.

ZB_ZCL_CMD_DOOR_LOCK_PROGRAMMING_EVENT_NOTIFICATION 

The door lock server sends out a programming event notification whenever a programming event takes place on the door lock.

§ zb_zcl_door_lock_door_state_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Values for DoorState attribute.

See also
ZCL spec, subclause 7.3.2.2.4
Enumerator
ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_OPEN 

"Open" value

ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_CLOSED 

"Closed" value

ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ERROR_JAMMED 

"Error (jammed)" value

ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ERROR_FORCED_OPEN 

"Error (forced open)" value

ZB_ZCL_ATTR_DOOR_LOCK_DOOR_STATE_ERROR_UNSPECIFIED 

"Error (unspecified)" value

§ zb_zcl_door_lock_keypad_operation_event_mask_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Enumerator
ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_UNKNOWN 
ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_LOCK 
ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_UNLOCK 

§ zb_zcl_door_lock_lock_state_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Values for LockState attribute.

See also
ZCL spec, subclause 7.3.2.2.1
Enumerator
ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_NOT_FULLY_LOCKED 

"Not fully locked" value

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_LOCKED 

"Locked" value

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNLOCKED 

"Unlocked" value

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNDEFINED 

"Not Defined" value

§ zb_zcl_door_lock_lock_type_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Values for LockType attribute.

See also
ZCL spec, subclause 7.3.2.2.2
Enumerator
ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_DEADBOLT 

"Deadbolt" value

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_MAGNETIC 

"Magnetic" value

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_OTHER 

"Other" value

ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_UNDEFINED 

"Not Defined" value

§ zb_zcl_door_lock_manual_operation_event_mask_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Enumerator
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_UNKNOWN 
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_THUMBTURN_LOCK 
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_THUMBTURN_UNLOCK 
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_KEY_LOCK 
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_KEY_UNLOCK 
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_MANUAL_LOCK 
ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_MANUAL_UNLOCK 

§ zb_zcl_door_lock_operation_event_code_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Enumerator
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_UNKNOWN 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_LOCK 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_UNLOCK 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_KEY_LOCK 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_KEY_UNLOCK 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_MANUAL_LOCK 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_CODE_MANUAL_UNLOCK 

§ zb_zcl_door_lock_operation_event_source_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Enumerator
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_KEYPAD 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_RF 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_MANUAL 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_RFID 
ZB_ZCL_DOOR_LOCK_OPERATION_EVENT_SOURCE_INDETERMINATE 

§ zb_zcl_door_lock_rf_operation_event_mask_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_door_lock.h>

Enumerator
ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_UNKNOWN 
ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_LOCK 
ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_UNLOCK