Diagnostics cluster attribute identifiers.
| Enumerator |
|---|
| ZB_ZCL_ATTR_DIAGNOSTICS_NUMBER_OF_RESETS_ID | number_of_resets, Zigbee Diagnostic Cluster spec 1.2.2.1.1
|
| ZB_ZCL_ATTR_DIAGNOSTICS_PERSISTENT_MEMORY_WRITES_ID | This attribute keeps track of the number of writes to persistent memory. HA spec 9.2.2.2.1.2
|
| ZB_ZCL_ATTR_DIAGNOSTICS_MAC_RX_BCAST_ID | MacRxBcast, HA spec 9.2.2.2.2.1.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_MAC_TX_BCAST_ID | MacTxBcast, HA spec 9.2.2.2.2.2.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_MAC_RX_UCAST_ID | MacRxUcast Attribute A counter that is incremented each time the MAC layer receives a unicast.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_MAC_TX_UCAST_ID | MacTxUcast, HA spec 9.2.2.2.2.4.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_MAC_TX_UCAST_RETRY_ID | MacTxUcastRetry Attribute A counter that is incremented each time the MAC layer retries a unicast.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_MAC_TX_UCAST_FAIL_ID | MacTxUcastFail Attribute A counter that is incremented each time the MAC layer fails to send a unicast.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_RX_BCAST_ID | APSRxBcast Attribute A counter that is incremented each time the APS layer receives a broadcast.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_TX_BCAST_ID | aps_tx_bcast, HA spec 9.3.2.2.2 (??)
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_RX_UCAST_ID | APSRxUcast Attribute A counter that is incremented each time the APS layer receives a unicast.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_TX_UCAST_SUCCESS_ID | aps_tx_ucast_success, HA spec 9.3.2.2.2 (??)
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_TX_UCAST_RETRY_ID | APSTxUcastRetry Attribute A counter that is incremented each time the APS layer retries the sending of a unicast.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_TX_UCAST_FAIL_ID | aps_tx_ucast_fail, HA spec 9.3.2.2.2 (??)
|
| ZB_ZCL_ATTR_DIAGNOSTICS_ROUTE_DISC_INITIATED_ID | RouteDiscInitiated Attribute A counter that is incremented each time a route request is initiated .
|
| ZB_ZCL_ATTR_DIAGNOSTICS_NEIGHBOR_ADDED_ID | NeighborAdded Attribute A counter that is incremented each time an entry is added to the neighbor table.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_NEIGHBOR_REMOVED_ID | NeighborRemoved Attribute A counter that is incremented each time an entry is removed from the neighbor table.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_NEIGHBOR_STALE_ID | A counter that is incremented each time a neighbor table entry becomes stale because the neighbor has not been heard from.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_JOIN_INDICATION_ID | join_indication, HA spec 1.2.2.2.17
|
| ZB_ZCL_ATTR_DIAGNOSTICS_CHILD_MOVED_ID | A counter that is incremented each time an entry is removed from the child table.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_NWKFC_FAILURE_ID | A counter that is incremented each time a message is dropped at the network layer because the APS frame counter was not higher than the last message seen from that source.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APSFC_FAILURE_ID | A counter that is incremented each time a message is dropped at the APS layer because the APS frame counter was not higher than the last message seen from that source.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_UNAUTHORIZED_KEY_ID | A counter that is incremented each time a message is dropped at the APS layer because it had APS encryption but the key associated with the sender has not been authenticated, and thus the key is not authorized for use in APS data messages.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_NWK_DECRYPT_FAILURES_ID | A counter that is incremented each time a NWK encrypted message was received but dropped because decryption failed.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_APS_DECRYPT_FAILURES_ID | A counter that is incremented each time an APS encrypted message was received but dropped because decryption failed.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_PACKET_BUFFER_ALLOCATE_FAILURES_ID | A counter that is incremented each time the stack failed to allocate a packet buffers. This doesn't necessarily mean that the packet buffer count was 0 at the time, but that the number requested was greater than the number free.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_RELAYED_UCAST_ID | A counter that is incremented each time a unicast packet is relayed.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_PHYTOMACQUEUELIMITREACHED_ID | A counter that is incremented each time a packet is dropped because the PHY to MAC queue was exhausted
|
| ZB_ZCL_ATTR_DIAGNOSTICS_PACKET_VALIDATEDROPCOUNT_ID | A counter that is incremented each time a packet was dropped due to a packet validation error. This could be due to length or other formatting problems in the packet.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_AVERAGE_MAC_RETRY_PER_APS_ID | A counter that is equal to the average number of MAC retries needed to send an APS message, HA spec 9.2.2.2.2.27
|
| ZB_ZCL_ATTR_DIAGNOSTICS_LAST_LQI_ID | This is the Link Quality Indicator for the last message received. There is no current agreed upon standard for calculating the LQI. For some implementations LQI is related directly to RSSI for others it is a function of the number of errors received over a fixed number of bytes in a given message. The one thing that has been agreed is that the Link Quality Indicator is a value between 0 and 255 where 0 indicates the worst possible link and 255 indicates the best possible link. Note that for a device reading the Last Message LQI the returned value SHALL be the LQI for the read attribute message used to read the attribute itself.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_LAST_RSSI_ID | This is the receive signal strength indication for the last message received. As with Last Message LQI, a device reading the Last Message RSSI, the returned value SHALL be the RSSI of the read attribute message used to read the attribute itself.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_CUSTOM_ATTR_NWK_RETRY_OVERFLOW_ID | A counter that is incremented on the NWK layer each time tries number of a packet resending are gone.
|
| ZB_ZCL_ATTR_DIAGNOSTICS_CUSTOM_ATTR_PHY_CCA_FAILURES_ID | A non-standard counter that is incremented each time an the PHY layer was unable to transmit due to a failed CCA
|
| ZB_ZCL_ATTR_DIAGNOSTICS_CUSTOM_ATTR_BCAST_TABLE_FULL_ID | A non-standard counter of the number of times the NWK broadcast was dropped because the broadcast table was full.
|