Logo
Developing with ZBOSS for Zigbee
ZCL Daily Schedule cluster

Modules

 Daily Schedule cluster attributes
 
 Daily Schedule cluster commands
 

Macros

#define ZB_ZCL_DAILY_SCHEDULE_CURRENT_AUXILLARY_LOAD_SWITCH_STATE_DEFAULT_VALUE   0x00
 Default value for CurrentAuxiliaryLoadSwitchState attribute. More...
 
#define ZB_ZCL_DAILY_SCHEDULE_LINKY_PEAK_PERIOD_STATUS_DEFAULT_VALUE   0x00
 Default value for LinkyPeakPeriodStatus attribute. More...
 
#define ZB_ZCL_DAILY_SCHEDULE_PEAK_START_TIME_DEFAULT_VALUE   ((zb_uint32_t)0xFFFFFFFF)
 Default value for PeakStartTime attribute. More...
 
#define ZB_ZCL_DAILY_SCHEDULE_PEAK_END_TIME_DEFAULT_VALUE   ((zb_uint32_t)0xFFFFFFFF)
 Default value for PeakEndTime attribute. More...
 
#define ZB_ZCL_DAILY_SCHEDULE_CURRENT_TARIFF_LABEL_DEFAULT_VALUE   {0}
 Default value for CurrentTariffLabel attribute. More...
 

Detailed Description

The Daily Schedule cluster allows information that can be scheduled for an entire day to be transferred within the premises. The information is distributed by an ESI or similar server device.

Macro Definition Documentation

§ ZB_ZCL_DAILY_SCHEDULE_CURRENT_AUXILLARY_LOAD_SWITCH_STATE_DEFAULT_VALUE

#define ZB_ZCL_DAILY_SCHEDULE_CURRENT_AUXILLARY_LOAD_SWITCH_STATE_DEFAULT_VALUE   0x00

§ ZB_ZCL_DAILY_SCHEDULE_CURRENT_TARIFF_LABEL_DEFAULT_VALUE

#define ZB_ZCL_DAILY_SCHEDULE_CURRENT_TARIFF_LABEL_DEFAULT_VALUE   {0}

§ ZB_ZCL_DAILY_SCHEDULE_LINKY_PEAK_PERIOD_STATUS_DEFAULT_VALUE

#define ZB_ZCL_DAILY_SCHEDULE_LINKY_PEAK_PERIOD_STATUS_DEFAULT_VALUE   0x00

§ ZB_ZCL_DAILY_SCHEDULE_PEAK_END_TIME_DEFAULT_VALUE

#define ZB_ZCL_DAILY_SCHEDULE_PEAK_END_TIME_DEFAULT_VALUE   ((zb_uint32_t)0xFFFFFFFF)

§ ZB_ZCL_DAILY_SCHEDULE_PEAK_START_TIME_DEFAULT_VALUE

#define ZB_ZCL_DAILY_SCHEDULE_PEAK_START_TIME_DEFAULT_VALUE   ((zb_uint32_t)0xFFFFFFFF)