Macros | |
| #define | TRACE_ENABLED(m) TRACE_ENABLED_(m) |
| Check that trace is enabled for provided level. To be used in constructions like: More... | |
| #define | ZB_TRACE_FILE_ID 12345U |
Functions | |
| zb_bool_t | zb_trace_level_mask_enabled (zb_uint8_t level, zb_uint32_t mask) |
| Check that trace is enabled for provided level and mask. More... | |
| #define TRACE_ENABLED | ( | m | ) | TRACE_ENABLED_(m) |
Check that trace is enabled for provided level. To be used in constructions like:
| m | - trace level macro. |
| #define ZB_TRACE_FILE_ID 12345U |
Trace file ID used by win_com_dump to identify source file.
Must be first define in the .c file, just before first include directive.
| zb_bool_t zb_trace_level_mask_enabled | ( | zb_uint8_t | level, |
| zb_uint32_t | mask | ||
| ) |
Check that trace is enabled for provided level and mask.
| level | - trace level. |
| mask | - trace mask. |