Logo
DSR GreenBOSS  1.1.0
zb_mac_mhr_s Struct Reference

Parser MAC header. More...

#include <zb_mac.h>

Detailed Description

Parser MAC header.

Mac spec 7.2.1 General MAC frame format.

Note
Actually MHR is of variable length and this structure can't be used for physical data i/o, it is used only for function calls.

The documentation for this struct was generated from the following file: