DSR GreenBOSS
1.1.0
API Reference Guide
Here is a list of all modules:
[detail level
1
2
3
4
]
▼
Application GPD API
The module describes main GPD API that should be used to make own Green Power device
Application Initialization and Configuration
GPD Сommissioning API
▼
GPD Commands API
ON/OFF Сluster Сommands
Scene Сluster Сommands
Level Control Сluster Сommands
Color Control Сluster Сommands
Door Lock Сluster Сommands
▼
ZCL Attribute Reporting
Zigbee Cluster Common Definitions
IAS Zone Cluster Definitions
Power Configuration Cluster Definitions
▼
Bidirectional in Operational API
Specifics of Bidirectional in Operational mode
Commands to be sent by the Bidirectional in Operational application
Helper functions for handling received commands
Functions to provide Rx after Tx for Bidirectional in Operational application
▼
GreenBOSS Internals
The module describes some internal GreenBOSS interfaces
Basic Typedefs
Interface to the Radio
Interface to the Flash
GPD Security
MAC Level
Network Level
Commissioning Internals
▼
GreenBOSS Debug Capabilities
Asserts
Debug Trace
Build Configurations
Copyright (c) 2024 DSR Corporation Denver CO, USA.
http://www.dsr-iot.com
GreenBOSS ZGPD v. 1.1.0 documentation. Wed Oct 29 2025.