Data Fields
ECC_Param Union Reference

Union to format inputs to ECC library. More...

#include <ECCParams.h>

Data Fields

uint32_t word [(32+4)/sizeof(uint32_t)]
 
uint8_t byte [(32+4)]
 

Detailed Description

Union to format inputs to ECC library.

Field Documentation

§ word

uint32_t ECC_Param::word[(32+ 4)/sizeof(uint32_t)]

§ byte

uint8_t ECC_Param::byte[(32+ 4)]

The documentation for this union was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale