Data Fields
ECIESXX_Object Struct Reference

ECIESXX Object. More...

#include <ECIESXX.h>

Collaboration diagram for ECIESXX_Object:
Collaboration graph
[legend]

Data Fields

AESGCM_Config aesConfig
 
AESGCM_Handle aesHandle
 
ANSIX936KDF_Config kdfConfig
 
ANSIX936KDF_Handle kdfHandle
 
ECDH_Config ecdhConfig
 
ECDH_Handle ecdhHandle
 
RNG_Config rngConfig
 
RNG_Handle rngHandle
 
ANSIX936KDFXX_Object kdfObject
 
AESGCMCC26XX_Object aesObject
 
ECDHCC26X2_Object ecdhObject
 
RNGCC26XX_Object rngObject
 
bool isOpen
 

Detailed Description

ECIESXX Object.

The application must not access any member variables of this structure!

Field Documentation

§ aesConfig

AESGCM_Config ECIESXX_Object::aesConfig

§ aesHandle

AESGCM_Handle ECIESXX_Object::aesHandle

§ kdfConfig

ANSIX936KDF_Config ECIESXX_Object::kdfConfig

§ kdfHandle

ANSIX936KDF_Handle ECIESXX_Object::kdfHandle

§ ecdhConfig

ECDH_Config ECIESXX_Object::ecdhConfig

§ ecdhHandle

ECDH_Handle ECIESXX_Object::ecdhHandle

§ rngConfig

RNG_Config ECIESXX_Object::rngConfig

§ rngHandle

RNG_Handle ECIESXX_Object::rngHandle

§ kdfObject

ANSIX936KDFXX_Object ECIESXX_Object::kdfObject

§ aesObject

AESGCMCC26XX_Object ECIESXX_Object::aesObject

§ ecdhObject

ECDHCC26X2_Object ECIESXX_Object::ecdhObject

§ rngObject

RNGCC26XX_Object ECIESXX_Object::rngObject

§ isOpen

bool ECIESXX_Object::isOpen

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale