![]() |
![]() |
ECDSA Parameters. More...
#include <ECDSA.h>

Data Fields | |
| ECDSA_ReturnBehavior | returnBehavior |
| ECDSA_CallbackFxn | callbackFxn |
| uint32_t | timeout |
| void * | custom |
ECDSA Parameters.
ECDSA Parameters are used to with the ECDSA_open() call. Default values for these parameters are set using ECDSA_Params_init().
| ECDSA_ReturnBehavior ECDSA_Params::returnBehavior |
Blocking, callback, or polling return behavior
| ECDSA_CallbackFxn ECDSA_Params::callbackFxn |
Callback function pointer
| uint32_t ECDSA_Params::timeout |
Timeout in system ticks before the operation fails and returns
| void* ECDSA_Params::custom |
Custom argument used by driver implementation