Data Fields
CryptoKey_KeyStore Struct Reference

Key store CryptoKey datastructure. More...

#include <CryptoKey.h>

Data Fields

uint32_t keyLength
 
uint32_t keyID
 
const void * keyAttributes
 

Detailed Description

Key store CryptoKey datastructure.

This structure contains all the information necessary to access keying material stored in a dedicated key store or key database with memory access controls. The application must ensure that the key attributes struct used to initialize the pointer keyAttributes must either be a global variable or it must be available in the context of the function that makes the call to import the key associated with the same key attribute. Otherwise, the keyAttributes pointer will point to a location in stack that could be deallocated.

Field Documentation

§ keyLength

uint32_t CryptoKey_KeyStore::keyLength

§ keyID

uint32_t CryptoKey_KeyStore::keyID

§ keyAttributes

const void* CryptoKey_KeyStore::keyAttributes

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale