SHA2LPF3HSM.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2023-2025, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 /* NOTE: On CC27XX devices, SHA2-224 and SHA2-384 are not yet
34  * supported.
35  */
36 #ifndef ti_drivers_sha2_SHA2LPF3HSM__include
37 #define ti_drivers_sha2_SHA2LPF3HSM__include
38 
39 #include <stdint.h>
40 #include <stdbool.h>
41 
42 #include <ti/drivers/SHA2.h>
43 #include <ti/devices/DeviceFamily.h>
44 
45 #ifdef __cplusplus
46 extern "C" {
47 #endif
48 
51 #define SHA2LPF3HSM_MAX_BLOCK_SIZE_BYTES (SHA2_BLOCK_SIZE_BYTES_512)
52 #define SHA2LPF3HSM_MAX_DIGEST_LENGTH_BYTES (SHA2_DIGEST_LENGTH_BYTES_512)
53 
54 /* The HSM's DMA Controller allows for an inputDataLength
55  * of a DMA transfer to be 2^21 - 1 bytes.
56  */
57 #define DMA_MAX_TXN_LENGTH 0x1FFFFFU
58 
65 typedef struct
66 {
67  uint8_t reserved1;
68 } SHA2LPF3HSM_HWAttrs;
69 
75 typedef struct
76 {
77  CryptoKey *key;
78  uint32_t tempAssetID;
79  uint32_t keyAssetID;
80  uint8_t digest[SHA2LPF3HSM_MAX_DIGEST_LENGTH_BYTES];
81  uint8_t buffer[SHA2LPF3HSM_MAX_BLOCK_SIZE_BYTES];
82  uint32_t accessTimeout;
83  uint32_t bytesProcessed;
84  uint32_t totalDataLength;
85  int_fast16_t returnStatus;
86  SHA2_CallbackFxn callbackFxn;
87  SHA2_ReturnBehavior returnBehavior;
88  SHA2_HashType hashType;
89  uint8_t *input;
90  uint8_t *output;
91  size_t inputLength;
92  size_t digestLength;
93  uint16_t bytesInBuffer;
94  uint8_t algorithm;
95  uint8_t mode;
96  bool isOpen;
97  volatile bool operationInProgress;
98 #if ((DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX))
99  bool driverCreatedKeyAsset;
100 #endif
101 } SHA2LPF3HSM_Object;
102 
105 #ifdef __cplusplus
106 }
107 #endif
108 
109 #endif /* ti_drivers_sha2_SHA2LPF3HSM__include */
CryptoKey datastructure.
Definition: CryptoKey.h:211
SHA2_ReturnBehavior
The way in which SHA2 function calls return after performing an operation.
Definition: SHA2.h:481
SHA2_HashType
Enum for the hash types supported by the driver.
Definition: SHA2.h:502
SHA2 driver header.
void(* SHA2_CallbackFxn)(SHA2_Handle handle, int_fast16_t returnStatus)
The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLB...
Definition: SHA2.h:577
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale