Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
ECIES.h File Reference

Detailed Description

ECIES driver header.


Overview

The Elliptic Curve Integrated Encryption Scheme (ECIES) driver provides a public-key encryption scheme based on Elliptic Curve Cryptography. This driver supports the ECIES implementation defined in the SEC-1 v2.0 standard https://www.secg.org/sec1-v2.pdf except the cipher and MAC functions were changed to use AES-128-GCM:

Function Implementation
Key Agreement ECDH NIST P-256
KDF ANSI X9.63
Hash SHA-256
Cipher AES-128-GCM
MAC AES-128-GCM

Usage

Before starting a ECIES operation, the application must do the following:

Synopsis

// Import ECIES Driver definitions
// Import driver configuration
#include "ti_drivers_config.h"
// Initialize driver
// Open driver instance
handle = ECIES_open(CONFIG_ECIES_0, NULL);
// Perform ECIES encryption
result = ECIES_encrypt(handle, &publicKey, input, sizeof(input), output, sizeof(output));
// Close driver instance
ECIES_close(handle);

Example

The ECIES_encrypt() function performs an ECIES encryption operation in a single call.

After an ECIES operation completes, the application may either start another operation or close the driver by calling ECIES_close().

#define INPUT_SIZE 24
CryptoKey publicKey;
ECIES_Params params;
ECIES_Handle handle;
int_fast16_t result;
uint8_t sharedInfo[] = {0x75, 0xee, 0xf8, 0x1a, 0xa3, 0x04, 0x1e, 0x33,
0xb8, 0x09, 0x71, 0x20, 0x3d, 0x2c, 0x0c, 0x52};
uint8_t input[INPUT_SIZE] = {0x22, 0x51, 0x8b, 0x10, 0xe7, 0x0f, 0x2a, 0x3f,
0x24, 0x38, 0x10, 0xae, 0x32, 0x54, 0x13, 0x9e,
0xfb, 0xee, 0x04, 0xaa, 0x57, 0xc7, 0xaf, 0x7d};
uint8_t output[ECIES_PADDING_BYTES + ECIES_PUBLIC_KEY_SIZE + INPUT_SIZE + ECIES_TAG_SIZE];
uint8_t publicKeyMaterial[] = {0x04,
// X coordinate
0x33,0x91,0x50,0x84,0x4E,0xC1,0x52,0x34,
0x80,0x7F,0xE8,0x62,0xA8,0x6B,0xE7,0x79,
0x77,0xDB,0xFB,0x3A,0xE3,0xD9,0x6F,0x4C,
0x22,0x79,0x55,0x13,0xAE,0xAA,0xB8,0x2F,
// Y coordinate
0xB1,0xC1,0x4D,0xDF,0xDC,0x8E,0xC1,0xB2,
0x58,0x3F,0x51,0xE8,0x5A,0x5E,0xB3,0xA1,
0x55,0x84,0x0F,0x20,0x34,0x73,0x0E,0x9B,
0x5A,0xDA,0x38,0xB6,0x74,0x33,0x6A,0x21};
// RNG initialization should be handled by the application after the RNG
// driver is seeded with the noise input from Radio Control Layer.
handle = ECIES_open(CONFIG_ECIES_0, &params);
assert(handle != NULL);
CryptoKeyPlaintext_initKey(&publicKey, publicKeyMaterial, sizeof(publicKeyMaterial));
result = ECIES_encrypt(handle, &publicKey, input, sizeof(input), output, sizeof(output));
assert(result == ECIES_STATUS_SUCCESS);
ECIES_close(handle);
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/ANSIX936KDF.h>
#include <ti/drivers/cryptoutils/ecc/ECCParams.h>
Include dependency graph for ECIES.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ECIES_Config
 ECIES Global configuration. More...
 
struct  ECIES_Params
 ECIES Parameters. More...
 

Macros

#define ECIES_STATUS_RESERVED   ((int_fast16_t)-32)
 
#define ECIES_STATUS_SUCCESS   ((int_fast16_t)0)
 Successful status code. More...
 
#define ECIES_STATUS_ERROR   ((int_fast16_t)-1)
 Generic error status code. More...
 
#define ECIES_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-2)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define ECIES_STATUS_INSUFFICIENT_OUTPUT_LENGTH   ((int_fast16_t)-3)
 An error status code returned if the output length is insufficient. More...
 
#define ECIES_STATUS_MAC_INVALID   ((int_fast16_t)-4)
 An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation. More...
 
#define ECIES_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED
 The operation does not support non-word-aligned input and/or output. More...
 
#define ECIES_TAG_SIZE   16U
 ECIES authentication tag size in bytes. More...
 
#define ECCParams_NISTP256_LENGTH   32U
 Length of NIST P256 curve parameters in bytes. More...
 
#define ECIES_PUBLIC_KEY_SIZE   (1U + (2U * ECCParams_NISTP256_LENGTH))
 ECIES public key size in bytes. More...
 
#define ECIES_PADDING_BYTES   3U
 ECIES padding size in bytes. More...
 

Typedefs

typedef ECIES_ConfigECIES_Handle
 A handle that is returned from an ECIES_open() call. More...
 

Enumerations

enum  ECIES_ReturnBehavior { ECIES_RETURN_BEHAVIOR_BLOCKING = 2, ECIES_RETURN_BEHAVIOR_POLLING = 4 }
 The way in which ECIES function calls return after performing an operation. More...
 

Functions

void ECIES_init (void)
 Initializes the ECIES driver module. More...
 
void ECIES_Params_init (ECIES_Params *params)
 Initializes params with default values. More...
 
ECIES_Handle ECIES_open (uint_least8_t index, const ECIES_Params *params)
 Initializes a ECIES driver instance and returns a handle. More...
 
void ECIES_close (ECIES_Handle handle)
 Closes a ECIES peripheral specified by handle. More...
 
int_fast16_t ECIES_encrypt (ECIES_Handle handle, const CryptoKey *publicKey, const void *input, size_t inputLen, void *paddedOutput, size_t paddedOutputLen)
 Performs ECIES encryption of a message. More...
 
int_fast16_t ECIES_decrypt (ECIES_Handle handle, const CryptoKey *privateKey, const void *paddedInput, size_t paddedInputLen, void *output, size_t outputLen)
 Performs ECIES decryption of a message. More...
 
ECIES_Handle ECIES_construct (ECIES_Config *config, const ECIES_Params *params)
 Constructs a new ECIES object. More...
 

Variables

const ECIES_Config ECIES_config []
 Global ECIES configuration struct. More...
 
const uint_least8_t ECIES_count
 Global ECIES configuration count. More...
 
const ECIES_Params ECIES_defaultParams
 Default ECIES_Params structure. More...
 

Macro Definition Documentation

§ ECIES_STATUS_RESERVED

#define ECIES_STATUS_RESERVED   ((int_fast16_t)-32)

Common ECIES status code reservation offset. ECIES driver implementations should offset status codes with ECIES_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ECIESXYZ_STATUS_ERROR0 ECIES_STATUS_RESERVED - 0
#define ECIESXYZ_STATUS_ERROR1 ECIES_STATUS_RESERVED - 1
#define ECIESXYZ_STATUS_ERROR2 ECIES_STATUS_RESERVED - 2

§ ECIES_STATUS_SUCCESS

#define ECIES_STATUS_SUCCESS   ((int_fast16_t)0)

Successful status code.

Functions return ECIES_STATUS_SUCCESS if the function was executed successfully.

§ ECIES_STATUS_ERROR

#define ECIES_STATUS_ERROR   ((int_fast16_t)-1)

Generic error status code.

Functions return ECIES_STATUS_ERROR if the function was not executed successfully and no more specific error is applicable.

§ ECIES_STATUS_RESOURCE_UNAVAILABLE

#define ECIES_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-2)

An error status code returned if the hardware or software resource is currently unavailable.

ECIES driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ ECIES_STATUS_INSUFFICIENT_OUTPUT_LENGTH

#define ECIES_STATUS_INSUFFICIENT_OUTPUT_LENGTH   ((int_fast16_t)-3)

An error status code returned if the output length is insufficient.

§ ECIES_STATUS_MAC_INVALID

#define ECIES_STATUS_MAC_INVALID   ((int_fast16_t)-4)

An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation.

This code is returned by ECIES_decrypt() if the verification of the MAC fails.

§ ECIES_STATUS_UNALIGNED_IO_NOT_SUPPORTED

#define ECIES_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED

The operation does not support non-word-aligned input and/or output.

ECIES driver implementations may have restrictions on the alignment of input/output data due to performance limitations of the hardware.

§ ECIES_TAG_SIZE

#define ECIES_TAG_SIZE   16U

ECIES authentication tag size in bytes.

§ ECCParams_NISTP256_LENGTH

#define ECCParams_NISTP256_LENGTH   32U

Length of NIST P256 curve parameters in bytes.

§ ECIES_PUBLIC_KEY_SIZE

#define ECIES_PUBLIC_KEY_SIZE   (1U + (2U * ECCParams_NISTP256_LENGTH))

ECIES public key size in bytes.

The size of the ECIES public key in uncompressed octet string format (0x04 || x || y)

§ ECIES_PADDING_BYTES

#define ECIES_PADDING_BYTES   3U

ECIES padding size in bytes.

The beginning of the input to ECIES_decrypt and the beginning of the output to ECIES_encrypt must be padded with 3-bytes in order to word-align the ciphertext or plaintext as required by the AESGCMLPF3 driver.

Typedef Documentation

§ ECIES_Handle

A handle that is returned from an ECIES_open() call.

Enumeration Type Documentation

§ ECIES_ReturnBehavior

The way in which ECIES function calls return after performing an operation.

Not all ECIES operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

ECIES functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
ECIES_RETURN_BEHAVIOR_BLOCKING X
ECIES_RETURN_BEHAVIOR_POLLING X X X
Enumerator
ECIES_RETURN_BEHAVIOR_BLOCKING 

The function call will block while the ECIES operation goes on in the background. ECIES operation results are available after the function returns.

ECIES_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while the ECIES operation goes on in the background. ECIES operation results are available after the function returns.

Function Documentation

§ ECIES_init()

void ECIES_init ( void  )

Initializes the ECIES driver module.

Precondition
The ECIES_config structure must exist and be persistent before this function can be called. This function must also be called before any other ECIES driver APIs. This function call does not modify any peripheral registers.

§ ECIES_Params_init()

void ECIES_Params_init ( ECIES_Params params)

Initializes params with default values.

Parameters
paramsA pointer to ECIES_Params structure for initialization.

Default values:
returnBehavior = ECIES_RETURN_BEHAVIOR_POLLING
timeout = SemaphoreP_WAIT_FOREVER

§ ECIES_open()

ECIES_Handle ECIES_open ( uint_least8_t  index,
const ECIES_Params params 
)

Initializes a ECIES driver instance and returns a handle.

Warning
The return behavior specified in the ECIES_Params struct must match the RNG's global return behavior setting for this function to succeed.
Precondition
ECIES controller has been initialized using ECIES_init()
Parameters
indexLogical peripheral number for the ECIES indexed into the ECIES_config table.
paramsPointer to a ECIES_Params struct, if NULL it will use default values.
Returns
A ECIES_Handle on success, otherwise NULL if an error occurs or if the driver instance has been opened already.
See also
ECIES_init()
ECIES_close()

§ ECIES_close()

void ECIES_close ( ECIES_Handle  handle)

Closes a ECIES peripheral specified by handle.

Precondition
ECIES_open() has to be called first.
Parameters
handleA ECIES_Handle returned from ECIES_open()
See also
ECIES_open()

§ ECIES_encrypt()

int_fast16_t ECIES_encrypt ( ECIES_Handle  handle,
const CryptoKey publicKey,
const void *  input,
size_t  inputLen,
void *  paddedOutput,
size_t  paddedOutputLen 
)

Performs ECIES encryption of a message.

Performs authenticated encryption (AES-128-GCM) of a message to a NIST P-256 public key which is used to derive the AES-128-GCM encryption key and Initialization Vector (IV).

Note
The paddedOutput will be padded with ECIES_PADDING_BYTES of zeros. This padding must be discarded by the application.
Precondition
ECIES_open() has to be called first.
Parameters
handleA ECIES_Handle returned from ECIES_open().
publicKeyA pointer to the NIST P-256 public key in uncompressed octet string format and big-endian byte order.
inputA pointer to the input buffer containing the data to encrypt.
inputLenThe length of input in bytes.
paddedOutputA pointer to the location to write the output (pad || Q || C || T) where pad is ECIES_PADDING_BYTES of zeros, Q is the public key, C is the ciphertext, and T is the authentication tag.
paddedOutputLenOutput buffer length in bytes. It should be at least (ECIES_PADDING_BYTES + ECIES_PUBLIC_KEY_SIZE + inputLen + ECIES_TAG_SIZE).
Return values
ECIES_STATUS_SUCCESSThe operation succeeded.
ECIES_STATUS_ERRORThe operation failed.
ECIES_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
ECIES_STATUS_INSUFFICIENT_OUTPUT_LENGTHThe outputLen is insufficient to write the output.
ECIES_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
See also
ECIES_open()

§ ECIES_decrypt()

int_fast16_t ECIES_decrypt ( ECIES_Handle  handle,
const CryptoKey privateKey,
const void *  paddedInput,
size_t  paddedInputLen,
void *  output,
size_t  outputLen 
)

Performs ECIES decryption of a message.

Performs authenticated decryption (AES-128-GCM) of a message to a NIST P-256 private key which is used to derive the AES-128-GCM decryption key and Initialization Vector (IV).

Note
The paddedInput must be padded with ECIES_PADDING_BYTES of zeros.
Precondition
ECIES_open() has to be called first.
Parameters
handleA ECIES_Handle returned from ECIES_open().
privateKeyA pointer to the NIST P-256 private key in uncompressed octet string format and big-endian byte order.
paddedInputA pointer to the input buffer containing (pad || Q || C || T) where pad is ECIES_PADDING_BYTES of zeros, Q is the public key, C is the ciphertext, and T is the authentication tag.
paddedInputLenThe length of input in bytes.
outputA pointer to the location to write the output plaintext.
outputLenOutput buffer length in bytes. It should be at least inputLen - ECIES_PUBLIC_KEY_SIZE - ECIES_TAG_SIZE - ECIES_PADDING_BYTES.
Return values
ECIES_STATUS_SUCCESSThe operation succeeded.
ECIES_STATUS_ERRORThe operation failed.
ECIES_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
ECIES_STATUS_INSUFFICIENT_OUTPUT_LENGTHThe outputLen is insufficient to write the output.
ECIES_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
ECIES_STATUS_MAC_INVALIDThe provided authentication tag did not match the recomputed one.
See also
ECIES_open()

§ ECIES_construct()

ECIES_Handle ECIES_construct ( ECIES_Config config,
const ECIES_Params params 
)

Constructs a new ECIES object.

Unlike ECIES_open(), ECIES_construct() does not require the hwAttrs and object to be allocated in a ECIES_Config array that is indexed into. Instead, the ECIES_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Precondition
The ECIES_Config struct must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.
Warning
The return behavior specified in the ECIES_Params struct must match the RNG's global return behavior setting for this function to succeed.
Parameters
configA pointer to a ECIES_Config struct describing the location of the object and hwAttrs.
paramsA pointer to a ECIES_Params struct to configure the driver instance.
Returns
Returns a ECIES_Handle on success or NULL on failure.

Variable Documentation

§ ECIES_config

const ECIES_Config ECIES_config[]

Global ECIES configuration struct.

Specifies context objects and hardware attributes for every driver instance.

This variable is supposed to be defined in the board file.

§ ECIES_count

const uint_least8_t ECIES_count

Global ECIES configuration count.

Specifies the number of available ECIES driver instances.

This variable is supposed to be defined in the board file.

§ ECIES_defaultParams

const ECIES_Params ECIES_defaultParams

Default ECIES_Params structure.

See also
ECIES_Params_init()
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale