548 #ifndef ti_drivers_AESCMAC__include 549 #define ti_drivers_AESCMAC__include 574 #define AESCMAC_STATUS_RESERVED AES_STATUS_RESERVED 582 #define AESCMAC_STATUS_SUCCESS AES_STATUS_SUCCESS 590 #define AESCMAC_STATUS_ERROR AES_STATUS_ERROR 600 #define AESCMAC_STATUS_RESOURCE_UNAVAILABLE AES_STATUS_RESOURCE_UNAVAILABLE 608 #define AESCMAC_STATUS_MAC_INVALID AES_STATUS_MAC_INVALID 613 #define AESCMAC_STATUS_CANCELED AES_STATUS_CANCELED 619 #define AESCMAC_STATUS_FEATURE_NOT_SUPPORTED AES_STATUS_FEATURE_NOT_SUPPORTED 624 #define AESCMAC_STATUS_KEYSTORE_INVALID_ID AES_STATUS_KEYSTORE_INVALID_ID 630 #define AESCMAC_STATUS_KEYSTORE_GENERIC_ERROR AES_STATUS_KEYSTORE_GENERIC_ERROR 638 #define AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTED AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED 746 #define AESCMAC_OP_CODE_MASK 0x0F 762 #define AESCMAC_OP_FLAG_SIGN 0x10 767 #define AESCMAC_OP_FLAGS_MASK (AESCMAC_OP_FLAG_SIGN | AESCMAC_OP_FLAG_VERIFY) 797 int_fast16_t returnValue,
799 AESCMAC_OperationType operationType);
AESCMAC_OperationalMode operationalMode
Definition: AESCMAC.h:812
size_t inputLength
Definition: AESCMAC.h:730
size_t macLength
Definition: AESCMAC.h:736
void AESCMAC_Operation_init(AESCMAC_Operation *operation)
Initializes an AESCMAC_Operation struct to its defaults.
int_fast16_t AESCMAC_oneStepSign(AESCMAC_Handle handle, AESCMAC_Operation *operation, CryptoKey *key)
Performs a AESCMAC signature in one call.
Definition: AESCMAC.h:711
The CryptoKey type is an opaque representation of a cryptographic key.
int_fast16_t AESCMAC_setupSign(AESCMAC_Handle handle, const CryptoKey *key)
Prepares a segmented AESCMAC sign operation.
Definition: AESCMAC.h:776
Definition: AESCMAC.h:779
int_fast16_t AESCMAC_setupVerify(AESCMAC_Handle handle, const CryptoKey *key)
Prepares a segmented AESCMAC verify operation.
AES Global configuration.
Definition: AESCommon.h:154
CryptoKey datastructure.
Definition: CryptoKey.h:211
Definition: AESCMAC.h:754
Definition: AESCommon.h:186
AESCMAC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCMAC.h:772
void AESCMAC_close(AESCMAC_Handle handle)
Closes a AESCMAC peripheral specified by the CMAC handle.
Definition: AESCMAC.h:777
Definition: AESCommon.h:196
AESCMAC_Handle AESCMAC_open(uint_least8_t index, const AESCMAC_Params *params)
Opens a given AESCMAC peripheral.
void AESCMAC_Params_init(AESCMAC_Params *params)
Initializes the AESCMAC_Params struct to its defaults.
#define AESCMAC_OP_FLAG_SIGN
Flag indicating a sign operation. If this bit is not set, then it is a verify operation.
Definition: AESCMAC.h:762
int_fast16_t AESCMAC_cancelOperation(AESCMAC_Handle handle)
Cancels an ongoing AESCMAC operation.
void AESCMAC_init(void)
Initializes the CMAC module.
void(* AESCMAC_CallbackFxn)(AESCMAC_Handle handle, int_fast16_t returnValue, AESCMAC_Operation *operation, AESCMAC_OperationType operationType)
The definition of a callback function used by the AESCMAC driver when used in AESCMAC_RETURN_BEHAVIOR...
Definition: AESCMAC.h:796
const AESCMAC_Params AESCMAC_defaultParams
Default AESCMAC_Params structure.
Definition: AESCommon.h:192
AESCMAC_OperationalMode
Defines the operation modes for the AESCMAC driver.
Definition: AESCMAC.h:708
Definition: AESCMAC.h:778
AESCommon_Config AESCMAC_Config
CMAC Global configuration.
Definition: AESCMAC.h:651
AESCMAC_Config * AESCMAC_Handle
A handle that is returned from an AESCMAC_open() call.
Definition: AESCMAC.h:656
Definition: AESCMAC.h:774
AESCMAC Parameters.
Definition: AESCMAC.h:809
Definition: AESCMAC.h:775
Definition: AESCMAC.h:710
int_fast16_t AESCMAC_finalize(AESCMAC_Handle handle, AESCMAC_Operation *operation)
Finalizes the current segmented operation.
int_fast16_t AESCMAC_oneStepVerify(AESCMAC_Handle handle, AESCMAC_Operation *operation, CryptoKey *key)
Performs a AESCMAC verification in one call.
Definition: AESCMAC.h:680
Definition: AESCMAC.h:753
AESCMAC_CallbackFxn callbackFxn
Definition: AESCMAC.h:813
uint8_t * mac
Definition: AESCMAC.h:724
AES common module header for all devices.
AESCMAC_ReturnBehavior returnBehavior
Definition: AESCMAC.h:811
AESCMAC_Handle AESCMAC_construct(AESCMAC_Config *config, const AESCMAC_Params *params)
Constructs a new AESCMAC object.
uint8_t * input
Definition: AESCMAC.h:719
Struct containing the parameters required for signing or verifying a message.
Definition: AESCMAC.h:717
Definition: AESCMAC.h:755
int_fast16_t AESCMAC_addData(AESCMAC_Handle handle, AESCMAC_Operation *operation)
Adds data to the current segmented operation.
uint32_t timeout
Definition: AESCMAC.h:814
Definition: AESCMAC.h:687
AESCMAC_ReturnBehavior
The return behavior of AESCMAC functions.
Definition: AESCMAC.h:678
void * custom
Definition: AESCMAC.h:817
AESCMAC_OperationCode
Enum for the operation codes supported by the driver.
Definition: AESCMAC.h:751
Definition: AESCMAC.h:692