Data Structures | Typedefs
AESCBCLPF3.h File Reference

Detailed Description

AESCBC driver implementation for the Low Power F3 devices.

==========================================================================

Hardware Accelerator

The Low Power F3 family of devices has dedicated hardware accelerators. CC23XX devices have one dedicated accelerator whereas CC27XX devices have two (Primary and Secondary). Combined they can perform AES encryption operations with 128-bit, 192-bit and 256-bit keys. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted to ensure sensible access timeouts are set.

Implementation Limitations

Runtime Parameter Validation

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input parameter validation coverage is achieved by turning on assertions when compiling the driver.

#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/AESCBC.h>
#include <ti/drivers/cryptoutils/aes/AESCommonLPF3.h>
#include <ti/drivers/cryptoutils/sharedresources/CryptoResourceLPF3.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA.h>
Include dependency graph for AESCBCLPF3.h:

Go to the source code of this file.

Data Structures

struct  AESCBCLPF3_Object
 AESCBCLPF3 Object. More...
 

Typedefs

typedef AESCommonLPF3_HWAttrs AESCBCLPF3_HWAttrs
 AESCBCLPF3 Hardware Attributes. More...
 

Typedef Documentation

§ AESCBCLPF3_HWAttrs

AESCBCLPF3 Hardware Attributes.

AESCBCLPF3 hardware attributes should be included in the board file and pointed to by the AESCBC_config struct.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale