SimpleLink Common Components Module 9.14.00 Release Notes

Table of Contents

Introduction

The SimpleLink Common Components Module (SCCM) includes NV Interface (Non-volatile Memory Interface) and MCUboot. These release notes include bug fixes, updates, and new features for the SCCM components.

Documentation

The follow table details which SCCM components are supported by the different SimpleLink stacks

Stack NV MCUboot
BLE X X
PropRF X
Zigbee X X

What’s New

ID Summary
SCCM-606 Enable NVOCMP voltage check for CC23XX and CC27XX
SCCM-585 Add SCCM Examples for LP_EM_CC2755R10_BG

Fixed Issues

ID Summary
SCCM-608 Compaction bug that results in items lost

Known Issues and Limitations

ID Summary
None None

It should be noted that multiple external NVS regions are not supported. If a user attempts to create a second external NVS region, all actions on the second region will be done on the first region.

Upgrade and Compatibility Information

Dependencies

SCCM components were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.

Technical Support and Product Updates