Radio Control Layer (RCL)
.__unnamed__.rxTx Struct Reference

Data Fields

uint32_t ccaTxStartTime
 
uint32_t * ackData
 
uint16_t fifoCfg
 
uint8_t numPan
 
RCL_StopType txActionStop
 
RCL_Handler_Ieee_TxState txState
 
RCL_Handler_Ieee_RxState rxState
 
RCL_Handler_Ieee_TxAckState txAckState
 
uint8_t ccaContentionWindow
 
bool waitingForValidRssi
 
bool allowTxDelay
 
bool alwaysStoreAck
 
bool frameFiltStop
 
bool immAckExpected
 
bool temperatureRestart
 
uint8_t expSeqNo
 
bool restoreThresh
 
bool coexNoGrant
 
uint8_t coexPriority
 
bool coexPriorityChange
 
bool coexRestart
 
RCL_IEEE_SourceMatchingUpdate srcMatchUpdateDesc
 
RCL_CmdIeee_PanIdAddr srcMatchNewPanIdAddr
 
bool(* srcMatchUpdateFun )(RCL_CmdIeeeRxTx *ieeeCmd)
 
uint16_t demc1be1
 
uint16_t demc1be2
 
volatile uint8_t ackNumRemainingWords
 
volatile uint8_t ackNumWords
 
volatile RCL_IEEE_AckEntryResult ackResult
 
volatile uint8_t bytesReadFromFifo
 
volatile uint16_t savedRxfRp
 
volatile bool rxActionUpdate
 
volatile RCL_Handler_Ieee_SourceMatchUpdatePhase srcMatchUpdatePhase
 

Field Documentation

§ ccaTxStartTime

§ ackData

§ fifoCfg

§ numPan

§ txActionStop

§ txState

§ rxState

§ txAckState

§ ccaContentionWindow

§ waitingForValidRssi

§ allowTxDelay

§ alwaysStoreAck

§ frameFiltStop

§ immAckExpected

§ temperatureRestart

§ expSeqNo

§ restoreThresh

§ coexNoGrant

§ coexPriority

§ coexPriorityChange

§ coexRestart

§ srcMatchUpdateDesc

§ srcMatchNewPanIdAddr

§ srcMatchUpdateFun

§ demc1be1

§ demc1be2

§ ackNumRemainingWords

§ ackNumWords

§ ackResult

§ bytesReadFromFifo

§ savedRxfRp

§ rxActionUpdate

§ srcMatchUpdatePhase


The documentation for this struct was generated from the following files: