Radio Control Layer (RCL)
RCL_Scheduler.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2022-2023, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_drivers_RCL_Scheduler_h__include
34 #define ti_drivers_RCL_Scheduler_h__include
35 
36 #include <stdint.h>
37 #include <stddef.h>
38 
40 #include <ti/drivers/rcl/hal/hal.h>
41 
45 #define RCL_SCHEDULER_SYSTIM_US(x) (((uint32_t) (x)) * 4U)
46 
49 #define RCL_SCHEDULER_SYSTIM_MS(x) (((uint32_t) (x)) * 4U * 1000U)
50 
51 
52 /* Timing constants */
53 #define ABS_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(100U)
54 #define IMM_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(90U)
55 #define RCL_SCHEDULER_MARGIN_ARM RCL_SCHEDULER_SYSTIM_US(40U)
56 #define RCL_SCHEDULER_MARGIN_CONFIGURE RCL_SCHEDULER_SYSTIM_US(76U)
57 #define RCL_SCHEDULER_MARGIN_LOAD RCL_SCHEDULER_SYSTIM_US(460U)
58 #define RCL_SCHEDULER_SLEEP_CUTOFF RCL_SCHEDULER_SYSTIM_MS(5U)
59 #define RCL_SCHEDULER_TRIG_NOW_DELAY RCL_SCHEDULER_SYSTIM_US(50U)
60 #if defined(DeviceFamily_CC23X0R5) || defined(DeviceFamily_CC23X0R2) || defined(DeviceFamily_CC23X0R22) || defined(DeviceFamily_CC2340R53)
61 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(390U)
62 #elif defined(DeviceFamily_CC27XX)
63 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(150U)
64 #else
65 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(1000U)
66 #endif
67 
68 typedef enum {
74 
75 typedef enum {
80 
81 typedef struct RCL_SchedulerStopInfo_s {
82  uint32_t cmdStopEnabled : 1;
83  uint32_t schedStopEnabled : 1;
84  uint32_t apiStopEnabled : 1;
85  RCL_SchedulerStopReason stopReason : 2;
86  uint32_t cmdStopTime;
87  uint32_t schedStopTime;
89 
90 typedef struct RCL_SchedulerState_s {
91  RCL_Command *currCmd;
92  uint32_t nextWantsStop : 1;
93  RCL_SchedulerStopTimeState stopTimeState : 2;
94  RCL_SchedulerStopReason descheduleReason : 2;
95  RCL_Events postedRclEvents; /* Events to be handled by the command handler */
96  uint32_t actualStartTime;
101 
103 
122 
134 RCL_CommandStatus RCL_Scheduler_setStartStopTime(const RCL_Command *cmd);
135 
149 RCL_CommandStatus RCL_Scheduler_setStartStopTimeEarliestStart(const RCL_Command *cmd, uint32_t earliestStartTime);
150 
166 RCL_CommandStatus RCL_Scheduler_setCustomStartStopTime(const RCL_CommandTiming *timing, RCL_ScheduleType scheduling, bool allowDelay);
167 
185 RCL_CommandStatus RCL_Scheduler_setCustomStartStopTimeEarliestStart(const RCL_CommandTiming *timing, RCL_ScheduleType scheduling, bool allowDelay, uint32_t earliestStartTime);
186 
199 
208 
220 RCL_CommandStatus RCL_Scheduler_setNewStartAbsTime(uint32_t startTime, bool allowDelay);
221 
232 
243 
266 bool RCL_Scheduler_isLater(uint32_t refTime, uint32_t chkTime);
267 
283 int32_t RCL_Scheduler_delta(uint32_t refTime, uint32_t chkTime);
284 
290 static inline uint32_t RCL_Scheduler_getCurrentTime(void)
291 {
292  return hal_get_current_time();
293 }
294 
308 RCL_StopType RCL_Scheduler_setSchedStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t schedStopTime);
309 
323 RCL_StopType RCL_Scheduler_setCmdStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t cmdStopTime);
324 
337 
350 
359 bool RCL_Scheduler_postEvent(RCL_Command_Handle c, RCL_Events e);
360 
364 #endif
RCL_StopType RCL_Scheduler_setStopTimes(void)
Function to apply relevant stop times.
Definition: RCL_Scheduler.c:432
RCL_Events postedRclEvents
Definition: RCL_Scheduler.h:95
RCL_SchedulerStopInfo gracefulStopInfo
Definition: RCL_Scheduler.h:98
RCL_SchedulerState rclSchedulerState
Definition: RCL_Scheduler.c:51
Definition: RCL_Scheduler.h:76
RCL_CommandStatus RCL_Scheduler_setStartStopTime(const RCL_Command *cmd)
Set start and stop time for LRF based on command.
Definition: RCL_Scheduler.c:139
RCL_CommandStatus RCL_Scheduler_setNewStartRelTime(uint32_t relStartTime)
Set new start time for LRF to given time relative to previous LRF start.
Definition: RCL_Scheduler.c:292
bool RCL_Scheduler_isLater(uint32_t refTime, uint32_t chkTime)
Find if a time instant occurs after another, allowing wrap-around.
Definition: RCL_Scheduler.c:483
static uint32_t RCL_Scheduler_getCurrentTime(void)
Get current time.
Definition: RCL_Scheduler.h:289
Definition: RCL_Scheduler.h:77
RCL_StopType
Stop types.
Definition: RCL_Command.h:145
RCL_StopType RCL_Scheduler_setSchedStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t schedStopTime)
Set scheduler stop time.
Definition: RCL_Scheduler.c:529
Definition: RCL_Scheduler.h:81
Definition: RCL_Scheduler.h:72
RCL_ScheduleType
Schedule type.
Definition: RCL_Command.h:157
RCL_StopType RCL_Scheduler_setCmdStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t cmdStopTime)
Set command stop time.
Definition: RCL_Scheduler.c:537
RCL_SchedulerStopReason
Definition: RCL_Scheduler.h:68
RCL_StopType RCL_Scheduler_cancelSchedStopTime(RCL_SchedulerStopInfo *stopInfo)
Cancel scheduler stop time.
Definition: RCL_Scheduler.c:545
RCL_SchedulerStopTimeState
Definition: RCL_Scheduler.h:75
RCL_CommandStatus RCL_Scheduler_setNewStartNow(void)
Set new start time for LRF to now, after a previous start.
Definition: RCL_Scheduler.c:275
RCL_CommandStatus RCL_Scheduler_setStartStopTimeEarliestStart(const RCL_Command *cmd, uint32_t earliestStartTime)
Set start and stop time for LRF based on command with earliest start time.
Definition: RCL_Scheduler.c:164
Definition: RCL_Scheduler.h:70
Definition: RCL_Scheduler.h:71
Definition: RCL_Scheduler.h:69
int32_t RCL_Scheduler_delta(uint32_t refTime, uint32_t chkTime)
Find the time difference between two times, allowing wrap-around.
Definition: RCL_Scheduler.c:501
void * RCL_Command_Handle
Definition: RCL_Types.h:36
uint32_t schedStopTime
Definition: RCL_Scheduler.h:87
uint32_t actualStartTime
Definition: RCL_Scheduler.h:96
uint32_t hal_get_current_time(void)
Definition: hal_cc23x0.c:188
RCL_StopType RCL_Scheduler_cancelCmdStopTime(RCL_SchedulerStopInfo *stopInfo)
Cancel command stop time.
Definition: RCL_Scheduler.c:553
RCL_Command * currCmd
Definition: RCL_Scheduler.h:91
RCL_CommandStatus RCL_Scheduler_setCmdStopTimeNoStartTrigger(const RCL_Command *cmd)
Set stop time for LRF based on command when it does not need a start trigger.
Definition: RCL_Scheduler.c:265
Definition: RCL_Scheduler.h:78
uint16_t requestedPhyFeatures
Definition: RCL_Scheduler.h:99
bool RCL_Scheduler_postEvent(RCL_Command_Handle c, RCL_Events e)
Post event to command handler.
Definition: RCL_Scheduler.c:745
Definition: RCL_Scheduler.h:90
RCL_CommandStatus RCL_Scheduler_setNewStartAbsTime(uint32_t startTime, bool allowDelay)
Set new start time for LRF to given absolute time, after a previous start.
Definition: RCL_Scheduler.c:283
uint32_t cmdStopTime
Definition: RCL_Scheduler.h:86
RCL_CommandStatus RCL_Scheduler_setCustomStartStopTimeEarliestStart(const RCL_CommandTiming *timing, RCL_ScheduleType scheduling, bool allowDelay, uint32_t earliestStartTime)
Set start and stop time for LRF with earliest start time.
Definition: RCL_Scheduler.c:227
RCL_CommandStatus
Command status.
Definition: RCL_Command.h:86
RCL_SchedulerStopInfo hardStopInfo
Definition: RCL_Scheduler.h:97
RCL_CommandStatus RCL_Scheduler_findStopStatus(RCL_StopType stopType)
Get relevant status when a command was stopped.
Definition: RCL_Scheduler.c:70
RCL_CommandStatus RCL_Scheduler_setCustomStartStopTime(const RCL_CommandTiming *timing, RCL_ScheduleType scheduling, bool allowDelay)
Set start and stop time for LRF.
Definition: RCL_Scheduler.c:202