RadioConfig8 9.14.00.03 Release Notes

Table of Contents

Introduction

RadioConfig8 is a SysConfig meta-data package that is used to generate code for configuring the radio.

Documentation

The following documentation is included in RadioConfig8:

What’s New

This list contains all new features since: v9.14.00

ID Summary
RFCONFIG-192 CC2340R53WCSP: BLE 1M/2M/Coded, IEEE Zigbee, 1Mbps/2Mbps GFSK 160khz/320kHz deviation - Add characterized (CZ) settings
RFCONFIG-205 CC2340R53: NESB 1M/2M - Add characterized (CZ) settings

Fixed Issues

This list contains all bugfixes since: v9.14.00

ID Summary
RFCONFIG-196 CC27xx: BLE PHY configuration missing disable ‘TONEINSERT’ for default operation
RFCONFIG-201 CC27XX: Missing compensation for pilot tone extension in PRETXIFS

Known Issues

ID Summary
None None

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

Supported PHYs

Phys available in the external release are marked in bold.

CC2340R2 CC2340R22 CC2340R5 CC2340R53 CC2340R53 on LP-EM-CC2340R53-YBG-WCSP CC2340R53Q1 CC2340R5Q1 CC2744R7Q1 CC2745P10Q1 CC2745R10Q1 CC2745R7Q1 CC2755P10 CC2755R10 CC2755R10 on LP-EM-CC2755R10-YCJ-BG
1 Mbps / 2 Mbps N/A characterized characterized characterized N/A N/A N/A N/A N/A N/A N/A N/A N/A N/A
1 Mbps / 2 Mbps / Coded characterized characterized characterized characterized N/A characterized characterized characterized characterized characterized characterized characterized characterized experimental
1 Mbps / 2 Mbps / Coded High Performance experimental experimental experimental experimental N/A N/A experimental experimental experimental experimental experimental experimental experimental N/A
1 Mbps, 160 kHz dev, GFSK N/A characterized characterized characterized N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
100 kbps, 25 kHz dev, GFSK N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
2 Mbps, 320 kHz dev, GFSK N/A characterized characterized characterized N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
2 Mbps, 500 kHz dev, GFSK N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
20 kbps, 19 kHz dev, FSK, TX N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
250 kbps, 160 kHz dev, GFSK N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
250 kbps, 62.5 kHz dev, GFSK N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
250 kbps, MSK N/A characterized characterized experimental experimental N/A N/A N/A N/A N/A N/A experimental experimental N/A
250 kbps, MSK, FEC N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
250 kbps, O-QPSK characterized characterized characterized characterized N/A N/A N/A characterized characterized characterized characterized characterized characterized experimental
500 kbps, 125 kHz dev, GFSK N/A experimental experimental experimental N/A N/A N/A N/A N/A N/A N/A experimental experimental N/A
ADC Noise characterized characterized characterized characterized experimental characterized characterized experimental experimental experimental experimental experimental experimental N/A
Bare-Metal ACK 2 Mbps, 500 kHz dev, GFSK experimental experimental experimental experimental N/A experimental experimental N/A N/A N/A N/A N/A N/A N/A
Channel Sounding N/A N/A experimental experimental N/A experimental experimental experimental experimental experimental experimental experimental experimental N/A
wBMS, 2 Mbps / 1 Mbps, GFSK N/A N/A N/A N/A N/A N/A N/A N/A N/A experimental N/A N/A N/A N/A

Description of quality levels

Quality Level Description
Experimental Preliminary settings that have been added without being fully characterized on silicon.
The settings are based on previous devices and should not be used for regulatory certification, nor used in a production environment.
Preview Early release settings for getting started with product development.
These settings are not optimized and should not be used for regulatory certification, nor used in a production environment.
- Basic RF parameters have been tested, but not optimized,
- Setting has only been tested at room temperature
Release Candidate This is a fairly mature setting, but has not undergone full characterization and will typically be further optimized.
Characterized Setting is fully characterized and can be used in a production environment.