Packet format debugging
=======================

When testing a custom packet format, it is often convenient to see what the
|PROPRFDEVICE| sends on the air.  The RF core provides the internal signal
``MCE_GPO0`` which reflects the binary modulator input.
:numref:`fig_rf_mce_gpo0_output` shows a pin dump for a packet with the
following configuration:

- ``.preamConf.nPreamBytes`` = 1
- ``.syncWord`` = 0x930B51DE
- ``.pktConf.bVarLen`` = 0x0
- payload: 4 bytes: { 0x81, 0x82, 0x83, 0x84}

.. _fig_rf_mce_gpo0_output:
.. figure:: mce_gpo0_output.png

    Output of the internal modulator signal ``MCE_GPO0`` dumped with a logic
    analyer.

The triggers represent the parts:

A. Preamble
B. Sync word
C. Payload
D. CRC
E. End

There are signal fragments at the beginning of the packet which need to be
filtered out.  The following code snippet routes ``MCE_GPO0`` to
``Board_LED1``::

    #include <inc/hw_rfc_dbell.h>

    // Overrides for CMD_PROP_RADIO_DIV_SETUP
    static uint32_t pOverrides[] =
    {
        // Route MCE_GPO0 to RFC_GPO0
        HW_REG_OVERRIDE(0x1110, RFC_DBELL_SYSGPOCTL_GPOCTL0_MCEGPO0),
        // ...
    }


    #include <ti/drivers/gpio/GPIOCC26XX.h>

    // Route RFC_GPO0 to an LED
    GPIO_setConfigAndMux(Board_LED1, GPIO_CFG_OUTPUT, IOC_PORT_RFC_GPO1);

More information on signal routing can be found
:ref:`here<rf_signal_routing>`.