.. _rflib-rcl-migration-guide:

rflib to RCL Migration Guide
****************************

As |DEVICE| devices do not have a separate CM0 core for RF, a 
`Radio Control Layer (RCL)`_ which is entirely different from the
existing CC26x2 device rflib must be used.

The following sections discuss the major changes to radio commands from the 
main application file between CC26x2 devices and the |DEVICE| devices, 
using ``rfPacketTx.c`` as an example.

.. warning::
    This is not a fully comprehensive list and the API documentation 
    should be consulted when attempting to convert radio commands. File 
    comparison software is highly recommended to compare the difference 
    between application files' radio commands.

Includes 
========

The rflib directory was included for CC26x2 devices

.. code-block:: c

   /***** Includes *****/
   //...

   /* TI Drivers */
   #include <ti/drivers/rf/RF.h>

   /* Driverlib Header files */
   #include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)

   /* Board Header files */
   #include <ti_radio_config.h>

|DEVICE| devices will use RCL instead

.. code-block:: c

   /***** Includes *****/
   //...

   /* TI Drivers */
   #include <ti/drivers/rcl/RCL.h>
   #include <ti/drivers/rcl/RCL_Scheduler.h>
   #include <ti/drivers/rcl/commands/generic.h>

   #if defined(USE_250KBPS_MSK) || defined(USE_500KBPS_MSK)
   #include <setup/generic_fsk_prop_setup.h>
   #else
   #include <setup/generic_1m_prop_setup.h>
   #endif

Defines 
=======

|DEVICE| devices are bound to rely on different definitions since the commands 
are not similar 

.. code-block:: c 

   /***** Defines *****/
   /* Packet TX Configuration */
   #define MAX_LENGTH              (30U) // Max packet length
   #define NUM_DATA_ENTRIES        (2U)  // Number of data entries
   #define NUM_PAD_BYTES           (3U)  // Number of pad bytes

   /* Header length */
   #if defined(USE_500KBPS_MSK) || defined(FIXED_LENGTH_SETUP) // 500KBPS is always set up for fixed length packets
   #define HDR_LEN                 (0U)
   #else
   #if defined(USE_250KBPS_MSK) // 250KBPS with variable length enabled
   #define HDR_LEN                 (1U)
   #else // 1 Mbps with variable length enabled
   #define HDR_LEN                 (2U)
   #endif
   #endif

   #define PACKET_INTERVAL     500000  /* Set packet interval to 500000us or 500ms */

   /* Indicates if FS is off */
   #define FS_OFF                  (1U)  // 0: On, 1: Off

   #if defined(USE_250KBPS_MSK) || defined(USE_500KBPS_MSK)
   #define FREQUENCY               (2433000000U)
   #else
   #define FREQUENCY               (2440000000U)
   #endif

Variables and initialization
============================

``RF_*`` had been initialized for CC26x2 devices

.. code-block:: c

   static RF_Object rfObject;
   static RF_Handle rfHandle;

   // ...

   void *mainThread(void *arg0)
   {
      RF_Params rfParams;
      RF_Params_init(&rfParams);

      /* Request access to the radio */
   #if defined(DeviceFamily_CC26X0R2)
      rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioSetup, &rfParams);
   #else
      rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
   #endif// DeviceFamily_CC26X0R2

      /* Set the frequency */
      RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);

Which |DEVICE| devices replace with ``RCL_*`` variants

.. code-block:: c

   /* RCL Commands */
   RCL_CmdGenericTx   txCmd;               // TX command

   /* RCL Client used to open RCL */
   static RCL_Client  rclClient;

   // ...

   void *mainThread(void *arg0)
   {
      /* Initialize and open RCL */
      RCL_init();

   #if defined(USE_250KBPS_MSK)
      RCL_Handle rclHandle = RCL_open(&rclClient, &rclRadioConfigGenericMsk250k);
   #elif defined(USE_500KBPS_MSK)
      RCL_Handle rclHandle = RCL_open(&rclClient, &rclRadioConfigGenericMsk500k);
   #else
      RCL_Handle rclHandle = RCL_open(&rclClient, &rclRadioConfigGenericBle);
   #endif

      /* Setup generic transmit command */
      txCmd = RCL_CmdGenericTx_DefaultRuntime();

      /* Set RF frequency */
      txCmd.rfFrequency = FREQUENCY;
   #if !(defined(USE_250KBPS_MSK) || defined(USE_500KBPS_MSK))
      txCmd.common.phyFeatures = RCL_GENERIC_PHY_FEATURE_PHY_1MBPS;
   #endif

RF commands
===========

Different command parameters should be expected. Below is an example for CC26x2 
devices

.. code-block:: c 

   RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
   RF_cmdPropTx.pPkt = packet;
   RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW;

   // ...

   while(1)
   {
       /* Create packet with incrementing sequence number and random payload */
       packet[0] = (uint8_t)(seqNumber >> 8);
       packet[1] = (uint8_t)(seqNumber++);
       uint8_t i;
       for (i = 2; i < PAYLOAD_LENGTH; i++)
       {
           packet[i] = rand();
       }

       /* Send packet */
       RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx,
                                                   RF_PriorityNormal, NULL, 0);

Compared to |DEVICE| devices

.. code-block:: c 

      /* Start command as soon as possible */
      txCmd.common.scheduling = RCL_Schedule_Now;
      txCmd.common.status = RCL_CommandStatus_Idle;

      txCmd.config.fsOff = FS_OFF; // Turn off FS

      /* Callback triggers on last command done */
      txCmd.common.runtime.callback = defaultCallback;
      txCmd.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value;

      /* Set RCL TX buffer packet to be packet buffer */
      RCL_Buffer_TxBuffer *txPacket = (RCL_Buffer_TxBuffer *)&packet;

      while(1)
      {
         /* Create packet with random payload */
         uint8_t *txData;
         txData = RCL_TxBuffer_init(txPacket, NUM_PAD_BYTES, HDR_LEN, MAX_LENGTH);
   #if !(defined(USE_500KBPS_MSK) || defined(FIXED_LENGTH_SETUP))
   #if defined(USE_250KBPS_MSK)
         txData[0] = MAX_LENGTH;
   #else
         txData[0] = 0;
         txData[1] = MAX_LENGTH;
   #endif
   #endif
         for (int i = HDR_LEN; i < MAX_LENGTH; i++)
         {
               txData[i] = rand();
         }

         /* Set packet to transmit */
         RCL_TxBuffer_put(&txCmd.txBuffers, txPacket);

         txCmd.common.status = RCL_CommandStatus_Idle;

         /* Submit command */
         RCL_Command_submit(rclHandle, &txCmd);

         /* Pend on command completion */
         RCL_Command_pend(&txCmd);

.. note:: If changing the ``txCmd->txPower`` parameter it is important to note that 
   two additional sub-parameters, ``dbm`` and ``fraction``, will each need to be 
   initialized.  For example, 
   ``txCmd->txPower = (RCL_Command_TxPower){.dBm = txPower_dBm, .fraction = 0};``

RF API comparison
=================

Below is a table summarizing the different API functions, however it is once 
again advised that the rflib and `Radio Control Layer (RCL)`_ APIs be further 
referenced for a full understanding of differences.

+----------------------------------------+----------------+--------------------+
| **Function**                           | **rflib API**  | **RCL API**        +
+========================================+================+====================+
| Initialize the radio driver            | RF_Params_init | RCL_init           |
+----------------------------------------+----------------+--------------------+
| Open the radio instance                | RF_open        | RCL_open           |
+----------------------------------------+----------------+--------------------+
| Close the radio instance               | RF_close       | RCL_close          |
+----------------------------------------+----------------+--------------------+
| Submit a radio command                 | RF_postCmd     | RCL_Command_submit |
+----------------------------------------+----------------+--------------------+
| Wait for the radio command to complete | RF_pendCmd     | RCL_Command_pend   |
+----------------------------------------+----------------+--------------------+
| Submit a radio command and wait for it | RF_runCmd      | RCL_Command_submit |
| to complete                            |                | & RCL_Command_pend |
+----------------------------------------+----------------+--------------------+
| Stop a radio command                   | RF_cancelCmd   | RCL_Command_stop   |
+----------------------------------------+----------------+--------------------+
| Get RSSI                               | RF_getRssi     | RCL_readRssi       |
+----------------------------------------+----------------+--------------------+