Data Fields
SPILPF3DMA_HWAttrs Struct Reference

SPILPF3DMA Hardware attributes. More...

#include <SPILPF3DMA.h>

Data Fields

uint32_t baseAddr
 SPI Peripheral's base address. More...
 
uint32_t swiPriority
 SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file. More...
 
uint32_t rxChannelBitMask
 
uint32_t txChannelBitMask
 
volatile uDMAControlTableEntry * dmaTxTableEntryPri
 
volatile uDMAControlTableEntry * dmaRxTableEntryPri
 
volatile uDMAControlTableEntry * dmaTxTableEntryAlt
 
volatile uDMAControlTableEntry * dmaRxTableEntryAlt
 
int32_t pociPinMux
 
int32_t picoPinMux
 
int32_t sclkPinMux
 
int32_t csnPinMux
 
uint32_t minDmaTransferSize
 
PowerLPF3_Resource powerID
 
uint16_t defaultTxBufValue
 
uint8_t txChannelEvtMux
 
uint8_t rxChannelEvtMux
 
uint8_t intNum
 
uint8_t intPriority
 SPILPF3DMA Peripheral's interrupt priority. More...
 
uint_least8_t picoPin
 
uint_least8_t pociPin
 
uint_least8_t sclkPin
 
uint_least8_t csnPin
 
uint32_t txChannelSubscriberId
 
uint32_t rxChannelSubscriberId
 

Detailed Description

SPILPF3DMA Hardware attributes.

Many of these fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For driverlib these definitions are found in:

intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

const SPILPF3DMA_HWAttrs SPILPF3DMAobjects[CONFIG_SPI_COUNT] = {
{
.baseAddr = SPI0_BASE,
.intNum = INT_SPI0_COMB,
.intPriority = (~0),
.rxChannelBitMask = UDMA_CHANNEL_1_M,
.txChannelBitMask = UDMA_CHANNEL_0_M,
.rxChannelEvtMux = EVTSVT_DMA_TRIG_SPI0RXTRG,
.txChannelEvtMux = EVTSVT_DMA_TRIG_SPI0TXTRG,
.rxChannelSubscriberId = EVTSVT_DMA_CH1,
.txChannelSubscriberId = EVTSVT_DMA_CH0,
.dmaTxTableEntryPri = &dmaChannel0ControlTableEntry,
.dmaRxTableEntryPri = &dmaChannel1ControlTableEntry,
.dmaTxTableEntryAlt = &dmaChannel0AltControlTableEntry,
.dmaRxTableEntryAlt = &dmaChannel1AltControlTableEntry,
.picoPin = CONFIG_GPIO_SPI_CONTROLLER_PICO,
.pociPin = CONFIG_GPIO_SPI_CONTROLLER_POCI,
.sclkPin = CONFIG_GPIO_SPI_CONTROLLER_SCLK,
.csnPin = CONFIG_SPI_CSN_0,
},
};

Field Documentation

§ baseAddr

uint32_t SPILPF3DMA_HWAttrs::baseAddr

SPI Peripheral's base address.

§ swiPriority

uint32_t SPILPF3DMA_HWAttrs::swiPriority

SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file.

§ rxChannelBitMask

uint32_t SPILPF3DMA_HWAttrs::rxChannelBitMask

uDMA controlTable channel index

§ txChannelBitMask

uint32_t SPILPF3DMA_HWAttrs::txChannelBitMask

uDMA controlTable channel index

§ dmaTxTableEntryPri

volatile uDMAControlTableEntry* SPILPF3DMA_HWAttrs::dmaTxTableEntryPri

uDMA controlTable primary tx entry

§ dmaRxTableEntryPri

volatile uDMAControlTableEntry* SPILPF3DMA_HWAttrs::dmaRxTableEntryPri

uDMA controlTable primary tx entry

§ dmaTxTableEntryAlt

volatile uDMAControlTableEntry* SPILPF3DMA_HWAttrs::dmaTxTableEntryAlt

uDMA controlTable alternate tx entry

§ dmaRxTableEntryAlt

volatile uDMAControlTableEntry* SPILPF3DMA_HWAttrs::dmaRxTableEntryAlt

uDMA controlTable alternate rx entry

§ pociPinMux

int32_t SPILPF3DMA_HWAttrs::pociPinMux

POCI PIN mux value. Can be applied to either PICO or POCI

§ picoPinMux

int32_t SPILPF3DMA_HWAttrs::picoPinMux

PICO PIN mux value. Can be applied to either PICO or POCI

§ sclkPinMux

int32_t SPILPF3DMA_HWAttrs::sclkPinMux

SCLK PIN mux value for flow control

§ csnPinMux

int32_t SPILPF3DMA_HWAttrs::csnPinMux

CSN PIN mux value for flow control

§ minDmaTransferSize

uint32_t SPILPF3DMA_HWAttrs::minDmaTransferSize

Minimum transfer size for DMA based transfer

§ powerID

PowerLPF3_Resource SPILPF3DMA_HWAttrs::powerID

Power driver ID for this SPI instance

§ defaultTxBufValue

uint16_t SPILPF3DMA_HWAttrs::defaultTxBufValue

Default TX value if txBuf == NULL

§ txChannelEvtMux

uint8_t SPILPF3DMA_HWAttrs::txChannelEvtMux

DMA Mux ID for this SPI TX channel

§ rxChannelEvtMux

uint8_t SPILPF3DMA_HWAttrs::rxChannelEvtMux

DMA Mux ID for this SPI RX channel

§ intNum

uint8_t SPILPF3DMA_HWAttrs::intNum

SPILPF3DMA Peripheral's interrupt vector

§ intPriority

uint8_t SPILPF3DMA_HWAttrs::intPriority

SPILPF3DMA Peripheral's interrupt priority.

The Low Power F3 devices use either three or two priority bits, depending on the device. That means ~0 has the same effect as (7 << 5) or (3 << 6), respectively.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.

§ picoPin

uint_least8_t SPILPF3DMA_HWAttrs::picoPin

SPI PICO pin

§ pociPin

uint_least8_t SPILPF3DMA_HWAttrs::pociPin

SPI POCI pin

§ sclkPin

uint_least8_t SPILPF3DMA_HWAttrs::sclkPin

SPI SCLK pin

§ csnPin

uint_least8_t SPILPF3DMA_HWAttrs::csnPin

SPI CSN pin

§ txChannelSubscriberId

uint32_t SPILPF3DMA_HWAttrs::txChannelSubscriberId

DMA subscriber ID for this SPI TX channel, as defined in driverlib/evtsvt.h

§ rxChannelSubscriberId

uint32_t SPILPF3DMA_HWAttrs::rxChannelSubscriberId

DMA subscriber ID for this SPI RX channel, as defined in driverlib/evtsvt.h


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale