![]() |
![]() |
NVSRAM Hardware Attributes. More...
#include <NVSRAM.h>
Data Fields | |
| void * | regionBase |
| size_t | regionSize |
| size_t | sectorSize |
NVSRAM Hardware Attributes.
The 'sectorSize' is the minimal amount of data to that is cleared on an erase operation. Devices which feature internal FLASH memory usually have a 4096 byte sector size (refer to device specific documentation). It is recommended that the 'sectorSize' used match the FLASH memory sector size.
The 'regionBase' field must point to the base address of the region to be managed. It is also required that the region be aligned on a sectorSize boundary (example below to demonstrate how to do this).
The 'regionSize' must be an integer multiple of the 'sectorSize'.
Defining and reserving RAM memory regions can be done entirely within the ti_drivers_config.c file.
The example below defines a char array, 'ramBuf' and uses compiler pragmas to place 'ramBuf' at an aligned address within RAM.
| void* NVSRAM_HWAttrs::regionBase |
Base address of RAM region
| size_t NVSRAM_HWAttrs::regionSize |
The size of the region in bytes
| size_t NVSRAM_HWAttrs::sectorSize |
Sector size in bytes