Data Fields
MCAN_TxFifoQStatus Struct Reference

Structure for MCAN Tx FIFO/Queue Status. More...

#include <MCAN.h>

Data Fields

uint32_t freeLvl
 
uint32_t getIdx
 
uint32_t putIdx
 
uint32_t fifoFull
 

Detailed Description

Structure for MCAN Tx FIFO/Queue Status.

Field Documentation

§ freeLvl

uint32_t MCAN_TxFifoQStatus::freeLvl

Tx FIFO Free Level

§ getIdx

uint32_t MCAN_TxFifoQStatus::getIdx

Tx FIFO Get Index. Read as zero when Tx Queue operation is configured.

§ putIdx

uint32_t MCAN_TxFifoQStatus::putIdx

Tx FIFO/Queue Put Index

§ fifoFull

uint32_t MCAN_TxFifoQStatus::fifoFull

Tx FIFO/Queue Full
0 = Tx FIFO/Queue not full
1 = Tx FIFO/Queue full


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale