Data Fields
ComparatorLPF3LP_HWAttrs Struct Reference

ComparatorLPF3LP Hardware attributes. More...

#include <ComparatorLPF3LP.h>

Data Fields

uint32_t intNum
 
uint32_t intPriority
 
uint32_t intSubscriberId
 
ComparatorLPF3LP_PositiveInputChannel positiveInputChannel
 
ComparatorLPF3LP_NegativeInputChannel negativeInputChannel
 
ComparatorLPF3LP_VoltageDividerPath voltageDividerPath
 
ComparatorLPF3LP_VoltageDividerFactor voltageDividerFactor
 
uint8_t positiveInputPin
 
uint8_t positiveInputPinMux
 
uint8_t negativeInputPin
 
uint8_t negativeInputPinMux
 

Detailed Description

ComparatorLPF3LP Hardware attributes.

A sample structure is shown below:

Field Documentation

§ intNum

uint32_t ComparatorLPF3LP_HWAttrs::intNum

Device-specific interrupt number

§ intPriority

uint32_t ComparatorLPF3LP_HWAttrs::intPriority

Device-specific interrupt priority

§ intSubscriberId

uint32_t ComparatorLPF3LP_HWAttrs::intSubscriberId

Device-specific interrupt subscriber ID, as defined in driverlib/evtsvt.h. This must match intNum.

§ positiveInputChannel

ComparatorLPF3LP_PositiveInputChannel ComparatorLPF3LP_HWAttrs::positiveInputChannel

Internal muxing on the positive channel

§ negativeInputChannel

ComparatorLPF3LP_NegativeInputChannel ComparatorLPF3LP_HWAttrs::negativeInputChannel

Internal muxing on the negative channel

§ voltageDividerPath

ComparatorLPF3LP_VoltageDividerPath ComparatorLPF3LP_HWAttrs::voltageDividerPath

Voltage divider path

§ voltageDividerFactor

ComparatorLPF3LP_VoltageDividerFactor ComparatorLPF3LP_HWAttrs::voltageDividerFactor

Voltage divider factor

§ positiveInputPin

uint8_t ComparatorLPF3LP_HWAttrs::positiveInputPin

Positive input pin index

§ positiveInputPinMux

uint8_t ComparatorLPF3LP_HWAttrs::positiveInputPinMux

Positive input pin muxing

§ negativeInputPin

uint8_t ComparatorLPF3LP_HWAttrs::negativeInputPin

Negative input pin index

§ negativeInputPinMux

uint8_t ComparatorLPF3LP_HWAttrs::negativeInputPinMux

Negative input pin muxing


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale