Data Fields
BatteryMonitor_NotifyObj Struct Reference

Battery Monitor notify object structure. More...

#include <BatteryMonitor.h>

Collaboration diagram for BatteryMonitor_NotifyObj:
Collaboration graph
[legend]

Data Fields

List_Elem link
 
BatteryMonitor_NotifyFxn notifyFxn
 
uint16_t thresholdHigh
 
uint16_t thresholdLow
 
uintptr_t clientArg
 
bool isRegistered
 

Detailed Description

Battery Monitor notify object structure.

This structure specification is for internal use. Notification clients must pre-allocate a notify object when registering for a notification; BatteryMonitor_registerNotifyHigh(), BatteryMonitor_registerNotifyLow(), or BatteryMonitor_registerNotifyRange() will take care initializing the internal elements appropriately.

Field Documentation

§ link

List_Elem BatteryMonitor_NotifyObj::link

For placing on the notify list

§ notifyFxn

BatteryMonitor_NotifyFxn BatteryMonitor_NotifyObj::notifyFxn

Application callback function

Referenced by BatteryMonitor_getNotifyFxn().

§ thresholdHigh

uint16_t BatteryMonitor_NotifyObj::thresholdHigh

High threshold in millivolts

Referenced by BatteryMonitor_getThresholdHigh(), and BatteryMonitor_getThresholdRange().

§ thresholdLow

uint16_t BatteryMonitor_NotifyObj::thresholdLow

Low threshold in millivolts

Referenced by BatteryMonitor_getThresholdLow(), and BatteryMonitor_getThresholdRange().

§ clientArg

uintptr_t BatteryMonitor_NotifyObj::clientArg

Application provided arg

Referenced by BatteryMonitor_getClientArg().

§ isRegistered

bool BatteryMonitor_NotifyObj::isRegistered

Is the notification active


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale