Data Fields
ADCBufLPF3_Object Struct Reference

ADCBufLPF3 Object. More...

#include <ADCBufLPF3.h>

Collaboration diagram for ADCBufLPF3_Object:
Collaboration graph
[legend]

Data Fields

SemaphoreP_Struct conversionSemaphore
 
ADCBuf_ConversioncurrentConversion
 
HwiP_Struct hwi
 
ADCBuf_Callback callbackFxn
 
uint32_t * activeSampleBuffer
 
uint32_t semaphoreTimeout
 
uint32_t samplingFrequency
 
ADCBufLPF3_ConversionStatus conversionStatus
 
ADCBuf_Return_Mode returnMode
 
ADCBuf_Recurrence_Mode recurrenceMode
 
bool isOpen
 
bool userAcquiredAdcSemaphore
 

Detailed Description

ADCBufLPF3 Object.

The application must not access any member variables of this structure!

Field Documentation

§ conversionSemaphore

SemaphoreP_Struct ADCBufLPF3_Object::conversionSemaphore

Conversion semaphore. Used in blocking mode only.

§ currentConversion

ADCBuf_Conversion* ADCBufLPF3_Object::currentConversion

Pointer to the current conversion struct

§ hwi

HwiP_Struct ADCBufLPF3_Object::hwi

Hwi object

§ callbackFxn

ADCBuf_Callback ADCBufLPF3_Object::callbackFxn

Pointer to callback function

§ activeSampleBuffer

uint32_t* ADCBufLPF3_Object::activeSampleBuffer

The last complete sample buffer used by the DMA

§ semaphoreTimeout

uint32_t ADCBufLPF3_Object::semaphoreTimeout

Timeout for read semaphore in ADCBuf_RETURN_MODE_BLOCKING

§ samplingFrequency

uint32_t ADCBufLPF3_Object::samplingFrequency

Frequency in Hz at which the ADC is triggered

§ conversionStatus

ADCBufLPF3_ConversionStatus ADCBufLPF3_Object::conversionStatus

Is the ADC currently doing conversions

§ returnMode

ADCBuf_Return_Mode ADCBufLPF3_Object::returnMode

Mode for all conversions

§ recurrenceMode

ADCBuf_Recurrence_Mode ADCBufLPF3_Object::recurrenceMode

Should we convert continuously or one-shot

§ isOpen

bool ADCBufLPF3_Object::isOpen

Has the object been opened

§ userAcquiredAdcSemaphore

bool ADCBufLPF3_Object::userAcquiredAdcSemaphore

Did the user manually acquire the ADC semaphore?


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale