![]() |
![]() |
| C_NoRTOS_Config | NoRTOS framework global configuration |
| C_QueueP_Elem | |
| C_QueueP_Obj | |
| CADC_Config_ | ADC driver's custom configuration structure |
| CADC_FxnTable | The definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation |
| CADC_Params | ADC Parameters used with ADC_open() |
| CADCBuf_Config_ | ADC driver's custom configuration structure |
| CADCBuf_Conversion | Defines a conversion to be used with ADCBuf_convert() |
| CADCBuf_FxnTable | The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation |
| CADCBuf_Params | ADCBuf parameters used with ADCBuf_open() |
| CADCBufLPF3_AdcChannelLutEntry | Table entry that maps a virtual adc channel to the corresponding hardware configuration |
| CADCBufLPF3_HWAttrs | ADCBufLPF3 Hardware Attributes |
| CADCBufLPF3_Object | ADCBufLPF3 Object |
| CADCLPF3_HWAttrs | ADCLPF3 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions |
| CADCLPF3_Object | ADCLPF3 Object |
| CAPULPF3_ComplexMatrix | APULPF3 Matrix Struct |
| CAPULPF3_ComplexTriangleMatrix | APULPF3 Upper Triangle Matrix Struct |
| CAPULPF3_ComplexVector | APULPF3 Vector Struct |
| CAPULPF3_Config | APULPF3 Global configuration |
| CAPULPF3_HWAttrs | APULPF3 Hardware attributes |
| CBatMonSupportLPF3_Config | BatMon Support Configuration |
| CBatteryMonitor_NotifyObj | Battery Monitor notify object structure |
| CButton_Config | Button configuration |
| CButton_HWAttrs | Hardware specific settings for a button |
| CButton_Object | Internal to Button module. Members should not be accessed by the application |
| CButton_Params | Button Parameters |
| CCAN_BitRateTimingRaw | Structure defining the raw MCAN bit rate configuration |
| CCAN_Config_ | CAN Global configuration |
| CCAN_DataBitRateTimingRaw | Structure defining the raw MCAN CAN FD data phase bit rate configuration |
| CCAN_HWAttrs | CAN hardware attributes |
| CCAN_MsgRamConfig | CAN Message RAM configuration |
| CCAN_Object | CAN Object |
| CCAN_Params | CAN Parameters |
| CCANCC27XXX10_Config | CANCC27XXX10 global configuration |
| CClockP_FreqHz | Frequency-in-hertz struct |
| CClockP_Params | Basic ClockP Parameters |
| CClockP_Struct | ClockP structure |
| CComparator_Config | Comparator driver's custom configuration structure |
| CComparator_FxnTable | The definition of a comparator function table that contains the required set of functions to control a specific comparator driver implementation |
| CComparator_Params | Comparator parameters |
| CComparatorLPF3LP_HWAttrs | ComparatorLPF3LP Hardware attributes |
| CComparatorLPF3LP_Object | ComparatorLPF3LP Object |
| CDisplay_Config | Display Global configuration |
| CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
| CDisplay_Params | Display Parameters |
| CDisplayHost_HWAttrs | DisplayHost Attributes |
| CDisplayHost_Object | DisplayHost Object |
| CDisplayUart2_HWAttrs | DisplayUart2 Attributes |
| CDisplayUart2_Object | DisplayUart2 Object |
| CEventP_Struct | EventP structure |
| CGPIO_Config | GPIO driver configuration structure |
| CHwiP_Params | Basic HwiP Parameters |
| CHwiP_Struct | HwiP structure |
| CI2C_Config_ | I2C driver's custom configuration structure |
| CI2C_Params | I2C parameters used with I2C_open() |
| CI2C_Transaction | Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout() |
| CI2CLPF3_HWAttrs | I2CLPF3 Hardware attributes |
| CI2CLPF3_I2CPinCfg | I2CLPF3 Pin Configuration |
| CI2CLPF3_Object | I2CLPF3 Object |
| CI2CTarget_Config_ | I2CTarget Global configuration |
| CI2CTarget_Params | I2CTarget Parameters |
| CI2CTargetLPF3_HWAttrs | I2CTargetLPF3 Hardware attributes |
| CI2CTargetLPF3_Object | I2CTargetLPF3 Object |
| CI2S_Config | I2S Global configuration |
| CI2S_Params | Basic I2S Parameters |
| CI2S_Transaction | I2S transaction descriptor |
| CI2SLPF3_HWAttrs | I2S Hardware attributes |
| CITM_HWAttrs | ITM Hardware Attributes |
| CITMLPF3_HWAttrs | |
| CLED_Config | LED configuration |
| CLED_HWAttrs | Hardware specific settings for a LED module |
| CLED_Object | LED Object structure |
| CLED_Params | LED Parameters |
| CLGPTimerLPF3_ChannelConf | LGPTimerLPF3 channel dependent pin configuration struct |
| CLGPTimerLPF3_ChannelProp | LGPTimerLPF3 channel dependent properties struct |
| CLGPTimerLPF3_Config | LGPTimer Global configuration |
| CLGPTimerLPF3_HWAttrs | LGPTimerLPF3 Hardware attributes |
| CLGPTimerLPF3_Object | LGPTimerLPF3 Object |
| CLGPTimerLPF3_Params | LGPTimerLPF3 Parameters |
| CList_Elem_ | |
| CList_List | |
| CLogSinkBuf_Instance | |
| CLogSinkBuf_Rec | |
| CLogSinkITM_Instance | |
| CLogSinkTraceLPF3_Config | LogSinkTraceLPF3 global configuration |
| CLogSinkUART_Config | LogSinkUART Global configuration |
| CLogSinkUART_HWAttrs | LogSinkUART Hardware attributes |
| CLogSinkUART_Instance | LogSinkUART Sink parameters |
| CLogSinkUART_Object | LogSinkUART Object |
| CMCAN_BitTimingParams | Structure for bit timing parameters |
| CMCAN_ConfigParams | Structure for MCAN configuration parameters |
| CMCAN_ErrCntStatus | Structure for MCAN error logging counters status |
| CMCAN_ExtMsgIDFilterElement | Structure for MCAN Extended Message ID Filter Element |
| CMCAN_GlobalFiltConfig | Structure for MCAN Global Filter Configuration parameters |
| CMCAN_HighPriorityMsgInfo | Structure for MCAN High Priority Message |
| CMCAN_InitParams | Structure for MCAN initialization parameters |
| CMCAN_MsgRamConfig | Structure for MCAN Message RAM Configuration Parameters |
| CMCAN_ProtocolStatus | Structure for MCAN protocol status |
| CMCAN_RxBufElement | Structure for MCAN Rx Buffer element |
| CMCAN_RxBufElementNoCpy | Structure for MCAN Rx Buffer element which takes data as a pointer. Please note that as the data field is a pointer so wrong value for payload size passed from application will lead to data corruption |
| CMCAN_RxFifoStatus | Structure for MCAN Rx FIFO Status |
| CMCAN_RxNewDataStatus | Structure for MCAN new data flag for Rx buffer |
| CMCAN_StdMsgIDFilterElement | Structure for MCAN Standard Message ID Filter Element |
| CMCAN_TDCConfig | Structure for MCAN Transmitter Delay Compensation parameters |
| CMCAN_TxBufElement | Structure for MCAN Tx Buffer element |
| CMCAN_TxBufElementNoCpy | Structure for MCAN Tx Buffer element which takes data as a pointer |
| CMCAN_TxEventFifoElement | Structure for MCAN Tx Event FIFO element |
| CMCAN_TxEventFifoStatus | Structure for MCAN Tx Event FIFO Status |
| CMCAN_TxFifoQStatus | Structure for MCAN Tx FIFO/Queue Status |
| CMessageQueueP_Struct | MessageQueueP structure |
| CMutexP_Params | Basic MutexP Parameters |
| CMutexP_Struct | MutexP structure |
| CNVS_Attrs | NVS attributes |
| CNVS_Config_ | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CNVSLPF3_HWAttrs | NVSLPF3 hardware attributes |
| CNVSLPF3_Object | |
| CNVSRAM_HWAttrs | NVSRAM Hardware Attributes |
| CNVSRAM_Object | |
| CNVSSPI25X_HWAttrs | NVSSPI25X attributes |
| CNVSSPI25X_Object | |
| CPower_NotifyObj | Power notify object structure |
| CPowerCC23X0_Config | Global configuration structure |
| CPowerCC27XX_Config | Global configuration structure |
| CPowerLPF3_LfoscCompensationProfile | LFOSC Compensation Profile structure |
| CPWM_Config_ | PWM Global configuration |
| CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params | PWM Parameters |
| CPWMTimerLPF3_HwAttrs | PWMTimerLPF3 Hardware attributes |
| CPWMTimerLPF3_Object | PWMTimerLPF3 Object |
| CRingBuf_Object | |
| CSD_Config_ | SD Global configuration |
| CSD_FxnTable | The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation |
| CSD_Params | SD Parameters |
| CSDFatFS_Config | SDFatFS Global configuration |
| CSDFatFS_Object | SDFatFS Object The application must not access any member variables of this structure! |
| CSDSPI_HWAttrs | SDSPI Hardware attributes |
| CSDSPI_Object | SDSPI Object |
| CSecureCallback_Config | |
| CSecureCallback_Object | |
| CSemaphoreP_Params | Basic SemaphoreP Parameters |
| CSemaphoreP_Struct | SemaphoreP structure |
| CSPI_Config_ | SPI Global configuration |
| CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params | SPI Parameters |
| CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| Cspiffs_config | |
| Cspiffs_DIR | |
| Cspiffs_dirent | |
| Cspiffs_stat | |
| Cspiffs_t | |
| CSPIFFSNVS_Data_ | SPIFFSNVS data object |
| CSPIFFSNVS_Lock_ | SPIFFSNVS Lock |
| CSPILPF3DMA_HWAttrs | SPILPF3DMA Hardware attributes |
| CSPILPF3DMA_Object | SPILPF3DMA Object |
| CStructRingBuf_Object | |
| CSwiP_Params | Basic SwiP Parameters |
| CSwiP_Struct | SemaphoreP structure |
| CTaskP_Params | |
| CTaskP_Struct | TaskP structure |
| CTCAN455X_Config | TCAN455X global configuration |
| CTemperature_NotifyObj | Temperature notify object structure |
| CTemperatureLPF3_Config | Temperature driver configuration struct for Low Power F3 devices |
| CTimestampP_Format | |
| CUART2_Config_ | UART2 Global configuration |
| CUART2_Params | UART2 Parameters |
| CUART2LPF3_HWAttrs | UART2LPF3 Hardware attributes |
| CUART2LPF3_Object | UART2LPF3 Object |
| CUDMALPF3_Config | UDMALPF3 Global configuration |
| CWatchdog_Config_ | Watchdog Global configuration |
| CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params | Watchdog Parameters |
| CWatchdogLPF3_HWAttrs | Watchdog hardware attributes for CC23X0 |
| CWatchdogLPF3_Object | Watchdog Object for CC23X0 |