91 #ifndef ti_drivers_batterymonitor_BatMonSupportLPF3__include 92 #define ti_drivers_batterymonitor_BatMonSupportLPF3__include uint32_t intPriority
Definition: BatMonSupportLPF3.h:124
void BatMonSupportLPF3_registerTemperatureCb(uint32_t eventMask, BatMonSupportLPF3_EventCb callback)
This function registers a callback dedicated for the Temperature driver.
void BatMonSupportLPF3_init(void)
This function initializes the BatMon Support layer.
BatMon Support Configuration.
Definition: BatMonSupportLPF3.h:116
void(* BatMonSupportLPF3_EventCb)(uint32_t eventFlags)
Function prototype for an event callback.
Definition: BatMonSupportLPF3.h:144
uint32_t intSubscriberId
Definition: BatMonSupportLPF3.h:129
uint32_t intNum
Definition: BatMonSupportLPF3.h:121
void BatMonSupportLPF3_registerBatteryCb(uint32_t eventMask, BatMonSupportLPF3_EventCb callback)
This function registers a callback dedicated for the Battery Monitor driver.
Linked List interface for use in drivers.