Instance: VIMS
Component: VIMS
Base address: 0x40024000
Versatile Instruction Memory System
Controls memory access to the Flash and encapsulates the following instruction memories:
- Boot ROM
- Caches
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RO |
32 |
0xD140 0010 |
0x0000 0000 |
0x4002 4000 |
|
|
RO |
32 |
0x11FF 801F |
0x0000 0004 |
0x4002 4004 |
|
|
RW |
32 |
0x0000 000F |
0x0000 0008 |
0x4002 4008 |
|
|
RW |
32 |
0x0000 000F |
0x0000 000C |
0x4002 400C |
|
|
RW |
32 |
0x131A 0000 |
0x0000 0018 |
0x4002 4018 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x4002 401C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x4002 4020 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4002 4024 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x4002 4028 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0100 |
0x4002 4100 |
|
|
RW |
32 |
0x0000 0309 |
0x0000 03FC |
0x4002 43FC |
|
|
RW |
32 |
0x0000 000F |
0x0000 0400 |
0x4002 4400 |
|
|
RW |
32 |
0x0000 00BF |
0x0000 0404 |
0x4002 4404 |
|
|
RW |
32 |
0x0000 00BF |
0x0000 0408 |
0x4002 4408 |
|
|
RW |
32 |
0x0000 0001 |
0x0000 040C |
0x4002 440C |
|
|
RW |
32 |
0xFFFF FFFF |
0x0000 0410 |
0x4002 4410 |
|
|
RW |
32 |
0xFFFF FFFF |
0x0000 0414 |
0x4002 4414 |
|
|
RW |
32 |
0xFFFF FFFF |
0x0000 0418 |
0x4002 4418 |
|
|
RW |
32 |
0x0000 001F |
0x0000 041C |
0x4002 441C |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0420 |
0x4002 4420 |
|
|
RW |
32 |
0x0000 0091 |
0x0000 0424 |
0x4002 4424 |
|
|
RO |
32 |
0x0000 0003 |
0x0000 0428 |
0x4002 4428 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0430 |
0x4002 4430 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0434 |
0x4002 4434 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 04FC |
0x4002 44FC |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0x4002 4000 | Instance | 0x4002 4000 |
| Description | Description Register. This register provides IP module ID, revision information, instance index and standard MMR registers offset. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | MODID | Module identification contains a unique peripheral identification number. | RO | 0xD140 | ||
| 15:12 | STDIPOFF | Standard IP MMR block offset. Standard IP MMRs are the set of from aggregated IRQ registers till DTB. 0: Standard IP MMRs do not exist 0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address) |
RO | 0x0 | ||
| 11:8 | INSTIDX | IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number (0-15). | RO | 0x0 | ||
| 7:4 | MAJREV | Major revision of IP | RO | 0x1 | ||
| 3:0 | MINREV | Minor revision of IP | RO | 0x0 | ||
| Address Offset | 0x0000 0004 | ||
| Physical Address | 0x4002 4004 | Instance | 0x4002 4004 |
| Description | Extended Description Register.This register describes the configuration of VIMS. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | ||
| 28:27 | NBANK | Number of Flash banks | RO | 0b10 | ||
| 26:15 | FLSZ | FLASH size in Kilo Bytes. The total FLASH size is (FLSZ + 1) KB | RO | 0x3FF | ||
| 14:0 | ROMSZ | ROM size in Kilo Bytes. The total ROM size is (ROMSZ + 1) KB | RO | 0b000 0000 0001 1111 | ||
| Address Offset | 0x0000 0008 | ||
| Physical Address | 0x4002 4008 | Instance | 0x4002 4008 |
| Description | Flash Wait State 1T. This register is used to specify the number of waitstates necessary for accessing the flash in 1T mode. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||||||||||||||||||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||||||||||||||||||||||||||||||||||||||||||||
| 3:0 | VAL | Flash read wait states for 1T accesses
|
RW | 0xF | |||||||||||||||||||||||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 000C | ||
| Physical Address | 0x4002 400C | Instance | 0x4002 400C |
| Description | Flash Wait State 1T. This register is used to specify the number of waitstates necessary for accessing the flash in 2T mode. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||||||||||||||||||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||||||||||||||||||||||||||||||||||||||||||||
| 3:0 | VAL | Flash read wait states for 2T accesses
|
RW | 0xF | |||||||||||||||||||||||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 0018 | ||
| Physical Address | 0x4002 4018 | Instance | 0x4002 4018 |
| Description | FLASH Pump trim Bank 0. This register stores different PUMP trims. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Flash charge pump trim value. | RW | 0x131A 0000 | ||
| Address Offset | 0x0000 001C | ||
| Physical Address | 0x4002 401C | Instance | 0x4002 401C |
| Description | FLASH Bank 0 Trim [59:32]. This register stores different bank trims. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | RESERVED28 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | ||
| 27:0 | VAL | Flash bank trim value. | RW | 0x000 0000 | ||
| Address Offset | 0x0000 0020 | ||
| Physical Address | 0x4002 4020 | Instance | 0x4002 4020 |
| Description | FLASH Bank 0 Trim [31:0]. This register stores different bank trims. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Flash bank trim value. | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0024 | ||
| Physical Address | 0x4002 4024 | Instance | 0x4002 4024 |
| Description | FLASH Bank 1 Trim [59:32]. This register stores different bank trims. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | RESERVED28 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | ||
| 27:0 | VAL | Flash bank trim value. | RW | 0x000 0000 | ||
| Address Offset | 0x0000 0028 | ||
| Physical Address | 0x4002 4028 | Instance | 0x4002 4028 |
| Description | FLASH Bank 1 Trim [31:0]. This register stores different bank trims. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Flash bank trim value. | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0100 | ||
| Physical Address | 0x4002 4100 | Instance | 0x4002 4100 |
| Description | Flash Block. This register is used to block user read, write and erase operation to flash. This register is sticky 1 and writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 0 | ACCESS | Flash Access
|
RW | 0 | |||||||||||
| Address Offset | 0x0000 03FC | ||
| Physical Address | 0x4002 43FC | Instance | 0x4002 43FC |
| Description | Configuration Register. This register is used for VIMS configuration. This register is writable only when CFG.LOCK is 1 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
| 31:11 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 0000 | |||||||||||||||||||||||||||||
| 10:8 | HSMSZ | HSM Size. Number of 32KB blocks allocated to HSM
|
RW | 0b011 | |||||||||||||||||||||||||||||
| 7:5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | |||||||||||||||||||||||||||||
| 4 | SPLMODE | Split Mode. The logical address space is split into two equal regions
|
RW | 0 | |||||||||||||||||||||||||||||
| 3 | RDPRROM | ROM Read Protection Disable
|
RW | 1 | |||||||||||||||||||||||||||||
| 2 | ATTEST | This bit is used to enable flash test mode.
|
RW | 0 | |||||||||||||||||||||||||||||
| 1 | TRMVLID | TRIM Valid. This bit indicates if flash charge pump and bank trim values are as applicable.
|
RW | 0 | |||||||||||||||||||||||||||||
| 0 | LOCK | Lock. Lock VIMS configuration. This bit is sticky '0' and when 0 write protects following registers FLWS1T FLWS2T PTRMC0 B0TRMC1 B0TRMC0 B1TRMC1 B1TRMC0 FLBLCK CFG
|
RW | 1 | |||||||||||||||||||||||||||||
| Address Offset | 0x0000 0400 | ||
| Physical Address | 0x4002 4400 | Instance | 0x4002 4400 |
| Description | Read Protect Main. First 16KB of flash main region can be protected with granularity of 2KB. This register is sticky 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||||||||||||||||||||||||||||||||
| 3:0 | VAL | Protection configuration value. Undefined values will read protect whole protectable region
|
RW | 0xF | ||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 0404 | ||
| Physical Address | 0x4002 4404 | Instance | 0x4002 4404 |
| Description | Read Protect Non-Main regions. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
| 7 | VLOG | VLOG read protection configuration. This field is sticky 0 | RW | 1 | ||
| 6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||
| 5:0 | CCFG | CCFG read protection configuration. Last 512 bytes of CCFG can be protected with granularity of 16Bytes. This field is sticky 0 | RW | 0b11 1111 | ||
| Address Offset | 0x0000 0408 | ||
| Physical Address | 0x4002 4408 | Instance | 0x4002 4408 |
| Description | Read Protect Trim |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
| 7 | SCFG | SCFG read protection configuration. This field is sticky 0 | RW | 1 | ||
| 6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||
| 5:0 | FCFG | FCFG read protection configuration. Last 512 bytes of CCFG can be protected with granularity of 16Bytes. This register is sticky 0 | RW | 0b11 1111 | ||
| Address Offset | 0x0000 040C | ||
| Physical Address | 0x4002 440C | Instance | 0x4002 440C |
| Description | Read Protect ENGR. This register is sticky 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
| 0 | ENGR | ENGR read protection configuration. | RW | 1 | ||
| Address Offset | 0x0000 0410 | ||
| Physical Address | 0x4002 4410 | Instance | 0x4002 4410 |
| Description | Write Erase Protect Main A. This register allows the first 32 sectors of the logical bank 0 main region to be protected from program or erase, with 1 bit protecting each sector (sector 0 to sector 31). This register is sticky 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Flash write/erase protection configuration value. | RW | 0xFFFF FFFF | ||
| Address Offset | 0x0000 0414 | ||
| Physical Address | 0x4002 4414 | Instance | 0x4002 4414 |
| Description | Write Erase Protect Main Bank 0. This register allows physical bank 0 main region sectors to be protected from program and erase. Each bit corresponds to a group of 8 sectors. First 4-bit are reserved if physical Bank 0 is logical bank 0 CTL.SWAP = 0. This register is sticky 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Flash write/erase protection configuration value. | RW | 0xFFFF FFFF | ||
| Address Offset | 0x0000 0418 | ||
| Physical Address | 0x4002 4418 | Instance | 0x4002 4418 |
| Description | Write Erase Protect Main Bank 1. This register allows physical bank 1 main region sectors to be protected from program and erase. Each bit corresponds to a group of 8 sectors. First 4-bit are reserved if physical Bank 1 is logical bank 0 CTL.SWAP = 1. This register is sticky 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Flash write/erase protection configuration value. | RW | 0xFFFF FFFF | ||
| Address Offset | 0x0000 041C | ||
| Physical Address | 0x4002 441C | Instance | 0x4002 441C |
| Description | Write Erase Protect Auxillary. Flash Write/Erase protection for Non-Main, TRIM and ENGR Regions. This register is sticky 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 | ||
| 4 | VLOG | Write/Erase Protection for VLOG | RW | 1 | ||
| 3 | SCFG | Write/Erase Protection for SCFG | RW | 1 | ||
| 2 | ENGR | Write/Erase Protection for ENGR | RW | 1 | ||
| 1 | FCFG | Write/Erase Protection for FCFG | RW | 1 | ||
| 0 | CCFG | Write/Erase Protection for CCFG | RW | 1 | ||
| Address Offset | 0x0000 0420 | ||
| Physical Address | 0x4002 4420 | Instance | 0x4002 4420 |
| Description | Flash Status. This register is used to indicate status of flash. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 | |||||||||||
| 5 | B1BSY | Bank 1 Busy. This bit indicates if flash Bank 1 is busy.
|
RO | 0 | |||||||||||
| 4 | B0BSY | Bank 0 Busy. This bit indicates if flash Bank 0 is busy.
|
RO | 0 | |||||||||||
| 3 | PARERR | Parity Error. This bit indicates parity error on write/erase & read protection MMRs. This bit is sticky when set to 1 by hardware.
|
RO | 0 | |||||||||||
| 2 | BUSY | This bit indicates if flash is busy.
|
RO | 0 | |||||||||||
| 1 | FL2TRDY | Flash 2T Ready. This bit indicates if flash is ready in 2T mode.
|
RO | 0 | |||||||||||
| 0 | FL1TRDY | Flash 1T Ready. This bit indicates if flash is ready in 1T mode.
|
RO | 0 | |||||||||||
| Address Offset | 0x0000 0424 | ||
| Physical Address | 0x4002 4424 | Instance | 0x4002 4424 |
| Description | Cache Control Register. This register is used for cache control on code bus Interface. This register can only be written when CCHSTA.BUSY is 0 |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | |||||||||||
| 16 | HCHFLUSH | Cache Flush for HSM Cache. This bit is used to flush the cache on HSM bus Interface. This bit is self clearing
|
WO | 0 | |||||||||||
| 15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | |||||||||||
| 8 | CNTCLR | Cache Hit/Miss Count Clear. Writing 0 to this bit has no affect
|
WO | 0 | |||||||||||
| 7 | CNTEN | Cache Hit/Miss Count Enable.
|
RW | 1 | |||||||||||
| 6 | RPOLICY | Replacement policy for Cache.
|
RW | 0 | |||||||||||
| 5 | LINFLUSH | Line Buffer Flush. This bit is used to flush the Line buffer on system bus Interface. This bit is self clearing. Writing 0 to this bit has no affect
|
WO | 0 | |||||||||||
| 4 | LINEN | Line Buffer Enable. This bit is used to enable the Line buffer on system bus Interface. Disabling the Line buffer will flush it
|
RW | 1 | |||||||||||
| 3 | CCHFLUSH | Cache Flush. This bit is used to flush the cache on code bus Interface. This bit is self clearing. Writing 0 to this bit has no affect
|
WO | 0 | |||||||||||
| 2:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | |||||||||||
| 0 | CCHEN | Cache Enable. This bit is used to enable the cache. Disabling the cache will flush it
|
RW | 1 | |||||||||||
| Address Offset | 0x0000 0428 | ||
| Physical Address | 0x4002 4428 | Instance | 0x4002 4428 |
| Description | Cache Status. This register gives cache status |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 1 | BUSY | Busy. This bit indicate Cache is changing state
|
RO | 1 | |||||||||||
| 0 | EN | Enabled. This bit indicate whether cache is enabled or disabled
|
RO | 1 | |||||||||||
| Address Offset | 0x0000 0430 | ||
| Physical Address | 0x4002 4430 | Instance | 0x4002 4430 |
| Description | Cache Hit Counter |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Hit Counter Value. This counter is cleared by writing CCHCTL.CNTCLR | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0434 | ||
| Physical Address | 0x4002 4434 | Instance | 0x4002 4434 |
| Description | Cache Miss Counter |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Miss Counter Value. This counter is cleared by writing CCHCTL.CNTCLR | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 04FC | ||
| Physical Address | 0x4002 44FC | Instance | 0x4002 44FC |
| Description | Control Register. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31 | SWAPLOCK | Swap Lock. If set, CTL.SWAP bit is blocked for writing. This bit is sticky 1
|
RW | 0 | |||||||||||
| 30:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 0 | SWAP | Swaps the logical to physical bank mapping. This bit has no effect if CTL.SPLMODE is 0 and is writable ony when CTL.SWAPLOCK is 0
|
RW | 0 | |||||||||||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |