Instance: TPIU
Component: TPIU
Base address: 0xE0040000
Cortex-M's Trace Port Interface Unit (TPIU)
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RO |
32 |
0x0000 000B |
0x0000 0000 |
0xE004 0000 |
|
|
RW |
32 |
0x0000 0001 |
0x0000 0004 |
0xE004 0004 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0xE004 0010 |
|
|
RW |
32 |
0x0000 0001 |
0x0000 00F0 |
0xE004 00F0 |
|
|
RO |
32 |
0x0000 0008 |
0x0000 0300 |
0xE004 0300 |
|
|
RW |
32 |
0x0000 0102 |
0x0000 0304 |
0xE004 0304 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0308 |
0xE004 0308 |
|
|
RO |
32 |
0x0000 000F |
0x0000 0FA0 |
0xE004 0FA0 |
|
|
WO |
32 |
0x0000 000F |
0x0000 0FA0 |
0xE004 0FA0 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0FA4 |
0xE004 0FA4 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0FA4 |
0xE004 0FA4 |
|
|
RO |
32 |
0x0000 0CA0 |
0x0000 0FC8 |
0xE004 0FC8 |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0xE004 0000 | Instance | 0xE004 0000 |
| Description | Supported Sync Port Sizes This register represents a single port size that is supported on the device, that is, 4, 2 or 1. This is to ensure that tools do not attempt to select a port width that an attached TPA cannot capture. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
| 3 | FOUR | 4-bit port size support 0x0: Not supported 0x1: Supported |
RO | 1 | ||
| 2 | THREE | 3-bit port size support 0x0: Not supported 0x1: Supported |
RO | 0 | ||
| 1 | TWO | 2-bit port size support 0x0: Not supported 0x1: Supported |
RO | 1 | ||
| 0 | ONE | 1-bit port size support 0x0: Not supported 0x1: Supported |
RO | 1 | ||
| Address Offset | 0x0000 0004 | ||
| Physical Address | 0xE004 0004 | Instance | 0xE004 0004 |
| Description | Current Sync Port Size This register has the same format as SSPSR but only one bit can be set, and all others must be zero. Writing values with more than one bit set, or setting a bit that is not indicated as supported can cause Unpredictable behavior. On reset this defaults to the smallest possible port size, 1 bit. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x000 0000 | ||
| 3 | FOUR | 4-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
RW | 0 | ||
| 2 | THREE | 3-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
RW | 0 | ||
| 1 | TWO | 2-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
RW | 0 | ||
| 0 | ONE | 1-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
RW | 1 | ||
| Address Offset | 0x0000 0010 | ||
| Physical Address | 0xE004 0010 | Instance | 0xE004 0010 |
| Description | Async Clock Prescaler This register scales the baud rate of the asynchronous output. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:13 | RESERVED13 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 0000 | ||
| 12:0 | PRESCALER | Divisor for input trace clock is (PRESCALER + 1). | RW | 0b0 0000 0000 0000 | ||
| Address Offset | 0x0000 00F0 | ||
| Physical Address | 0xE004 00F0 | Instance | 0xE004 00F0 |
| Description | Selected Pin Protocol This register selects the protocol to be used for trace output. Note: If this register is changed while trace data is being output, data corruption occurs. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||
| 31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 0000 0000 0000 | ||||||||||||||
| 1:0 | PROTOCOL | Trace output protocol
|
RW | 0b01 | ||||||||||||||
| Address Offset | 0x0000 0300 | ||
| Physical Address | 0xE004 0300 | Instance | 0xE004 0300 |
| Description | Formatter and Flush Status | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
| 3 | FTNONSTOP | 0: Formatter can be stopped 1: Formatter cannot be stopped |
RO | 1 | ||
| 2:0 | RESERVED0 | This field always reads as zero | RO | 0b000 | ||
| Address Offset | 0x0000 0304 | ||
| Physical Address | 0xE004 0304 | Instance | 0xE004 0304 |
| Description | Formatter and Flush Control When one of the two single wire output (SWO) modes is selected, ENFCONT enables the formatter to be bypassed. If the formatter is bypassed, only the ITM/DWT trace source (ATDATA2) passes through. The TPIU accepts and discards data that is presented on the ETM port (ATDATA1). This function is intended to be used when it is necessary to connect a device containing an ETM to a trace capture device that is only able to capture Serial Wire Output (SWO) data. Enabling or disabling the formatter causes momentary data corruption. Note: If the selected pin protocol register (SPPR.PROTOCOL) is set to 0x00 (TracePort mode), this register always reads 0x102, because the formatter is automatically enabled. If one of the serial wire modes is then selected, the register reverts to its previously programmed value. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 0000 0000 | ||
| 8 | TRIGIN | Indicates that triggers are inserted when a trigger pin is asserted. | RW | 1 | ||
| 7:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 | ||
| 1 | ENFCONT | Enable continuous formatting: 0: Continuous formatting disabled 1: Continuous formatting enabled |
RW | 1 | ||
| 0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
| Address Offset | 0x0000 0308 | ||
| Physical Address | 0xE004 0308 | Instance | 0xE004 0308 |
| Description | Periodic Synchronization Control Registers | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
| 4:0 | PSCOUNT | Periodic Synchronization Count. Determines the reload value of the Periodic Synchronization Counter. The reload value takes effect the next time the counter reaches zero. Reads from this register return the reload value programmed into this register 0b00000 Synchronization disabled. 0b00111 128 bytes 0b01000 256 bytes 0b11111 2^31 bytes |
RW | 0x00 | ||
| Address Offset | 0x0000 0FA0 | ||
| Physical Address | 0xE004 0FA0 | Instance | 0xE004 0FA0 |
| Description | Claim Tag Mask | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CLAIMMASK | This register forms one half of the Claim Tag value. When reading this register returns the number of bits that can be set (each bit is considered separately): 0: This claim tag bit is not implemented 1: This claim tag bit is not implemented The behavior when writing to this register is described in CLAIMSET. |
RO | 0x0000 000F | ||
| Address Offset | 0x0000 0FA0 | ||
| Physical Address | 0xE004 0FA0 | Instance | 0xE004 0FA0 |
| Description | Claim Tag Set | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CLAIMSET | This register forms one half of the Claim Tag value. Writing to this location allows individual bits to be set (each bit is considered separately): 0: No effect 1: Set this bit in the claim tag The behavior when reading from this location is described in CLAIMMASK. |
WO | 0x0000 000F | ||
| Address Offset | 0x0000 0FA4 | ||
| Physical Address | 0xE004 0FA4 | Instance | 0xE004 0FA4 |
| Description | Current Claim Tag | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CLAIMTAG | This register forms one half of the Claim Tag value. Reading this register returns the current Claim Tag value. Reading CLAIMMASK determines how many bits from this register must be used. The behavior when writing to this register is described in CLAIMCLR. |
RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0FA4 | ||
| Physical Address | 0xE004 0FA4 | Instance | 0xE004 0FA4 |
| Description | Claim Tag Clear | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CLAIMCLR | This register forms one half of the Claim Tag value. Writing to this location enables individual bits to be cleared (each bit is considered separately): 0: No effect 1: Clear this bit in the claim tag. The behavior when reading from this location is described in CLAIMTAG. |
WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0FC8 | ||
| Physical Address | 0xE004 0FC8 | Instance | 0xE004 0FC8 |
| Description | Device ID | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | DEVID | This field returns: 0xCA1 if there is an ETM present. 0xCA0 if there is no ETM present. | RO | 0x0000 0CA0 | ||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |