DMA

Instance: DMA
Component: DMA
Base address: 0x400C4000


ARM Micro Direct Memory Access Controller

TOP:DMA Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

STATUS

RO

32

0x000B 0000

0x0000 0000

0x400C 4000

CFG

WO

32

0x0000 0000

0x0000 0004

0x400C 4004

CTRL

RW

32

0x0000 0000

0x0000 0008

0x400C 4008

ALTCTRL

RO

32

0x0000 0100

0x0000 000C

0x400C 400C

WAITONREQ

RO

32

0x0000 0FFF

0x0000 0010

0x400C 4010

SOFTREQ

WO

32

0x0000 0000

0x0000 0014

0x400C 4014

SETBURST

RW

32

0x0000 0000

0x0000 0018

0x400C 4018

CLEARBURST

WO

32

0x0000 0000

0x0000 001C

0x400C 401C

SETREQMASK

RW

32

0x0000 0000

0x0000 0020

0x400C 4020

CLEARREQMASK

WO

32

0x0000 0000

0x0000 0024

0x400C 4024

SETCHANNELEN

RW

32

0x0000 0000

0x0000 0028

0x400C 4028

CLEARCHANNELEN

WO

32

0x0000 0000

0x0000 002C

0x400C 402C

SETCHNLPRIALT

RW

32

0x0000 0000

0x0000 0030

0x400C 4030

CLEARCHNLPRIALT

WO

32

0x0000 0000

0x0000 0034

0x400C 4034

SETCHNLPRIORITY

RW

32

0x0000 0000

0x0000 0038

0x400C 4038

CLEARCHNLPRIORITY

WO

32

0x0000 0000

0x0000 003C

0x400C 403C

ERROR

RW

32

0x0000 0000

0x0000 004C

0x400C 404C

REQDONE

RW

32

0x0000 0000

0x0000 0504

0x400C 4504

DONEMASK

RW

32

0x0000 0000

0x0000 0520

0x400C 4520

TOP:DMA Register Descriptions

TOP:DMA:STATUS

Address Offset 0x0000 0000
Physical Address 0x400C 4000 Instance 0x400C 4000
Description Status Register.
Type RO
Bits Field Name Description Type Reset
31:28 TEST
0x0: Controller does not include the integration test logic
0x1: Controller includes the integration test logic
0x2: Undefined
...
0xF: Undefined
RO 0x0
27:21 RESERVED21 Reads to this field return zero, writes to this field are ignored. RO 0b000 0000
20:16 TOTALCHANNELS Register value returns number of available uDMA channels minus one. For example a read out value of:

0x00: Show that the controller is configured to use 1 uDMA channel
0x01: Shows that the controller is configured to use 2 uDMA channels
...
0x1F: Shows that the controller is configured to use 32 uDMA channels (32-1=31=0x1F)
RO 0b0 1011
15:8 RESERVED8 Reads to this field return zero, writes to this field are ignored. RO 0x00
7:4 STATE Current state of the control state machine. State can be one of the following:

0x0: Idle
0x1: Reading channel controller data
0x2: Reading source data end pointer
0x3: Reading destination data end pointer
0x4: Reading source data
0x5: Writing destination data
0x6: Waiting for uDMA request to clear
0x7: Writing channel controller data
0x8: Stalled
0x9: Done
0xA: Peripheral scatter-gather transition
0xB: Undefined
...
0xF: Undefined.
RO 0x0
3:1 RESERVED1 Reads to this field return zero, writes to this field are ignored. RO 0b000
0 MASTERENABLE Shows the enable status of the controller as configured by CFG.MASTERENABLE:
Value ENUM Name Description
0x0 DIS Controller is disabled
0x1 EN Controller is enabled
RO 0

TOP:DMA:CFG

Address Offset 0x0000 0004
Physical Address 0x400C 4004 Instance 0x400C 4004
Description Configuration Register.
Type WO
Bits Field Name Description Type Reset
31:8 RESERVED8 Reads to this field return zero, writes to this field are ignored. WO 0x00 0000
7:5 PRTOCTRL Sets the AHB-Lite bus protocol protection state by controlling the AHB signal HProt[3:1] as follows:

Bit [7] Controls HProt[3] to indicate if a cacheable access is occurring.
Bit [6] Controls HProt[2] to indicate if a bufferable access is occurring.
Bit [5] Controls HProt[1] to indicate if a privileged access is occurring.

When bit [n] = 1 then the corresponding HProt bit is high.
When bit [n] = 0 then the corresponding HProt bit is low.

This field controls HProt[3:1] signal for all transactions initiated by uDMA except two transactions below:
- the read from the address indicated by source address pointer
- the write to the address indicated by destination address pointer
HProt[3:1] for these two exceptions can be controlled by dedicated fields in the channel configutation descriptor.
WO 0b000
4:1 RESERVED1 Reads to this field return zero, writes to this field are ignored. WO 0x0
0 MASTERENABLE Enables the controller.
Value ENUM Name Description
0x0 DIS Disables the controller
0x1 EN Enables the controller
WO 0

TOP:DMA:CTRL

Address Offset 0x0000 0008
Physical Address 0x400C 4008 Instance 0x400C 4008
Description Channel Control Data Base Pointer Register.
Type RW
Bits Field Name Description Type Reset
31:9 BASEPTR This register point to the base address for the primary data structures of each DMA channel. This is not stored in module, but in system memory, thus space must be allocated for this usage when DMA is in usage RW 0b000 0000 0000 0000 0000 0000
8:0 RESERVED0 Reads to this field return zero, writes to this field are ignored. RO 0b0 0000 0000

TOP:DMA:ALTCTRL

Address Offset 0x0000 000C
Physical Address 0x400C 400C Instance 0x400C 400C
Description Channel Alternate Control Data Base Pointer Register.
Type RO
Bits Field Name Description Type Reset
31:0 BASEPTR This register shows the base address for the alternate data structures and is calculated by module, thus read only RO 0x0000 0100

TOP:DMA:WAITONREQ

Address Offset 0x0000 0010
Physical Address 0x400C 4010 Instance 0x400C 4010
Description Channel Wait On Request Status Register.
Type RO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLSTATUS Channel wait on request status:

Bit [Ch] = 0: Once uDMA receives a single or burst request on channel Ch, this channel may come out of active state even if request is still present.
Bit [Ch] = 1: Once uDMA receives a single or burst request on channel Ch, it keeps channel Ch in active state until the requests are deasserted. This handshake is necessary for channels where the requester is in an asynchronous domain or can run at slower clock speed than uDMA
RO 0xFFF

TOP:DMA:SOFTREQ

Address Offset 0x0000 0014
Physical Address 0x400C 4014 Instance 0x400C 4014
Description Channel Software Request Register.
Type WO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Set the appropriate bit to generate a software uDMA request on the corresponding uDMA channel

Bit [Ch] = 0: Does not create a uDMA request for channel Ch
Bit [Ch] = 1: Creates a uDMA request for channel Ch

Writing to a bit where a uDMA channel is not implemented does not create a uDMA request for that channel
WO 0x000

TOP:DMA:SETBURST

Address Offset 0x0000 0018
Physical Address 0x400C 4018 Instance 0x400C 4018
Description Channel Set UseBurst Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Returns the useburst status, or disables individual channels from generating single uDMA requests. The value R is the arbitration rate and stored in the controller data structure.

Read as:

Bit [Ch] = 0: uDMA channel Ch responds to both burst and single requests on channel Ch. The controller performs 2^R, or single, bus transfers.

Bit [Ch] = 1: uDMA channel Ch does not respond to single transfer requests. The controller only responds to burst transfer requests and performs 2^R transfers.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARBURST.CHNLS to set bit [Ch] to 0.
Bit [Ch] = 1: Disables single transfer requests on channel Ch. The controller performs 2^R transfers for burst requests.

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x000

TOP:DMA:CLEARBURST

Address Offset 0x0000 001C
Physical Address 0x400C 401C Instance 0x400C 401C
Description Channel Clear UseBurst Register.
Type WO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Set the appropriate bit to enable single transfer requests.

Write as:

Bit [Ch] = 0: No effect. Use the SETBURST.CHNLS to disable single transfer requests.

Bit [Ch] = 1: Enables single transfer requests on channel Ch.

Writing to a bit where a uDMA channel is not implemented has no effect.
WO 0x000

TOP:DMA:SETREQMASK

Address Offset 0x0000 0020
Physical Address 0x400C 4020 Instance 0x400C 4020
Description Channel Set Request Mask Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Returns the burst and single request mask status, or disables the corresponding channel from generating uDMA requests.

Read as:
Bit [Ch] = 0: External requests are enabled for channel Ch.
Bit [Ch] = 1: External requests are disabled for channel Ch.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARREQMASK.CHNLS to enable uDMA requests.
Bit [Ch] = 1: Disables uDMA burst request channel [Ch] and uDMA single request channel [Ch] input from generating uDMA requests.

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x000

TOP:DMA:CLEARREQMASK

Address Offset 0x0000 0024
Physical Address 0x400C 4024 Instance 0x400C 4024
Description Clear Channel Request Mask Register.
Type WO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Set the appropriate bit to enable uDMA request for the channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETREQMASK.CHNLS to disable channel Ch from generating requests.
Bit [Ch] = 1: Enables channel [Ch] to generate uDMA requests.

Writing to a bit where a uDMA channel is not implemented has no effect.
WO 0x000

TOP:DMA:SETCHANNELEN

Address Offset 0x0000 0028
Physical Address 0x400C 4028 Instance 0x400C 4028
Description Set Channel Enable Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Returns the enable status of the channels, or enable the corresponding channels.

Read as:
Bit [Ch] = 0: Channel Ch is disabled.
Bit [Ch] = 1: Channel Ch is enabled.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARCHANNELEN.CHNLS to disable a channel
Bit [Ch] = 1: Enables channel Ch

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x000

TOP:DMA:CLEARCHANNELEN

Address Offset 0x0000 002C
Physical Address 0x400C 402C Instance 0x400C 402C
Description Clear Channel Enable Register.
Type WO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Set the appropriate bit to disable the corresponding uDMA channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETCHANNELEN.CHNLS to enable uDMA channels.
Bit [Ch] = 1: Disables channel Ch

Writing to a bit where a uDMA channel is not implemented has no effect
WO 0x000

TOP:DMA:SETCHNLPRIALT

Address Offset 0x0000 0030
Physical Address 0x400C 4030 Instance 0x400C 4030
Description Channel Set Primary-Alternate Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Returns the channel control data structure status, or selects the alternate data structure for the corresponding uDMA channel.

Read as:
Bit [Ch] = 0: uDMA channel Ch is using the primary data structure.
Bit [Ch] = 1: uDMA channel Ch is using the alternate data structure.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARCHNLPRIALT.CHNLS to disable a channel
Bit [Ch] = 1: Selects the alternate data structure for channel Ch

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x000

TOP:DMA:CLEARCHNLPRIALT

Address Offset 0x0000 0034
Physical Address 0x400C 4034 Instance 0x400C 4034
Description Channel Clear Primary-Alternate Register.
Type WO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Clears the appropriate bit to select the primary data structure for the corresponding uDMA channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETCHNLPRIALT.CHNLS to select the alternate data structure.
Bit [Ch] = 1: Selects the primary data structure for channel Ch.

Writing to a bit where a uDMA channel is not implemented has no effect
WO 0x000

TOP:DMA:SETCHNLPRIORITY

Address Offset 0x0000 0038
Physical Address 0x400C 4038 Instance 0x400C 4038
Description Set Channel Priority Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Returns the channel priority mask status, or sets the channel priority to high.

Read as:
Bit [Ch] = 0: uDMA channel Ch is using the default priority level.
Bit [Ch] = 1: uDMA channel Ch is using a high priority level.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARCHNLPRIORITY.CHNLS to set channel Ch to the default priority level.
Bit [Ch] = 1: Channel Ch uses the high priority level.

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x000

TOP:DMA:CLEARCHNLPRIORITY

Address Offset 0x0000 003C
Physical Address 0x400C 403C Instance 0x400C 403C
Description Clear Channel Priority Register.
Type WO
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Clear the appropriate bit to select the default priority level for the specified uDMA channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETCHNLPRIORITY.CHNLS to set channel Ch to the high priority level.
Bit [Ch] = 1: Channel Ch uses the default priority level.

Writing to a bit where a uDMA channel is not implemented has no effect
WO 0x000

TOP:DMA:ERROR

Address Offset 0x0000 004C
Physical Address 0x400C 404C Instance 0x400C 404C
Description Error Status and Clear Register.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Reads to this field return zero, writes to this field are ignored. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 STATUS Returns the status of bus error flag in uDMA, or clears this bit

Read as:

0: No bus error detected
1: Bus error detected

Write as:

0: No effect, status of bus error flag is unchanged.
1: Clears the bus error flag.
RW 0

TOP:DMA:REQDONE

Address Offset 0x0000 0504
Physical Address 0x400C 4504 Instance 0x400C 4504
Description Channel Request Done Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Reflects the uDMA done status for the given channel, channel [Ch]. It's a sticky done bit. Unless cleared by writing a 1, it holds the value of 1.

Read as:
Bit [Ch] = 0: Request has not completed for channel Ch
Bit [Ch] = 1: Request has completed for the channel Ch

Writing a 1 to individual bits would clear the corresponding bit.

Write as:
Bit [Ch] = 0: No effect.
Bit [Ch] = 1: The corresponding [Ch] bit is cleared and is set to 0
RW 0x000

TOP:DMA:DONEMASK

Address Offset 0x0000 0520
Physical Address 0x400C 4520 Instance 0x400C 4520
Description Channel Request Done Mask Register.
Type RW
Bits Field Name Description Type Reset
31:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0 0000
11:0 CHNLS Controls the propagation of the uDMA done and active state to the assigned peripheral. Specifically used for software channels.

Read as:
Bit [Ch] = 0: uDMA done and active state for channel Ch is not blocked from reaching to the peripherals.
Note that the uDMA done state for channel [Ch] is blocked from contributing to generation of combined uDMA done signal

Bit [Ch] = 1: uDMA done and active state for channel Ch is blocked from reaching to the peripherals.
Note that the uDMA done state for channel [Ch] is not blocked from contributing to generation of combined uDMA done signal

Write as:
Bit [Ch] = 0: Allows uDMA done and active state to propagate to the peripherals.
Note that this disables uDMA done state for channel [Ch] from contributing to generation of combined uDMA done signal

Bit [Ch] = 1: Blocks uDMA done and active state to propagate to the peripherals.
Note that this enables uDMA done for channel [Ch] to contribute to generation of combined uDMA done signal.
RW 0x000