![]() |
![]() |
|
CC27xxDriverLibrary
|
#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_ints.h"#include "../inc/hw_memmap.h"#include "../inc/hw_systick.h"#include "debug.h"#include "interrupt.h"

Go to the source code of this file.
Functions | |
| __STATIC_INLINE void | SysTickEnable (void) |
| Enables the SysTick counter. More... | |
| __STATIC_INLINE void | SysTickDisable (void) |
| Disables the SysTick counter. More... | |
| __STATIC_INLINE void | SysTickRegisterInt (void(*pfnHandler)(void)) |
| Registers an interrupt handler for the SysTick interrupt in the dynamic interrupt table. More... | |
| __STATIC_INLINE void | SysTickUnregisterInt (void) |
| Unregisters the interrupt handler for the SysTick interrupt in the dynamic interrupt table. More... | |
| __STATIC_INLINE void | SysTickEnableInt (void) |
| Enables the SysTick interrupt. More... | |
| __STATIC_INLINE void | SysTickDisableInt (void) |
| Disables the SysTick interrupt. More... | |
| __STATIC_INLINE void | SysTickSetPeriod (uint32_t period) |
| Sets the period of the SysTick counter. More... | |
| __STATIC_INLINE uint32_t | SysTickGetPeriod (void) |
| Gets the period of the SysTick counter. More... | |
| __STATIC_INLINE uint32_t | SysTickGetValue (void) |
| Gets the current value of the SysTick counter. More... | |