CC27xxDriverLibrary
uDMAControlTableEntry Struct Reference

A structure that defines an entry in the channel control table. More...

#include <udma.h>

Data Fields

volatile void * pSrcEndAddr
 The ending source address of the data transfer. More...
 
volatile void * pDstEndAddr
 The ending destination address of the data transfer. More...
 
volatile uint32_t control
 The channel control mode. More...
 
volatile uint32_t spare
 An unused location. More...
 

Detailed Description

A structure that defines an entry in the channel control table.

These fields are used by the uDMA controller and normally it is not necessary for software to directly read or write fields in the table.

Field Documentation

§ pSrcEndAddr

volatile void* uDMAControlTableEntry::pSrcEndAddr

The ending source address of the data transfer.

Referenced by uDMASetChannelTransfer().

§ pDstEndAddr

volatile void* uDMAControlTableEntry::pDstEndAddr

The ending destination address of the data transfer.

Referenced by uDMASetChannelTransfer().

§ control

volatile uint32_t uDMAControlTableEntry::control

§ spare

volatile uint32_t uDMAControlTableEntry::spare

An unused location.

Referenced by uDMASetChannelTransfer().


The documentation for this struct was generated from the following file: