![]() |
![]() |
|
CC27xxDriverLibrary
|
SHA256SW Object. More...
#include <sha256sw.h>
Data Fields | |
| uint32_t | bitsProcessed |
| int8_t | offsetWb |
| uint8_t | reserved1 |
| uint8_t | reserved2 |
| uint8_t | reserved3 |
| uint32_t | digest32 [8] |
| uint32_t | Ws32 [16] |
SHA256SW Object.
The application must not access any member variables of this structure!
| uint32_t SHA256SW_Object::bitsProcessed |
| int8_t SHA256SW_Object::offsetWb |
| uint8_t SHA256SW_Object::reserved1 |
| uint8_t SHA256SW_Object::reserved2 |
| uint8_t SHA256SW_Object::reserved3 |
| uint32_t SHA256SW_Object::digest32[8] |
| uint32_t SHA256SW_Object::Ws32[16] |