![]() |
![]() |
|
CC27xxDriverLibrary
|
#include <stdbool.h>#include <stdint.h>#include "../inc/hw_ints.h"#include "../inc/hw_types.h"#include "../cmsis/cc27xx.h"#include "../cmsis/core/core_cm33.h"#include "cpu.h"

Go to the source code of this file.
Functions | |
| void | IntRegister (uint32_t intNum, void(*handler)(void)) |
| Registers a function as an interrupt handler in the dynamic vector table. More... | |
| void | IntUnregister (uint32_t intNum) |
| Unregisters an interrupt handler in the dynamic vector table. More... | |
| void | IntSetPriority (uint32_t intNum, uint8_t priority) |
| Sets the priority of an interrupt. More... | |
| int32_t | IntGetPriority (uint32_t intNum) |
| Gets the priority of an interrupt. More... | |
| bool | IntIsEnabled (uint32_t intNum) |
| Check whether an interrupt is enabled. More... | |
| void | IntEnable (uint32_t intNum) |
| Enables an interrupt or system exception. More... | |
| void | IntDisable (uint32_t intNum) |
| Disables an interrupt or system exception. More... | |
| void | IntSetPend (uint32_t intNum) |
| Pends an interrupt. More... | |
| bool | IntGetPend (uint32_t intNum) |
| Checks if an interrupt is pending. More... | |
| void | IntClearPend (uint32_t intNum) |
| Unpends an interrupt. More... | |
| __STATIC_INLINE bool | IntEnableMaster (void) |
| Enables the CPU interrupt. More... | |
| __STATIC_INLINE bool | IntDisableMaster (void) |
| Disables the CPU interrupts with configurable priority. More... | |