![]() |
![]() |
|
CC27xxDriverLibrary
|
|
Data Structures | |
| struct | uDMAControlTableEntry |
| A structure that defines an entry in the channel control table. More... | |
Macros | |
| #define | uDMATaskStructEntry(transferCount, itemSize, srcIncrement, pSrcAddr, dstIncrement, pDstAddr, arbSize, mode) |
| A helper macro for building scatter-gather task table entries. More... | |
| #define | UDMA_NUM_CHANNELS 8 |
| #define | UDMA_PRIORITY_LOW 0x00000000 |
| #define | UDMA_PRIORITY_HIGH 0x00000001 |
| #define | UDMA_ATTR_USEBURST 0x00000001 |
| #define | UDMA_ATTR_ALTSELECT 0x00000002 |
| #define | UDMA_ATTR_HIGH_PRIORITY 0x00000004 |
| #define | UDMA_ATTR_REQMASK 0x00000008 |
| #define | UDMA_ATTR_ALL 0x0000000F |
| #define | UDMA_MODE_STOP 0x00000000 |
| #define | UDMA_MODE_BASIC 0x00000001 |
| #define | UDMA_MODE_AUTO 0x00000002 |
| #define | UDMA_MODE_PINGPONG 0x00000003 |
| #define | UDMA_MODE_MEM_SCATTER_GATHER 0x00000004 |
| #define | UDMA_MODE_PER_SCATTER_GATHER 0x00000006 |
| #define | UDMA_MODE_M 0x00000007 |
| #define | UDMA_MODE_ALT_SELECT 0x00000001 |
| #define | UDMA_DST_INC_8 0x00000000 |
| #define | UDMA_DST_INC_16 0x40000000 |
| #define | UDMA_DST_INC_32 0x80000000 |
| #define | UDMA_DST_INC_NONE 0xC0000000 |
| #define | UDMA_DST_INC_M 0xC0000000 |
| #define | UDMA_DST_INC_S 30 |
| #define | UDMA_SRC_INC_8 0x00000000 |
| #define | UDMA_SRC_INC_16 0x04000000 |
| #define | UDMA_SRC_INC_32 0x08000000 |
| #define | UDMA_SRC_INC_NONE 0x0c000000 |
| #define | UDMA_SRC_INC_M 0x0C000000 |
| #define | UDMA_SRC_INC_S 26 |
| #define | UDMA_SIZE_8 0x00000000 |
| #define | UDMA_SIZE_16 0x11000000 |
| #define | UDMA_SIZE_32 0x22000000 |
| #define | UDMA_SIZE_M 0x33000000 |
| #define | UDMA_SIZE_S 24 |
| #define | UDMA_ARB_1 0x00000000 |
| #define | UDMA_ARB_2 0x00004000 |
| #define | UDMA_ARB_4 0x00008000 |
| #define | UDMA_ARB_8 0x0000c000 |
| #define | UDMA_ARB_16 0x00010000 |
| #define | UDMA_ARB_32 0x00014000 |
| #define | UDMA_ARB_64 0x00018000 |
| #define | UDMA_ARB_128 0x0001c000 |
| #define | UDMA_ARB_256 0x00020000 |
| #define | UDMA_ARB_512 0x00024000 |
| #define | UDMA_ARB_1024 0x00028000 |
| #define | UDMA_ARB_M 0x0003C000 |
| #define | UDMA_ARB_S 14 |
| #define | UDMA_NEXT_USEBURST 0x00000008 |
| #define | UDMA_XFER_SIZE_MAX 1024 |
| #define | UDMA_XFER_SIZE_M 0x00003FF0 |
| #define | UDMA_XFER_SIZE_S 4 |
| #define | UDMA_CHANNEL_0_M 0x001 |
| UDMA channel 0 (SPI0_TX or UART1_RX) More... | |
| #define | UDMA_CHANNEL_1_M 0x002 |
| UDMA channel 1 (SPI0_RX or UART1_TX) More... | |
| #define | UDMA_CHANNEL_2_M 0x004 |
| UDMA channel 2 (LRFD or UART0_TX) More... | |
| #define | UDMA_CHANNEL_3_M 0x008 |
| UDMA channel 3 (ADC0 or UART0_RX) More... | |
| #define | UDMA_CHANNEL_4_M 0x010 |
| UDMA channel 4 (AES_A or LRFD) More... | |
| #define | UDMA_CHANNEL_5_M 0x020 |
| UDMA channel 5 (AES_B or ADC0) More... | |
| #define | UDMA_CHANNEL_6_M 0x040 |
| UDMA channel 6 (CAN_A or SPI1_TX) More... | |
| #define | UDMA_CHANNEL_7_M 0x080 |
| UDMA channel 7 (CAN_B or SPI1_RX) More... | |
| #define | UDMA_CHANNEL_8_M 0x100 |
| UDMA channel 8 (Software Event Channel 0) More... | |
| #define | UDMA_CHANNEL_9_M 0x200 |
| UDMA channel 9 (Software Event Channel 1) More... | |
| #define | UDMA_CHANNEL_10_M 0x400 |
| UDMA channel 10 (Software Event Channel 2) More... | |
| #define | UDMA_CHANNEL_11_M 0x800 |
| UDMA channel 11 (Software Event Channel 3) More... | |
| #define | UDMA_PRI_SELECT 0x00000000 |
| #define | UDMA_ALT_SELECT 0x00000010 |
Functions | |
| __STATIC_INLINE void | uDMAEnable (void) |
| Enables the uDMA controller for use. More... | |
| __STATIC_INLINE void | uDMADisable (void) |
| Disables the uDMA controller for use. More... | |
| __STATIC_INLINE uint32_t | uDMAGetErrorStatus (void) |
| Gets the uDMA error status. More... | |
| __STATIC_INLINE void | uDMAClearErrorStatus (void) |
| Clears the uDMA error interrupt. More... | |
| __STATIC_INLINE void | uDMAEnableChannel (uint32_t channelBitMask) |
| Enables a uDMA channel for operation. More... | |
| __STATIC_INLINE void | uDMADisableChannel (uint32_t channelBitMask) |
| Disables a uDMA channel for operation. More... | |
| __STATIC_INLINE bool | uDMAIsChannelEnabled (uint32_t channelBitMask) |
| Checks if a uDMA channel is enabled for operation. More... | |
| __STATIC_INLINE void | uDMASetControlBase (void *pControlTable) |
| Sets the base address for the channel control table. More... | |
| __STATIC_INLINE void * | uDMAGetControlBase (void) |
| Gets the base address for the channel control table. More... | |
| __STATIC_INLINE void * | uDMAGetControlAlternateBase (void) |
| Gets the base address for the channel control table alternate structures. More... | |
| __STATIC_INLINE void | uDMARequestChannel (uint32_t channelBitMask) |
| Requests a uDMA channel to start a transfer. More... | |
| void | uDMAEnableChannelAttribute (uint32_t channelBitMask, uint32_t attr) |
| Enables attributes of a uDMA channel. More... | |
| void | uDMADisableChannelAttribute (uint32_t channelBitMask, uint32_t attr) |
| Disables attributes of an uDMA channel. More... | |
| uint32_t | uDMAGetChannelAttribute (uint32_t channelBitMask) |
| Gets the enabled attributes of a uDMA channel. More... | |
| void | uDMASetChannelControl (volatile uDMAControlTableEntry *pChannelControlStruct, uint32_t control) |
| Sets the control parameters for a uDMA channel control structure. More... | |
| void | uDMASetChannelTransfer (volatile uDMAControlTableEntry *pChannelControlStruct, uint32_t mode, void *pSrcAddr, void *pDstAddr, uint32_t transferSize) |
| Sets the transfer parameters for a uDMA channel control structure. More... | |
| uint32_t | uDMAGetChannelSize (volatile uDMAControlTableEntry const *pChannelControlStruct) |
| Gets the current transfer size for a uDMA channel control structure. More... | |
| uint32_t | uDMAGetChannelMode (volatile uDMAControlTableEntry const *pChannelControlStruct) |
| Gets the transfer mode for a uDMA channel control structure. More... | |
| __STATIC_INLINE void | uDMARegisterInt (uint32_t intChannel, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the uDMA controller in the dynamic interrupt table. More... | |
| __STATIC_INLINE void | uDMAUnregisterInt (uint32_t intChannel) |
| Unregisters an interrupt handler for the uDMA controller in the dynamic interrupt table. More... | |
| __STATIC_INLINE void | uDMAClearInt (uint32_t channelBitMask) |
| Clears uDMA interrupt done status. More... | |
| __STATIC_INLINE uint32_t | uDMAIntStatus (void) |
| Get the uDMA interrupt status. More... | |
| __STATIC_INLINE void | uDMAEnableSwEventInt (uint32_t intChannel) |
| Enable interrupt on software event driven uDMA transfers. More... | |
| __STATIC_INLINE void | uDMADisableSwEventInt (uint32_t intChannel) |
| Disable interrupt on software event driven uDMA transfers. More... | |
| __STATIC_INLINE uint32_t | uDMAGetStatus (void) |
| Return the status of the uDMA module. More... | |
| __STATIC_INLINE void | uDMASetChannelPriority (uint32_t channelBitMask) |
| Set the priority of a uDMA channel. More... | |
| __STATIC_INLINE bool | uDMAGetChannelPriority (uint32_t channelBitMask) |
| Get the priority of a uDMA channel. More... | |
| __STATIC_INLINE void | uDMAClearChannelPriority (uint32_t channelBitMask) |
| Clear the priority of a uDMA channel. More... | |
| #define uDMATaskStructEntry | ( | transferCount, | |
| itemSize, | |||
| srcIncrement, | |||
| pSrcAddr, | |||
| dstIncrement, | |||
| pDstAddr, | |||
| arbSize, | |||
| mode | |||
| ) |
A helper macro for building scatter-gather task table entries.
This macro is intended to be used to help populate a table of uDMA tasks for a scatter-gather transfer. This macro will calculate the values for the fields of a task structure entry based on the input parameters.
There are specific requirements for the values of each parameter. No checking is done so it is up to the caller to ensure that correct values are used for the parameters.
This macro is intended to be used to initialize individual entries of a structure of uDMAControlTableEntry type, like this:
uDMAControlTableEntry MyTaskList[] =
{
uDMATaskStructEntry(Task1Count, UDMA_SIZE_8,
UDMA_SRC_INC_8, MySourceBuf,
UDMA_DST_INC_8, MyDestBuf,
UDMA_ARB_8, UDMA_MODE_MEM_SCATTER_GATHER),
uDMATaskStructEntry(Task2Count, ... ),
}
| transferCount | is the count of items to transfer for this task. It must be in the range 1-1024. |
| itemSize | is the bit size of the items to transfer for this task. It must be one of: |
| srcIncrement | is the bit size increment for source data. It must be one of: |
| pSrcAddr | is the starting address of the data to transfer. |
| dstIncrement | is the bit size increment for destination data. It must be one of: |
| pDstAddr | is the starting address of the destination data. |
| arbSize | is the arbitration size to use for the transfer task. This is used to select the arbitration size in powers of 2, from 1 to 1024. It must be one of: |
| mode | is the transfer mode for this task. Note that normally all tasks will be one of the scatter-gather modes while the last task is a task list will be AUTO or BASIC. It must be one of: |
| #define UDMA_NUM_CHANNELS 8 |
Referenced by uDMADisableSwEventInt(), and uDMAEnableSwEventInt().
| #define UDMA_PRIORITY_LOW 0x00000000 |
Referenced by uDMAGetChannelPriority().
| #define UDMA_PRIORITY_HIGH 0x00000001 |
Referenced by uDMAGetChannelPriority().
| #define UDMA_ATTR_USEBURST 0x00000001 |
Referenced by uDMADisableChannelAttribute(), uDMAEnableChannelAttribute(), and uDMAGetChannelAttribute().
| #define UDMA_ATTR_ALTSELECT 0x00000002 |
Referenced by uDMADisableChannelAttribute(), uDMAEnableChannelAttribute(), and uDMAGetChannelAttribute().
| #define UDMA_ATTR_HIGH_PRIORITY 0x00000004 |
Referenced by uDMADisableChannelAttribute(), uDMAEnableChannelAttribute(), and uDMAGetChannelAttribute().
| #define UDMA_ATTR_REQMASK 0x00000008 |
Referenced by uDMADisableChannelAttribute(), uDMAEnableChannelAttribute(), and uDMAGetChannelAttribute().
| #define UDMA_ATTR_ALL 0x0000000F |
| #define UDMA_MODE_STOP 0x00000000 |
| #define UDMA_MODE_BASIC 0x00000001 |
| #define UDMA_MODE_AUTO 0x00000002 |
| #define UDMA_MODE_PINGPONG 0x00000003 |
| #define UDMA_MODE_MEM_SCATTER_GATHER 0x00000004 |
Referenced by uDMAGetChannelMode(), and uDMASetChannelTransfer().
| #define UDMA_MODE_PER_SCATTER_GATHER 0x00000006 |
Referenced by uDMAGetChannelMode(), and uDMASetChannelTransfer().
| #define UDMA_MODE_M 0x00000007 |
Referenced by uDMAGetChannelMode(), uDMAGetChannelSize(), and uDMASetChannelTransfer().
| #define UDMA_MODE_ALT_SELECT 0x00000001 |
Referenced by uDMAGetChannelMode(), and uDMASetChannelTransfer().
| #define UDMA_DST_INC_8 0x00000000 |
| #define UDMA_DST_INC_16 0x40000000 |
| #define UDMA_DST_INC_32 0x80000000 |
| #define UDMA_DST_INC_NONE 0xC0000000 |
Referenced by uDMASetChannelTransfer().
| #define UDMA_DST_INC_M 0xC0000000 |
Referenced by uDMASetChannelControl(), and uDMASetChannelTransfer().
| #define UDMA_DST_INC_S 30 |
Referenced by uDMASetChannelTransfer().
| #define UDMA_SRC_INC_8 0x00000000 |
| #define UDMA_SRC_INC_16 0x04000000 |
| #define UDMA_SRC_INC_32 0x08000000 |
| #define UDMA_SRC_INC_NONE 0x0c000000 |
Referenced by uDMASetChannelTransfer().
| #define UDMA_SRC_INC_M 0x0C000000 |
Referenced by uDMASetChannelControl(), and uDMASetChannelTransfer().
| #define UDMA_SRC_INC_S 26 |
Referenced by uDMASetChannelTransfer().
| #define UDMA_SIZE_8 0x00000000 |
| #define UDMA_SIZE_16 0x11000000 |
| #define UDMA_SIZE_32 0x22000000 |
| #define UDMA_SIZE_M 0x33000000 |
Referenced by uDMASetChannelControl().
| #define UDMA_SIZE_S 24 |
| #define UDMA_ARB_1 0x00000000 |
| #define UDMA_ARB_2 0x00004000 |
| #define UDMA_ARB_4 0x00008000 |
| #define UDMA_ARB_8 0x0000c000 |
| #define UDMA_ARB_16 0x00010000 |
| #define UDMA_ARB_32 0x00014000 |
| #define UDMA_ARB_64 0x00018000 |
| #define UDMA_ARB_128 0x0001c000 |
| #define UDMA_ARB_256 0x00020000 |
| #define UDMA_ARB_512 0x00024000 |
| #define UDMA_ARB_1024 0x00028000 |
| #define UDMA_ARB_M 0x0003C000 |
Referenced by uDMASetChannelControl().
| #define UDMA_ARB_S 14 |
| #define UDMA_NEXT_USEBURST 0x00000008 |
Referenced by uDMASetChannelControl().
| #define UDMA_XFER_SIZE_MAX 1024 |
Referenced by uDMASetChannelTransfer().
| #define UDMA_XFER_SIZE_M 0x00003FF0 |
Referenced by uDMAGetChannelSize(), and uDMASetChannelTransfer().
| #define UDMA_XFER_SIZE_S 4 |
Referenced by uDMAGetChannelSize(), and uDMASetChannelTransfer().
| #define UDMA_CHANNEL_0_M 0x001 |
UDMA channel 0 (SPI0_TX or UART1_RX)
| #define UDMA_CHANNEL_1_M 0x002 |
UDMA channel 1 (SPI0_RX or UART1_TX)
| #define UDMA_CHANNEL_2_M 0x004 |
UDMA channel 2 (LRFD or UART0_TX)
| #define UDMA_CHANNEL_3_M 0x008 |
UDMA channel 3 (ADC0 or UART0_RX)
| #define UDMA_CHANNEL_4_M 0x010 |
UDMA channel 4 (AES_A or LRFD)
| #define UDMA_CHANNEL_5_M 0x020 |
UDMA channel 5 (AES_B or ADC0)
| #define UDMA_CHANNEL_6_M 0x040 |
UDMA channel 6 (CAN_A or SPI1_TX)
| #define UDMA_CHANNEL_7_M 0x080 |
UDMA channel 7 (CAN_B or SPI1_RX)
| #define UDMA_CHANNEL_8_M 0x100 |
UDMA channel 8 (Software Event Channel 0)
| #define UDMA_CHANNEL_9_M 0x200 |
UDMA channel 9 (Software Event Channel 1)
| #define UDMA_CHANNEL_10_M 0x400 |
UDMA channel 10 (Software Event Channel 2)
| #define UDMA_CHANNEL_11_M 0x800 |
UDMA channel 11 (Software Event Channel 3)
| #define UDMA_PRI_SELECT 0x00000000 |
| #define UDMA_ALT_SELECT 0x00000010 |
Referenced by uDMASetChannelTransfer().
| __STATIC_INLINE void uDMAEnable | ( | void | ) |
Enables the uDMA controller for use.
This function enables the uDMA controller. The uDMA controller must be enabled before it can be configured and used.
| __STATIC_INLINE void uDMADisable | ( | void | ) |
Disables the uDMA controller for use.
This function disables the uDMA controller. Once disabled, the uDMA controller will not operate until re-enabled with uDMAEnable().
| __STATIC_INLINE uint32_t uDMAGetErrorStatus | ( | void | ) |
Gets the uDMA error status.
This function returns the uDMA error status. It should be called from within the uDMA error interrupt handler to determine if a uDMA error occurred.
| __STATIC_INLINE void uDMAClearErrorStatus | ( | void | ) |
Clears the uDMA error interrupt.
This function clears a pending uDMA error interrupt. It should be called from within the uDMA error interrupt handler to clear the interrupt.
| __STATIC_INLINE void uDMAEnableChannel | ( | uint32_t | channelBitMask | ) |
Enables a uDMA channel for operation.
This function enables the specified uDMA channels for use. This function must be used to enable a channel before it can be used to perform a uDMA transfer.
When a uDMA transfer is completed, the channel will be automatically disabled by the uDMA controller. Therefore, this function should be called prior to starting up any new transfer.
| channelBitMask | is the bitmask of the channels to enable. |
| __STATIC_INLINE void uDMADisableChannel | ( | uint32_t | channelBitMask | ) |
Disables a uDMA channel for operation.
This function disables the specified uDMA channels. Once disabled, a channel will not respond to uDMA transfer requests until re-enabled via uDMAEnableChannel().
| channelBitMask | is the bitmask of the channels to disable. |
| __STATIC_INLINE bool uDMAIsChannelEnabled | ( | uint32_t | channelBitMask | ) |
Checks if a uDMA channel is enabled for operation.
This function checks to see if a specific uDMA channel is enabled. This can be used to check the status of a transfer, since the channel will be automatically disabled at the end of a transfer. Note that if multiple channels are specified in the bitmask, the return value will be true if at least one channel is enabled.
| channelBitMask | is the bitmask of the channel to check. |
true : Channel is enabled.false : Channel is disabled. | __STATIC_INLINE void uDMASetControlBase | ( | void * | pControlTable | ) |
Sets the base address for the channel control table.
This function sets the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel. The table must be aligned on a 1024 byte boundary. The base address must be set before any of the channel functions can be used. Setting the base address of the primary control table will automatically set the address for the alternate control table as the next memory location after the primary control table.
The size of the channel control table depends on the number of uDMA channels, and which transfer modes are used. Refer to the introductory text and the microcontroller datasheet for more information about the channel control table.
| pControlTable | is a pointer to the 1024 byte aligned base address of the uDMA channel control table. The address must be an absolute address in system memory space. |
References ASSERT.
| __STATIC_INLINE void* uDMAGetControlBase | ( | void | ) |
Gets the base address for the channel control table.
This function gets the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel.
| __STATIC_INLINE void* uDMAGetControlAlternateBase | ( | void | ) |
Gets the base address for the channel control table alternate structures.
This function gets the base address of the second half of the channel control table that holds the alternate control structures for each channel.
| __STATIC_INLINE void uDMARequestChannel | ( | uint32_t | channelBitMask | ) |
Requests a uDMA channel to start a transfer.
This function allows software to request a uDMA channel to begin a transfer. This could be used for performing a memory to memory transfer, or if for some reason a transfer needs to be initiated by software instead of the peripheral associated with that channel.
| channelBitMask | is the bitmask of the channel on which to request a uDMA transfer. |
References uDMADisableChannelAttribute(), uDMAEnableChannelAttribute(), uDMAGetChannelAttribute(), uDMAGetChannelMode(), uDMAGetChannelSize(), uDMASetChannelControl(), and uDMASetChannelTransfer().
| void uDMAEnableChannelAttribute | ( | uint32_t | channelBitMask, |
| uint32_t | attr | ||
| ) |
Enables attributes of a uDMA channel.
This function is used to enable attributes of a uDMA channel.
| channelBitMask | is bitmask of the channel to configure. |
| attr | is a combination of attributes for the channel. The parameter is the bitwise OR of any of the following:
|
References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.
Referenced by uDMARequestChannel().
| void uDMADisableChannelAttribute | ( | uint32_t | channelBitMask, |
| uint32_t | attr | ||
| ) |
Disables attributes of an uDMA channel.
This function is used to disable attributes of a uDMA channel.
| channelBitMask | is bitmask of the channel to configure. |
| attr | is a combination of attributes for the channel. The parameter is the bitwise OR of any of the following:
|
References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.
Referenced by uDMARequestChannel().
| uint32_t uDMAGetChannelAttribute | ( | uint32_t | channelBitMask | ) |
Gets the enabled attributes of a uDMA channel.
This function returns a combination of flags representing the attributes of the uDMA channel.
| channelBitMask | is the bitmask of the channel to configure. |
References UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.
Referenced by uDMARequestChannel().
| void uDMASetChannelControl | ( | volatile uDMAControlTableEntry * | pChannelControlStruct, |
| uint32_t | control | ||
| ) |
Sets the control parameters for a uDMA channel control structure.
This function is used to set control parameters for a uDMA transfer. These are typically parameters that are not changed often.
| pChannelControlStruct | is a pointer to the primary or alternate control table of the uDMA channel to be set. |
| control | is the bitwise OR of five values:
|
References ASSERT, uDMAControlTableEntry::control, UDMA_ARB_M, UDMA_DST_INC_M, UDMA_NEXT_USEBURST, UDMA_SIZE_M, and UDMA_SRC_INC_M.
Referenced by uDMARequestChannel().
| void uDMASetChannelTransfer | ( | volatile uDMAControlTableEntry * | pChannelControlStruct, |
| uint32_t | mode, | ||
| void * | pSrcAddr, | ||
| void * | pDstAddr, | ||
| uint32_t | transferSize | ||
| ) |
Sets the transfer parameters for a uDMA channel control structure.
This function is used to set the parameters for a uDMA transfer. These are typically parameters that are changed often. The function uDMASetChannelControl() MUST be called at least once for this channel prior to calling this function.
The pSrcAddr and pDstAddr parameters are pointers to the first location of the data to be transferred. These addresses should be aligned according to the item size. The compiler will take care of this if the pointers are pointing to storage of the appropriate data type.
The two scatter/gather modes, MEMORY and PERIPHERAL, are actually different depending on whether the primary or alternate control structure is selected. This function will recognize from the address of the pChannelControlStruct if it's a primary or alternate control structure and will set the scatter/gather mode as appropriate for it.
The channel must also be enabled using uDMAEnableChannel() after calling this function. The transfer will not begin until the channel has been set up and enabled. Note that the channel is automatically disabled after the transfer is completed, meaning that uDMAEnableChannel() must be called again after setting up the next transfer.
| pChannelControlStruct | is a pointer to the primary or alternate control table of the uDMA channel to be set. |
| mode | is the type of uDMA transfer. The parameter should be one of the following values:
|
| pSrcAddr | is the source address for the transfer. |
| pDstAddr | is the destination address for the transfer. |
| transferSize | is the number of data items to transfer (NOT bytes). |
References ASSERT, uDMAControlTableEntry::control, uDMAControlTableEntry::pDstEndAddr, uDMAControlTableEntry::pSrcEndAddr, uDMAControlTableEntry::spare, UDMA_ALT_SELECT, UDMA_DST_INC_M, UDMA_DST_INC_NONE, UDMA_DST_INC_S, UDMA_MODE_ALT_SELECT, UDMA_MODE_M, UDMA_MODE_MEM_SCATTER_GATHER, UDMA_MODE_PER_SCATTER_GATHER, UDMA_SRC_INC_M, UDMA_SRC_INC_NONE, UDMA_SRC_INC_S, UDMA_XFER_SIZE_M, UDMA_XFER_SIZE_MAX, and UDMA_XFER_SIZE_S.
Referenced by uDMARequestChannel().
| uint32_t uDMAGetChannelSize | ( | volatile uDMAControlTableEntry const * | pChannelControlStruct | ) |
Gets the current transfer size for a uDMA channel control structure.
This function is used to get the uDMA transfer size for a channel. The transfer size is the number of items to transfer, where the size of an item might be 8, 16, or 32 bits. If a partial transfer has already occurred, then the number of remaining items will be returned. If the transfer is complete, then 0 will be returned.
| pChannelControlStruct | is a pointer to the primary or alternate control table of the uDMA channel in use. |
References ASSERT, uDMAControlTableEntry::control, UDMA_MODE_M, UDMA_XFER_SIZE_M, and UDMA_XFER_SIZE_S.
Referenced by uDMARequestChannel().
| uint32_t uDMAGetChannelMode | ( | volatile uDMAControlTableEntry const * | pChannelControlStruct | ) |
Gets the transfer mode for a uDMA channel control structure.
This function is used to get the transfer mode for the uDMA channel. It can be used to query the status of a transfer on a channel. When the transfer is complete the mode will be UDMA_MODE_STOP.
| pChannelControlStruct | is a pointer to the primary or alternate control table of the uDMA channel in use. |
References ASSERT, uDMAControlTableEntry::control, UDMA_MODE_ALT_SELECT, UDMA_MODE_M, UDMA_MODE_MEM_SCATTER_GATHER, and UDMA_MODE_PER_SCATTER_GATHER.
Referenced by uDMARequestChannel().
| __STATIC_INLINE void uDMARegisterInt | ( | uint32_t | intChannel, |
| void(*)(void) | pfnHandler | ||
| ) |
Registers an interrupt handler for the uDMA controller in the dynamic interrupt table.
This function registers a function as the interrupt handler for a specific interrupt and enables the corresponding interrupt in the interrupt controller.
| intChannel | specifies which uDMA interrupt is to be registered.
|
| pfnHandler | is a pointer to the function to be called when the interrupt is activated. |
References ASSERT, IntEnable(), and IntRegister().
| __STATIC_INLINE void uDMAUnregisterInt | ( | uint32_t | intChannel | ) |
Unregisters an interrupt handler for the uDMA controller in the dynamic interrupt table.
This function will disable and clear the handler to be called for the specified uDMA interrupt.
| intChannel | specifies which uDMA interrupt to unregister.
|
References ASSERT, IntDisable(), and IntUnregister().
| __STATIC_INLINE void uDMAClearInt | ( | uint32_t | channelBitMask | ) |
Clears uDMA interrupt done status.
Clears bits in the uDMA interrupt status register according to which bits are set in channelBitMask. There is one bit for each channel. If a a bit is set in channelBitMask, then that corresponding channel's interrupt status will be cleared (if it was set).
| channelBitMask | is a mask with one bit for each uDMA channel. |
| __STATIC_INLINE uint32_t uDMAIntStatus | ( | void | ) |
Get the uDMA interrupt status.
This function returns the interrupt status for the specified UDMA. This function does not differentiate between software or hardware activated interrupts.
| __STATIC_INLINE void uDMAEnableSwEventInt | ( | uint32_t | intChannel | ) |
Enable interrupt on software event driven uDMA transfers.
| intChannel | identifies which uDMA interrupt to enable software interrupts for. |
References ASSERT, and UDMA_NUM_CHANNELS.
| __STATIC_INLINE void uDMADisableSwEventInt | ( | uint32_t | intChannel | ) |
Disable interrupt on software event driven uDMA transfers.
This register disables the blocking of the uDMA status signals propagation to the hardware peripheral connected to the uDMA on the intChannel.
| intChannel | identifies which uDMA interrupt to disable software interrupts for. |
References ASSERT, and UDMA_NUM_CHANNELS.
| __STATIC_INLINE uint32_t uDMAGetStatus | ( | void | ) |
Return the status of the uDMA module.
| __STATIC_INLINE void uDMASetChannelPriority | ( | uint32_t | channelBitMask | ) |
Set the priority of a uDMA channel.
| channelBitMask | is bitmask of the uDMA channel to set the priority for. |
| __STATIC_INLINE bool uDMAGetChannelPriority | ( | uint32_t | channelBitMask | ) |
Get the priority of a uDMA channel.
| channelBitMask | The bitmask of the uDMA channel to get the priority for. |
References UDMA_PRIORITY_HIGH, and UDMA_PRIORITY_LOW.
| __STATIC_INLINE void uDMAClearChannelPriority | ( | uint32_t | channelBitMask | ) |
Clear the priority of a uDMA channel.
| channelBitMask | The bitmask of the uDMA channel to clear the priority for. |