SHA2 256/224 SW APIs.
More...
|
| int_fast16_t | SHA256SWHashData (SHA256SW_Handle handle, SHA2SW_HashType hashType, const void *data, size_t length, uint32_t digest[8]) |
| | Performs a complete hash operation, producing a final digest for the data. More...
|
| |
| int_fast16_t | SHA256SWStart (SHA256SW_Handle handle, SHA2SW_HashType hashType) |
| | Initialize a SHA256SW_Handle, preparing for hashing data. More...
|
| |
| int_fast16_t | SHA256SWAddData (SHA256SW_Handle handle, const void *data, size_t length) |
| | Add data to a SHA256/224 operation. More...
|
| |
| int_fast16_t | SHA256SWFinalize (SHA256SW_Handle handle, uint32_t digest[8]) |
| | Finalize a SHA256/224 operation, creating the final digest. More...
|
| |
SHA2 256/224 SW APIs.
Overview
Provides top-level general purpose SHA2 256/224 APIs. SHA2 algorithm is implemented in SW with no HW acceleration. The implementation is highly optimized for speed and code size. These functions reside in ROM, and are exposed through HAPI, and also through the function prototypes and macros below.
Availability of SHA2 224 depends on build configuration. See file sha2sw_config.h.
Limitations
- A maximum of 512MiB may be hashed by this implementation. (SHA2 standard supports 2 million Terabytes for 224/256)
- Input data may be 8-bit aligned. However, output digest must be 32-bit aligned.
- Intermediate values, input data, and final digest value may be left behind on the stack.
Usage
There are two general ways to execute a SHA2 operation:
The multi-step approach allows the hash to be extended by adding more data.
All input data is to be in little-endian (LE) format and the resulting hash values produced by these APIs are in LE format.
Synopsis
The following is a quick overview of one-step hashing.
uint32_t actualDigest[8];
message, strlen(message), actualDigest);
Examples
Hashing data in one call
int_fast16_t sha2SWresult;
uint32_t finalDigest[8];
int notsame;
char message[] =
"abcdefghijklmnabcdefghijklmnabcdefghijklmnabcdefghijklmn1234";
uint8_t expectedDigest[] =
{ 0x60, 0x06, 0x00, 0x24, 0x13, 0xe4, 0x27, 0x0d,
0x4d, 0xdb, 0x66, 0x93, 0x42, 0xa9, 0xe2, 0xdb,
0x66, 0x5e, 0xc8, 0x70, 0x73, 0xc4, 0x2e, 0xb5,
0x44, 0x99, 0x62, 0xf1, 0x2a, 0xb2, 0xe8, 0x60 };
message, strlen(message), finalDigest);
{
while(1);
}
notsame = memcmp(finalDigest, expectedDigest, sizeof(finalDigest));
if (notsame)
{
while(1);
}
Hashing data in multiple calls
int_fast16_t sha2SWresult;
uint32_t finalDigest[8];
int notsame;
char message[] =
"abcdefghijklmnabcdefghijklmnabcdefghijklmnabcdefghijklmn1234";
uint8_t expectedDigest[] =
{ 0x60, 0x06, 0x00, 0x24, 0x13, 0xe4, 0x27, 0x0d,
0x4d, 0xdb, 0x66, 0x93, 0x42, 0xa9, 0xe2, 0xdb,
0x66, 0x5e, 0xc8, 0x70, 0x73, 0xc4, 0x2e, 0xb5,
0x44, 0x99, 0x62, 0xf1, 0x2a, 0xb2, 0xe8, 0x60, };
}
sha2SWresult =
SHA256SWAddData(sha256SWHandle, &message[20], strlen(message) - 20);
}
}
{
while(1);
}
notsame = memcmp(finalDigest, expectedDigest, sizeof(finalDigest));
if (notsame)
{
while(1);
}
Configuration
See file sha2sw_config.h for full configuration information.
If SHA2SW_VALIDATE_INPUTS is not defined then:
- the caller is responsible for ensuring all inputs are valid, and
- the module's functions will only return SHA2SW_STATUS_SUCCESS
§ SHA256SWHashData
| #define SHA256SWHashData HAPI_TABLE_POINTER->sha256SwHashData |
§ SHA256SWStart
| #define SHA256SWStart HAPI_TABLE_POINTER->sha256SwStart |
§ SHA256SWAddData
| #define SHA256SWAddData HAPI_TABLE_POINTER->sha256SwAddData |
§ SHA256SWFinalize
| #define SHA256SWFinalize HAPI_TABLE_POINTER->sha256SwFinalize |
§ SHA256SW_Handle
§ SHA256SWHashData()
Performs a complete hash operation, producing a final digest for the data.
This function wraps SHA256SWStart(), SHA256SWAddData(), and SHA256SWFinalize().
There is no need to call SHA256SWStart() prior to calling this function.
The total length of data that can be hashed by this implementation is 512MiB (0x20000000 bytes.)
- Parameters
-
| [in] | handle | A SHA256SW_Handle. |
| [in] | hashType | The type of hash (256 or 224) to perform. |
| [in] | data | data (message) to hash. May point to zero. |
| [in] | length | the number of bytes (pointed to by data parameter) to add to the hash. |
| [out] | digest | Output location for the final digest. Must be able to hold 32 bytes of output and be 32-bit aligned. |
- Return values
-
§ SHA256SWStart()
§ SHA256SWAddData()
| int_fast16_t SHA256SWAddData |
( |
SHA256SW_Handle |
handle, |
|
|
const void * |
data, |
|
|
size_t |
length |
|
) |
| |
Add data to a SHA256/224 operation.
Adds data to a hash operation. The handle must have been initialized by a call to SHA256SWStart first.
The total length of data that can be hashed by this implementation is 512MiB (0x20000000 bytes.)
After passing in all data to be hashed, call SHA256SWFinalize() to obtain the final digest.
- Precondition
- handle was previously passed to SHA256SWStart().
- Parameters
-
| [in] | handle | A SHA256SW_Handle. |
| [in] | data | data (message) to add to the hash. May point to zero. |
| [in] | length | the number of bytes (pointed to by data parameter) to add to the hash. |
- Return values
-
- See also
- SHA256SWStart()
-
SHA256SWFinalize()
§ SHA256SWFinalize()
| int_fast16_t SHA256SWFinalize |
( |
SHA256SW_Handle |
handle, |
|
|
uint32_t |
digest[8] |
|
) |
| |
Finalize a SHA256/224 operation, creating the final digest.
After calling this function, handle should not be used again until it has been reinitialized via a call to SHA256SWStart().
- Precondition
- handle was previously passed to SHA256SWStart() and data to be hashed was passed to SHA256SWAddData()
- Parameters
-
| [in] | handle | A SHA256SW_Handle. |
| [out] | digest | Output location for the final digest. Must be able to hold 32 bytes of output and be 32-bit aligned. |
- Return values
-
- See also
- SHA256SWStart()
-
SHA256SWAddData()