CC27xxDriverLibrary
chipinfo.h
Go to the documentation of this file.
1 /******************************************************************************
2  * Filename: chipinfo.h
3  *
4  * Description: Collection of functions returning chip information.
5  *
6  * Copyright (c) 2022-2025 Texas Instruments Incorporated
7  *
8  * Redistribution and use in source and binary forms, with or without
9  * modification, are permitted provided that the following conditions are met:
10  *
11  * 1) Redistributions of source code must retain the above copyright notice,
12  * this list of conditions and the following disclaimer.
13  *
14  * 2) Redistributions in binary form must reproduce the above copyright notice,
15  * this list of conditions and the following disclaimer in the documentation
16  * and/or other materials provided with the distribution.
17  *
18  * 3) Neither the name of the copyright holder nor the names of its
19  * contributors may be used to endorse or promote products derived from this
20  * software without specific prior written permission.
21  *
22  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
23  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
24  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
25  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
26  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
27  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
28  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
29  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
30  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
31  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
32  * POSSIBILITY OF SUCH DAMAGE.
33  *
34  ******************************************************************************/
35 
36 #ifndef __CHIP_INFO_H__
37 #define __CHIP_INFO_H__
38 
39 //*****************************************************************************
40 //
45 //
46 //*****************************************************************************
47 
48 //*****************************************************************************
49 //
50 // If building with a C++ compiler, make all of the definitions in this header
51 // have a C binding.
52 //
53 //*****************************************************************************
54 #ifdef __cplusplus
55 extern "C" {
56 #endif
57 
58 #include "../inc/hw_types.h"
59 #include "../inc/hw_memmap.h"
60 #include "../inc/hw_sys0.h"
61 #include "../inc/hw_fcfg.h"
62 
63 //*****************************************************************************
64 //
66 //
67 //*****************************************************************************
68 typedef enum
69 {
70  CHIP_TYPE_CC2744 = 0x3548U,
71  CHIP_TYPE_CC2745 = 0xAF23U,
72  CHIP_TYPE_CC2755 = 0x6301U,
73 } ChipType;
74 
75 //*****************************************************************************
76 //
78 //
79 //*****************************************************************************
80 typedef enum
81 {
82  CC2744R74E0WRHARQ1 = 0x483548U,
83  CC2745R10E0WRHARQ1 = 0xE8AF23U,
84  CC2745R10E1WRHARQ1 = 0xE8AF23U,
85  CC2745P10E0WRHARQ1 = 0xDEAF23U,
86  CC2745R74E0WRHARQ1 = 0x87AF23U,
87  CC2755R105E0WRHAR = 0x9D6301U,
88  CC2755P105E0WRHAR = 0xE66301U,
89  CC2755R105E0YCJR = 0x316301U,
90 } ChipPartId;
91 
92 //*****************************************************************************
93 //
100 //
101 //*****************************************************************************
103 {
104  return (HWREG(SYS0_BASE + SYS0_O_DEVICEID) & SYS0_DEVICEID_VERSION_M) >> SYS0_DEVICEID_VERSION_S;
105 }
106 
107 #ifndef DRIVERLIB_NS
108 //*****************************************************************************
109 //
110 // Below functions will only be compiled into the driverlib.a library and not
111 // the driverlib_ns.a library.
112 // Non-secure applications might be able to access some/all of these functions
113 // through veneers declared further below in the #else case.
114 //
115 //*****************************************************************************
116 
117 //*****************************************************************************
118 //
123 //
124 //*****************************************************************************
126 {
127  return (ChipType)(fcfg->deviceInfo.partId.part);
128 }
129 
130 //*****************************************************************************
131 //
136 //
137 //*****************************************************************************
139 {
140  return (ChipPartId)(fcfg->deviceInfo.partId.val32 & 0x00FFFFFFU);
141 }
142 
143 #else
144 //*****************************************************************************
145 //
146 // Secure-only API functions available from non-secure context through
147 // veneers.
148 //
149 // These functions must be linked in from from the secure veneer library.
150 //
151 //*****************************************************************************
152 
153 extern ChipType ChipInfoGetChipType_veneer(void);
154  #define ChipInfoGetChipType ChipInfoGetChipType_veneer
155 
156 extern ChipPartId ChipInfoGetPartId_veneer(void);
157  #define ChipInfoGetPartId ChipInfoGetPartId_veneer
158 
159 #endif
160 
161 //*****************************************************************************
162 //
163 // Mark the end of the C bindings section for C++ compilers.
164 //
165 //*****************************************************************************
166 #ifdef __cplusplus
167 }
168 #endif
169 
170 //*****************************************************************************
171 //
175 //
176 //*****************************************************************************
177 
178 #endif // __CHIP_INFO_H__
ChipPartId
Chip part ID enumeration.
Definition: chipinfo.h:80
Part ID is CC2744R74E0WRHARQ1.
Definition: chipinfo.h:82
Part ID is CC2755P105E0WRHAR.
Definition: chipinfo.h:88
Part ID is CC2745R74E0WRHARQ1.
Definition: chipinfo.h:86
Chip type is CC2744.
Definition: chipinfo.h:70
Part ID is CC2745R10E1WRHARQ1.
Definition: chipinfo.h:84
Part ID is CC2755R105E0WRHAR.
Definition: chipinfo.h:87
Part ID is CC2745P10E0WRHARQ1.
Definition: chipinfo.h:85
ChipType
Chip type enumeration.
Definition: chipinfo.h:68
Chip type is CC2745.
Definition: chipinfo.h:71
__STATIC_INLINE ChipType ChipInfoGetChipType(void)
Returns chip type.
Definition: chipinfo.h:125
Part ID is CC2755R105E0YCJR.
Definition: chipinfo.h:89
__tz_c_veneer ChipPartId ChipInfoGetPartId_veneer(void)
Definition: chipinfo_veneers.c:45
__STATIC_INLINE ChipPartId ChipInfoGetPartId(void)
Returns part ID.
Definition: chipinfo.h:138
__STATIC_INLINE uint32_t ChipInfoGetVersion(void)
Returns hardware version number.
Definition: chipinfo.h:102
__tz_c_veneer ChipType ChipInfoGetChipType_veneer(void)
Definition: chipinfo_veneers.c:40
#define __STATIC_INLINE
Definition: cmsis_gcc.h:47
Part ID is CC2745R10E0WRHARQ1.
Definition: chipinfo.h:83
Chip type is CC2755.
Definition: chipinfo.h:72