Instance: SYS0
Component: SYS0
Base address: 0x40004000
This is top module of SYS0
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RO |
32 |
0x6B4E 0010 |
0x0000 0000 |
0x4000 4000 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 000C |
0x4000 400C |
|
|
RW |
32 |
0x0000 000F |
0x0000 0100 |
0x4000 4100 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0108 |
0x4000 4108 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 010C |
0x4000 410C |
|
|
RO |
32 |
0x0BB8 402F |
0x0000 03FC |
0x4000 43FC |
|
|
RW |
32 |
0x0000 0000 |
0x0000 07F8 |
0x4000 47F8 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0800 |
0x4000 4800 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0804 |
0x4000 4804 |
|
|
RW |
32 |
0x0080 0000 |
0x0000 0808 |
0x4000 4808 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 080C |
0x4000 480C |
|
|
RW |
32 |
0xB02E 603F |
0x0000 0810 |
0x4000 4810 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0814 |
0x4000 4814 |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0x4000 4000 | Instance | 0x4000 4000 |
| Description | Description Register This register provides IP module ID, revision information, instance index and standard MMR registers offset. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | MODID | Module Identifier is used to uniquely identify this IP | RO | 0x6B4E | ||
| 15:12 | STDIPOFF | Standard IP MMR block offset. Standard IP MMRs are the set from aggregated IRQ registers till DTB. 0: Standard IP MMRs do not exist 0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address) |
RO | 0x0 | ||
| 11:8 | INSTIDX | IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number (0-15). | RO | 0x0 | ||
| 7:4 | MAJREV | Major revision of IP (0-15). | RO | 0x1 | ||
| 3:0 | MINREV | Minor revision of IP (0-15). | RO | 0x0 | ||
| Address Offset | 0x0000 000C | ||
| Physical Address | 0x4000 400C | Instance | 0x4000 400C |
| Description | Mutable section Unlock This register unlocks registers in mutable section |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:0 | KEY | Write the unlock key 0xC5AF_6927 to temporarily unlock registers in mutable section. The lock is set automatically if no write accesses, to the mutable section, are detected for consecutive 32 CLKULL (24MHz) clock cycles. Writing any value other that the unlock key will immediately lock the mutable register space for write access.
|
WO | 0x0000 0000 | |||||||||||
| Address Offset | 0x0000 0100 | ||
| Physical Address | 0x4000 4100 | Instance | 0x4000 4100 |
| Description | ATEST Configuration This register is used to configure analog switches in ATEST module. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:24 | KEY | Key must be written with value 0x5A for successful write to ATESTCFG and to unlock register state. Write with any value other than 0x5A to KEY will be ignored and register content is not updated. It is recommended to write this register with incorrect KEY to lock back register state after necessary ATESTCFG updates are done. Read value of KEY is 0x0. |
WO | 0x00 | |||||||||||
| 23:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | |||||||||||
| 8 | VSEL | Selects supply for ATEST switches.
|
RW | 0 | |||||||||||
| 7 | VA2VA1 | Enables isolation switch between VA_ATEST_A1 and VA_PAD_A1.
|
RW | 0 | |||||||||||
| 6 | VA2VA0 | Enables isolation switch between VA_ATEST_A0 and VA_PAD_A0.
|
RW | 0 | |||||||||||
| 5 | VR2VA1 | Enables isolation switch between VR_ATEST_A1 and VA_ATEST_A1.
|
RW | 0 | |||||||||||
| 4 | VR2VA0 | Enables isolation switch between VR_ATEST_A0 and VA_ATEST_A0.
|
RW | 0 | |||||||||||
| 3 | SHTVA1 | Shorts VA_ATEST_A1 to ground.
|
RW | 1 | |||||||||||
| 2 | SHTVA0 | Shorts VA_ATEST_A0 to ground.
|
RW | 1 | |||||||||||
| 1 | SHTVR1 | Shorts VR_ATEST_A1 to ground.
|
RW | 1 | |||||||||||
| 0 | SHTVR0 | Shorts VR_ATEST_A0 to ground.
|
RW | 1 | |||||||||||
| Address Offset | 0x0000 0108 | ||
| Physical Address | 0x4000 4108 | Instance | 0x4000 4108 |
| Description | TSENSE Configuration This register is used to configure temperature sensor module. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||
| 31:12 | RESERVED12 | Software should not rely on the value of a reserved field. Writing any other value than the reset value may result in undefined behavior | RO | 0x0 0000 | ||||||||||||||
| 11:8 | SPARE | Spare bits | RW | 0x0 | ||||||||||||||
| 7:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | ||||||||||||||
| 1:0 | SEL | Used to enable and configure temperature sensor module. Setting the value to 0x3 will disable the temperature sensor.
|
RW | 0b00 | ||||||||||||||
| Address Offset | 0x0000 010C | ||
| Physical Address | 0x4000 410C | Instance | 0x4000 410C |
| Description | LPCMP configuration This register is used to configure and check the status of low-power comparator (LPCOMP) module. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||
| 31 | RESERVED31 | Software should not rely on the value of a reserved field. Writing any other value than the reset value may result in undefined behavior | RO | 0 | ||||||||||||||||||||||||||||||||
| 30 | HYSPOL | Spare bit for LPCOMP | RW | 0 | ||||||||||||||||||||||||||||||||
| 29:28 | ATESTMUX | Used to configure ATEST mux in comparator module and provides chosen output on VA_ATEST_A0. Note: This bit field is write-protected using global lock indicator on production device.
|
RW | 0b00 | ||||||||||||||||||||||||||||||||
| 27:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | ||||||||||||||||||||||||||||||||
| 24 | EVTIFG | Event flag The event flag is set when the comparator output transition is qualified based on the edge polarity configuration in EDGCFG.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 23:22 | RESERVED22 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||||||||||||||
| 21 | COUTEN | Enables LPCOMP output on device pin.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 20 | COUT | LPCOMP output status. This bit captures the value LPCOMP raw output.
|
RO | 0 | ||||||||||||||||||||||||||||||||
| 19 | RESERVED19 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||||||||||||||
| 18 | WUENSB | Enables lpcmpcfg output to wake device from standby.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 17 | EVTEN | Enables event generation. Comparator module will produce event on ULL event fabric when EVTIFG is set.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 16 | EDGCFG | Selects positive edge or negative edge detection on comparator output to set the event flag
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 15 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||||||||||||||
| 14:12 | NSEL | Negative input selection. Setting values 0x5-0x7 will open all the switches.
|
RW | 0b000 | ||||||||||||||||||||||||||||||||
| 11:8 | PSEL | Positive input selection. Setting values 0x9-0xF will open all the switches.
|
RW | 0x0 | ||||||||||||||||||||||||||||||||
| 7:5 | HYSSEL | Used to enable and select hysteresis level Hysteresis is disabled when HYSSEL = 0 and enabled for other values of HYSSEL from 1 to 7. Refer to device specific datasheet for individual hysteresis values.
|
RW | 0b000 | ||||||||||||||||||||||||||||||||
| 4 | DIVPATH | Used to select the path on which voltage divider is applied
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 3:1 | DIV | Used to configure reference divider. Setting values 0x5-0x7 will set the divide value to 1.
|
RW | 0b000 | ||||||||||||||||||||||||||||||||
| 0 | EN | Used to enable comparator module.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 03FC | ||
| Physical Address | 0x4000 43FC | Instance | 0x4000 43FC |
| Description | Device ID This register provides Device ID information. Note: This 32-bit register value is provided as output to DEBUGSS. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | VERSION | Monotonic increasing value indicating new hardware revision. A newer hardware revision shall never have a lower version than an older revision of hardware. | RO | 0x0 | ||
| 27:12 | DEVICE | Value generated by RAMP for the SOC. This value uniquely identifies the die from any other TI device. | RO | 0xBB84 | ||
| 11:1 | MANFACTURER | JEP 106 assigned manufacturer ID. This field identifies the device as a Texas Instruments device. | RO | 0b000 0001 0111 | ||
| 0 | ALWAYSONE | Value 1 in this bit field means that a 32-bit scan register exists. | RO | 1 | ||
| Address Offset | 0x0000 07F8 | ||
| Physical Address | 0x4000 47F8 | Instance | 0x4000 47F8 |
| Description | Part ID This register is programmed by boot code with Part ID information. Note: This 32-bit register value is provided as output to DEBUGSS |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31 | START | Start bit
|
RW | 0 | |||||||||||
| 30:28 | MAJORREV | Monotonic increasing value indicating a new revision of the SKU significant enough that users of the device may have to revise PCB or software design | RW | 0b000 | |||||||||||
| 27:24 | MINORREV | Monotonic increasing value indicating a new revision of the SKU that preserves compatibility with lesser MINORREV values | RW | 0x0 | |||||||||||
| 23:16 | VARIANT | Bit pattern uniquely identifying a variant of a part | RW | 0x00 | |||||||||||
| 15:0 | PART | Bit pattern uniquely identifying a part | RW | 0x0000 | |||||||||||
| Address Offset | 0x0000 0800 | ||
| Physical Address | 0x4000 4800 | Instance | 0x4000 4800 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CDACL | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0804 | ||
| Physical Address | 0x4000 4804 | Instance | 0x4000 4804 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CDACM | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0808 | ||
| Physical Address | 0x4000 4808 | Instance | 0x4000 4808 |
| Description | TMUTE2 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31 | RESERVED31 | RESERVED | RO | 0 | ||
| 30:26 | IBTRIM | LPCOMP: Bias current trim, 250nA to be terminated across I2V, 1M ohm setting. Resulting target trim voltage 250mV. | RW | 0b0 0000 | ||
| 25:23 | TRIM | ADC REFBUF trim bits. | RW | 0b001 | ||
| 22:16 | LATCH | SOC ADC: Latch trim bits. These bits are used in the analog IP. | RW | 0b000 0000 | ||
| 15:4 | OFFSET | SOCADC: Offset trim bits. These bits are used in DTC. | RW | 0x000 | ||
| 3:2 | RES | SOCADC: Resistor trim bits. These bits are used in the analog IP. | RW | 0b00 | ||
| 1:0 | CDACU | SOCADC: Upper 2 bits of CDAC trim. These bits are used in DTC. | RW | 0b00 | ||
| Address Offset | 0x0000 080C | ||
| Physical Address | 0x4000 480C | Instance | 0x4000 480C |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:26 | BATC1 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
| 25:19 | BATC0 | Internal. Only to be used through TI provided API. | RW | 0b000 0000 | ||
| 18:14 | TEMPC2 | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
| 13:8 | TEMPC1 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
| 7:0 | TEMPC0 | Internal. Only to be used through TI provided API. | RW | 0x00 | ||
| Address Offset | 0x0000 0810 | ||
| Physical Address | 0x4000 4810 | Instance | 0x4000 4810 |
| Description | TMUTE4 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | RECHCOMPREFLVL | Internal. Only to be used through TI provided API. | RW | 0xB | ||
| 27:26 | IOSTRCFG2 | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
| 25:22 | IOSTRCFG1 | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
| 21:19 | MAX | Internal. Only to be used through TI provided API. | RW | 0b101 | ||
| 18:16 | MED | Internal. Only to be used through TI provided API. | RW | 0b110 | ||
| 15:13 | MIN | Internal. Only to be used through TI provided API. | RW | 0b011 | ||
| 12:11 | DCDCLOAD | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
| 10:8 | IPEAK | DCDC: Set inductor peak current Min = 0x0 Max = 0x7 DCDC load support increases from 0x0 to 0x7 |
RW | 0b000 | ||
| 7:6 | DTIME | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
| 5:3 | LENSEL | Internal. Only to be used through TI provided API. | RW | 0b111 | ||
| 2:0 | HENSEL | Internal. Only to be used through TI provided API. | RW | 0b111 | ||
| Address Offset | 0x0000 0814 | ||
| Physical Address | 0x4000 4814 | Instance | 0x4000 4814 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:13 | RESERVED13 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 | ||
| 12:10 | DCDCDRVDS | Internal. Only to be used through TI provided API. | RW | 0b000 | ||
| 9:5 | GLDOISCLR | Internal. Only to be used through TI provided API. | WO | 0b0 0000 | ||
| 4:0 | GLDOISSET | Internal. Only to be used through TI provided API. | WO | 0b0 0000 | ||
| 4:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 | ||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |