![]() |
![]() |
|
CC23x0R5DriverLibrary
|
============================================================================

Go to the source code of this file.
Macros | |
| #define | SHA2SW_VALIDATE_INPUTS (1) |
| Include support for SHA2 224. More... | |
| #define | SHA2SW_FAST_MESSAGE_SCHEDULE (1) |
| Use a faster implementation of the message schedule which is slightly larger in code size. More... | |
| #define | SHA2SW_FAST_WORKING_VARS (1) |
| Use a faster implementation of the working variables a-h which is slightly larger in code size. More... | |
| #define | SHA2SW_USE_ARMCLE (1) |
| Use portions of the constants of the 512 algorithm to support the 256 and 224 algorithms. More... | |