![]() |
![]() |
|
CC23x0R5DriverLibrary
|
#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_flash.h"#include "../inc/hw_memmap.h"#include "../inc/hw_ints.h"#include "../inc/hw_vims.h"#include "hapi.h"#include "chipinfo.h"#include "interrupt.h"#include "debug.h"
Go to the source code of this file.
Macros | |
| #define | FAPI_STATUS_SUCCESS 0x00000000 |
| Function completed successfully. More... | |
| #define | FAPI_STATUS_FSM_BUSY 0x00000001 |
| FSM is Busy. More... | |
| #define | FAPI_STATUS_FSM_READY 0x00000002 |
| FSM is Ready. More... | |
| #define | FAPI_STATUS_INCORRECT_DATABUFFER_LENGTH 0x00000003 |
| Incorrect parameter value. More... | |
| #define | FAPI_STATUS_FSM_ERROR 0x00000004 |
| Flash program/erase operation failed. More... | |
| #define | FAPI_STATUS_ADDRESS_ERROR 0x00000005 |
| Address range or alignment error. More... | |
| #define | FAPI_STATUS_INVALID_KEY 0x00000010 |
| Invalid random jump protection key. More... | |
Functions | |
| __STATIC_INLINE uint32_t | FlashGetSectorSize (void) |
| Get size of a flash sector in number of bytes. More... | |
| __STATIC_INLINE uint32_t | FlashGetSize (void) |
| Get the size of the flash. More... | |
| __STATIC_INLINE uint32_t | FlashCheckFsmForError (void) |
| Checks if the Flash state machine has detected an error. More... | |
| __STATIC_INLINE uint32_t | FlashCheckFsmForReady (void) |
| Checks if the Flash state machine is ready. More... | |
| __STATIC_INLINE uint32_t | FlashEraseSector (uint32_t sectorAddress) |
| Erase a flash sector. More... | |
| __STATIC_INLINE uint32_t | FlashEraseBank (void) |
| __STATIC_INLINE uint32_t | FlashProgram (uint8_t *dataBuffer, uint32_t address, uint32_t count) |
| Programs unprotected flash sectors in the main bank. More... | |