CC23x0r2DriverLibrary
SHA256SW_Object Struct Reference

SHA256SW Object. More...

#include <sha256sw.h>

Data Fields

uint32_t bitsProcessed
 
int8_t offsetWb
 
uint8_t reserved1
 
uint8_t reserved2
 
uint8_t reserved3
 
uint32_t digest32 [8]
 
uint32_t Ws32 [16]
 

Detailed Description

SHA256SW Object.

The application must not access any member variables of this structure!

Field Documentation

§ bitsProcessed

uint32_t SHA256SW_Object::bitsProcessed

§ offsetWb

int8_t SHA256SW_Object::offsetWb

§ reserved1

uint8_t SHA256SW_Object::reserved1

§ reserved2

uint8_t SHA256SW_Object::reserved2

§ reserved3

uint8_t SHA256SW_Object::reserved3

§ digest32

uint32_t SHA256SW_Object::digest32[8]

§ Ws32

uint32_t SHA256SW_Object::Ws32[16]

The documentation for this struct was generated from the following file: