CC23x0r2DriverLibrary
lpcmp.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_sys0.h"
Include dependency graph for lpcmp.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Macros

#define LPCMP_DIVISION_PATH_N   SYS0_LPCMPCFG_DIVPATH_NSIDE
 Apply voltage divider to the negative input. More...
 
#define LPCMP_DIVISION_PATH_P   SYS0_LPCMPCFG_DIVPATH_PSIDE
 Apply voltage divider to the positive input. More...
 
#define LPCMP_DIVISION_FACTOR_1_1   SYS0_LPCMPCFG_DIV_VAL0
 Apply a 1/1 voltage division ratio. More...
 
#define LPCMP_DIVISION_FACTOR_3_4   SYS0_LPCMPCFG_DIV_VAL1
 Apply a 3/4 voltage division ratio. More...
 
#define LPCMP_DIVISION_FACTOR_1_2   SYS0_LPCMPCFG_DIV_VAL2
 Apply a 1/2 voltage division ratio. More...
 
#define LPCMP_DIVISION_FACTOR_1_3   SYS0_LPCMPCFG_DIV_VAL3
 Apply a 1/3 voltage division ratio. More...
 
#define LPCMP_DIVISION_FACTOR_1_4   SYS0_LPCMPCFG_DIV_VAL4
 Apply a 1/4 voltage division ratio. More...
 
#define LPCMP_POLARITY_FALL   SYS0_LPCMPCFG_EDGCFG_FALL
 Select falling edge for event generation. More...
 
#define LPCMP_POLARITY_RISE   SYS0_LPCMPCFG_EDGCFG_RISE
 Select rising edge for event generation. More...
 
#define LPCMP_NEG_INPUT_VDDD   SYS0_LPCMPCFG_NSEL_VDDD
 Select VDDD as negative input. More...
 
#define LPCMP_NEG_INPUT_VDDS   SYS0_LPCMPCFG_NSEL_VDDA
 Select VDDS(VDDA) as negative input. More...
 
#define LPCMP_NEG_INPUT_A2   SYS0_LPCMPCFG_NSEL_VA_PAD_A2
 Select PAD_A2 as negative input. More...
 
#define LPCMP_NEG_INPUT_A3   SYS0_LPCMPCFG_NSEL_VA_PAD_A3
 Select PAD_A3 as negative input. More...
 
#define LPCMP_NEG_INPUT_OPEN   SYS0_LPCMPCFG_NSEL_OPEN
 Leave negative input floating. More...
 
#define LPCMP_POS_INPUT_A1   SYS0_LPCMPCFG_PSEL_VA_PAD_A1
 Select PAD_A1 as positive input. More...
 
#define LPCMP_POS_INPUT_A2   SYS0_LPCMPCFG_PSEL_VA_PAD_A2
 Select PAD_A2 as positive input. More...
 
#define LPCMP_POS_INPUT_A3   SYS0_LPCMPCFG_PSEL_VA_PAD_A3
 Select PAD_A3 as positive input. More...
 
#define LPCMP_POS_INPUT_VDDS   SYS0_LPCMPCFG_PSEL_VDDA
 Selects VDDS(VDDA) as positive input. More...
 
#define LPCMP_POS_INPUT_OPEN   SYS0_LPCMPCFG_PSEL_OPEN
 Leave negative positive floating. More...
 

Functions

__STATIC_INLINE void LPCMPEnable (void)
 Enables LPCMP. More...
 
__STATIC_INLINE void LPCMPDisable (void)
 Disables LPCMP. More...
 
__STATIC_INLINE void LPCMPEnableEvent (void)
 Enables LPCMP event generation. More...
 
__STATIC_INLINE void LPCMPDisableEvent (void)
 Disables LPCMP event generation. More...
 
__STATIC_INLINE void LPCMPClearEvent (void)
 Clear LPCMP event flag. More...
 
__STATIC_INLINE void LPCMPEnableWakeup (void)
 Enables LPCMP as wakeup source from standby. More...
 
__STATIC_INLINE void LPCMPDisableWakeup (void)
 Disables LPCMP as wakeup source from standby. More...
 
__STATIC_INLINE void LPCMPSelectNegativeInput (uint32_t input)
 Selects the negative input of LPCMP. More...
 
__STATIC_INLINE bool LPCMPIsOutputHigh (void)
 Verifies if the raw output of LPCMP is high. More...
 
__STATIC_INLINE void LPCMPSelectPositiveInput (uint32_t input)
 Selects the positive input of LPCMP. More...
 
__STATIC_INLINE void LPCMPSetPolarity (uint32_t polarity)
 Selects the edge polarity of LPCMP output on which an event is triggered. More...
 
__STATIC_INLINE void LPCMPSetDividerRatio (uint32_t divider)
 Selects the ratio used by LPCMP voltage divider. More...
 
__STATIC_INLINE void LPCMPSetDividerPath (uint32_t path)
 Selects the input path on which the LPCMP voltage divider is applied. More...