![]() |
![]() |
|
CC23x0r2DriverLibrary
|


Go to the source code of this file.
Data Structures | |
| struct | HARD_API_T |
Macros | |
| #define | FLASH_API_KEY 0xB7E3A08F |
| #define | HAPI_TABLE_BASE_ADDR 0x0F00004C |
| #define | HAPI_TABLE_POINTER ((const HARD_API_T *)HAPI_TABLE_BASE_ADDR) |
| #define | HapiEnterStandby(p) HAPI_TABLE_POINTER->enterStandby((p)) |
| #define | HapiCrc32(p, n) HAPI_TABLE_POINTER->crc32((p), (n)) |
| #define | HapiApplyCopyList(p) HAPI_TABLE_POINTER->applyCopyList((p)) |
| #define | HapiFlashSectorErase(k, p) HAPI_TABLE_POINTER->flashSectorErase((k), (p)) |
| #define | HapiFlashBankErase(k) HAPI_TABLE_POINTER->flashBankErase((k)) |
| #define | HapiFlashProgram(k, s, d, n) HAPI_TABLE_POINTER->flashProgram((k), (s), (d), (n)) |
| #define | HapiCountBits(w) HAPI_TABLE_POINTER->countBits((w)) |
| #define | HapiSecdedEncode(p, d, n) HAPI_TABLE_POINTER->secdedEncode((p), (d), (n)) |
| #define | HapiSecdedDecode(d, p, n) HAPI_TABLE_POINTER->secdedDecode((d), (p), (n)) |
| #define | HapiEnterApplication() HAPI_TABLE_POINTER->enterApplication() |
| #define | HapiSha256SwHashData(h, d, l, g) HAPI_TABLE_POINTER->sha256SwHashData((h), SHA2SW_HASH_TYPE_256, (d), (l), (g)) |
| #define | HapiSha256SwStart(h) HAPI_TABLE_POINTER->sha256SwStart((h), SHA2SW_HASH_TYPE_256) |
| #define | HapiSha256SwAddData(h, d, l) HAPI_TABLE_POINTER->sha256SwAddData((h), (d), (l)) |
| #define | HapiSha256SwFinalize(h, g) HAPI_TABLE_POINTER->sha256SwFinalize((h), (g)) |
| #define | HapiResetDevice() HAPI_TABLE_POINTER->resetDevice() |
| #define | HapiSha256SWProcessBlock(d, w) HAPI_TABLE_POINTER->pSHA256SWProcessBlock((d), (w)) |
| #define | HapiSha256SW_K256 (*HAPI_TABLE_POINTER->sha256SW_K256) |
| #define | HapiSha256SW_initialDigest256 (*HAPI_TABLE_POINTER->sha256SW_initialDigest256) |
| #define | HapiWaitUs(n) HAPI_TABLE_POINTER->waitUs((n)) |
| #define | HapiClz(x) HAPI_TABLE_POINTER->clz((x)) |
| #define FLASH_API_KEY 0xB7E3A08F |
Magic value used to protect against inadvertent flash erasures/programming. (prevents corruption due to random jumps into the flash API, for example due to stack overflow or errant function pointers) Must be passed in key argument to all flash functions
Referenced by FlashEraseBank(), FlashEraseSector(), and FlashProgram().
| #define HAPI_TABLE_BASE_ADDR 0x0F00004C |
| #define HAPI_TABLE_POINTER ((const HARD_API_T *)HAPI_TABLE_BASE_ADDR) |
| #define HapiEnterStandby | ( | p | ) | HAPI_TABLE_POINTER->enterStandby((p)) |
| #define HapiCrc32 | ( | p, | |
| n | |||
| ) | HAPI_TABLE_POINTER->crc32((p), (n)) |
| #define HapiApplyCopyList | ( | p | ) | HAPI_TABLE_POINTER->applyCopyList((p)) |
Referenced by CopyList_apply().
| #define HapiFlashSectorErase | ( | k, | |
| p | |||
| ) | HAPI_TABLE_POINTER->flashSectorErase((k), (p)) |
Referenced by FlashEraseSector().
| #define HapiFlashBankErase | ( | k | ) | HAPI_TABLE_POINTER->flashBankErase((k)) |
Referenced by FlashEraseBank().
| #define HapiFlashProgram | ( | k, | |
| s, | |||
| d, | |||
| n | |||
| ) | HAPI_TABLE_POINTER->flashProgram((k), (s), (d), (n)) |
Referenced by FlashProgram().
| #define HapiCountBits | ( | w | ) | HAPI_TABLE_POINTER->countBits((w)) |
| #define HapiSecdedEncode | ( | p, | |
| d, | |||
| n | |||
| ) | HAPI_TABLE_POINTER->secdedEncode((p), (d), (n)) |
| #define HapiSecdedDecode | ( | d, | |
| p, | |||
| n | |||
| ) | HAPI_TABLE_POINTER->secdedDecode((d), (p), (n)) |
| #define HapiEnterApplication | ( | ) | HAPI_TABLE_POINTER->enterApplication() |
| #define HapiSha256SwHashData | ( | h, | |
| d, | |||
| l, | |||
| g | |||
| ) | HAPI_TABLE_POINTER->sha256SwHashData((h), SHA2SW_HASH_TYPE_256, (d), (l), (g)) |
| #define HapiSha256SwStart | ( | h | ) | HAPI_TABLE_POINTER->sha256SwStart((h), SHA2SW_HASH_TYPE_256) |
| #define HapiSha256SwAddData | ( | h, | |
| d, | |||
| l | |||
| ) | HAPI_TABLE_POINTER->sha256SwAddData((h), (d), (l)) |
| #define HapiSha256SwFinalize | ( | h, | |
| g | |||
| ) | HAPI_TABLE_POINTER->sha256SwFinalize((h), (g)) |
| #define HapiResetDevice | ( | ) | HAPI_TABLE_POINTER->resetDevice() |
| #define HapiSha256SWProcessBlock | ( | d, | |
| w | |||
| ) | HAPI_TABLE_POINTER->pSHA256SWProcessBlock((d), (w)) |
| #define HapiSha256SW_K256 (*HAPI_TABLE_POINTER->sha256SW_K256) |
| #define HapiSha256SW_initialDigest256 (*HAPI_TABLE_POINTER->sha256SW_initialDigest256) |
| #define HapiWaitUs | ( | n | ) | HAPI_TABLE_POINTER->waitUs((n)) |
| #define HapiClz | ( | x | ) | HAPI_TABLE_POINTER->clz((x)) |