CC23x0r2DriverLibrary
[pmctl.h] Power Management Controller
Collaboration diagram for [pmctl.h] Power Management Controller:

Functions

__STATIC_INLINE uint32_t PMCTLGetResetReason (void)
 Get the reason for the system reset. More...
 
__STATIC_INLINE void PMCTLResetSystem (void)
 Issue a system reset. More...
 
__STATIC_INLINE void PMCTLSetVoltageRegulator (uint32_t regulator)
 Set the VDDR regulator. More...
 
__STATIC_INLINE uint32_t PMCTLGetVoltageRegulator (void)
 Get the current VDDR regulator. More...
 

PMCTLGetResetReason() return values

#define PMCTL_RESET_SHUTDOWN_IO   (PMCTL_RSTSTA_SDDET | PMCTL_RSTSTA_IOWUSD)
 Device woke up from shutdown due to an IO event. More...
 
#define PMCTL_RESET_SHUTDOWN_SWD   PMCTL_RSTSTA_SDDET
 Device woke up from shutdown due to an SWD event. More...
 
#define PMCTL_RESET_WATCHDOG   (PMCTL_RSTSTA_SYSSRC_WDTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset because of a watchdog timeout. More...
 
#define PMCTL_RESET_SYSTEM   (PMCTL_RSTSTA_SYSSRC_SYSRSTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by software writing to RSTCTL.SYSRST. More...
 
#define PMCTL_RESET_CPU   (PMCTL_RSTSTA_SYSSRC_CPURSTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by CPU reset event. More...
 
#define PMCTL_RESET_LOCKUP   (PMCTL_RSTSTA_SYSSRC_LOCKUPEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by CPU lockup event. More...
 
#define PMCTL_RESET_ANALOG_FSM_TIMEOUT   (PMCTL_RSTSTA_SYSSRC_AFSMEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by Analog FSM timeout event. More...
 
#define PMCTL_RESET_ANALOG_ERROR   (PMCTL_RSTSTA_SYSSRC_AERREV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by Analog Error reset event. More...
 
#define PMCTL_RESET_DIGITAL_ERROR   (PMCTL_RSTSTA_SYSSRC_DERREV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by Digital Error reset event. More...
 
#define PMCTL_RESET_SWD   (PMCTL_RSTSTA_SYSSRC_SWDRSTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset triggered by Serial Wire Debug reset event. More...
 
#define PMCTL_RESET_LFXT   (PMCTL_RSTSTA_SYSSRC_LFLOSSEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)
 Device reset due to LFXT clock loss. More...
 
#define PMCTL_RESET_TSD   (PMCTL_RSTSTA_TSDEV | PMCTL_RSTSTA_RESETSRC_PINRESET)
 Device woke up from thermal shutdown after temperature drop. More...
 
#define PMCTL_RESET_VDDR   PMCTL_RSTSTA_RESETSRC_VDDRLOSS
 Device reset due to VDDR brownout event. More...
 
#define PMCTL_RESET_VDDS   PMCTL_RSTSTA_RESETSRC_VDDSLOSS
 Device reset due to VDDS brownout event. More...
 
#define PMCTL_RESET_PIN   PMCTL_RSTSTA_RESETSRC_PINRESET
 Device reset due to pin reset. More...
 
#define PMCTL_RESET_POR   PMCTL_RSTSTA_RESETSRC_PWRON
 Device booted due to power on reset. More...
 

PMCTLSetVoltageRegulator() inputs and PMCTLGetVoltageRegulator() return values

#define PMCTL_VOLTAGE_REGULATOR_DCDC   PMCTL_VDDRCTL_SELECT_DCDC
 DCDC voltage regulator. More...
 
#define PMCTL_VOLTAGE_REGULATOR_GLDO   PMCTL_VDDRCTL_SELECT_GLDO
 GLDO voltage regulator. More...
 

Detailed Description

Macro Definition Documentation

§ PMCTL_RESET_SHUTDOWN_IO

#define PMCTL_RESET_SHUTDOWN_IO   (PMCTL_RSTSTA_SDDET | PMCTL_RSTSTA_IOWUSD)

Device woke up from shutdown due to an IO event.

§ PMCTL_RESET_SHUTDOWN_SWD

#define PMCTL_RESET_SHUTDOWN_SWD   PMCTL_RSTSTA_SDDET

Device woke up from shutdown due to an SWD event.

§ PMCTL_RESET_WATCHDOG

#define PMCTL_RESET_WATCHDOG   (PMCTL_RSTSTA_SYSSRC_WDTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset because of a watchdog timeout.

§ PMCTL_RESET_SYSTEM

#define PMCTL_RESET_SYSTEM   (PMCTL_RSTSTA_SYSSRC_SYSRSTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by software writing to RSTCTL.SYSRST.

§ PMCTL_RESET_CPU

#define PMCTL_RESET_CPU   (PMCTL_RSTSTA_SYSSRC_CPURSTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by CPU reset event.

§ PMCTL_RESET_LOCKUP

#define PMCTL_RESET_LOCKUP   (PMCTL_RSTSTA_SYSSRC_LOCKUPEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by CPU lockup event.

§ PMCTL_RESET_ANALOG_FSM_TIMEOUT

#define PMCTL_RESET_ANALOG_FSM_TIMEOUT   (PMCTL_RSTSTA_SYSSRC_AFSMEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by Analog FSM timeout event.

§ PMCTL_RESET_ANALOG_ERROR

#define PMCTL_RESET_ANALOG_ERROR   (PMCTL_RSTSTA_SYSSRC_AERREV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by Analog Error reset event.

§ PMCTL_RESET_DIGITAL_ERROR

#define PMCTL_RESET_DIGITAL_ERROR   (PMCTL_RSTSTA_SYSSRC_DERREV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by Digital Error reset event.

§ PMCTL_RESET_SWD

#define PMCTL_RESET_SWD   (PMCTL_RSTSTA_SYSSRC_SWDRSTEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset triggered by Serial Wire Debug reset event.

§ PMCTL_RESET_LFXT

#define PMCTL_RESET_LFXT   (PMCTL_RSTSTA_SYSSRC_LFLOSSEV | PMCTL_RSTSTA_RESETSRC_SYSRESET)

Device reset due to LFXT clock loss.

§ PMCTL_RESET_TSD

#define PMCTL_RESET_TSD   (PMCTL_RSTSTA_TSDEV | PMCTL_RSTSTA_RESETSRC_PINRESET)

Device woke up from thermal shutdown after temperature drop.

§ PMCTL_RESET_VDDR

#define PMCTL_RESET_VDDR   PMCTL_RSTSTA_RESETSRC_VDDRLOSS

Device reset due to VDDR brownout event.

§ PMCTL_RESET_VDDS

#define PMCTL_RESET_VDDS   PMCTL_RSTSTA_RESETSRC_VDDSLOSS

Device reset due to VDDS brownout event.

§ PMCTL_RESET_PIN

#define PMCTL_RESET_PIN   PMCTL_RSTSTA_RESETSRC_PINRESET

Device reset due to pin reset.

§ PMCTL_RESET_POR

#define PMCTL_RESET_POR   PMCTL_RSTSTA_RESETSRC_PWRON

Device booted due to power on reset.

§ PMCTL_VOLTAGE_REGULATOR_DCDC

#define PMCTL_VOLTAGE_REGULATOR_DCDC   PMCTL_VDDRCTL_SELECT_DCDC

DCDC voltage regulator.

§ PMCTL_VOLTAGE_REGULATOR_GLDO

#define PMCTL_VOLTAGE_REGULATOR_GLDO   PMCTL_VDDRCTL_SELECT_GLDO

GLDO voltage regulator.

Function Documentation

§ PMCTLGetResetReason()

§ PMCTLResetSystem()

__STATIC_INLINE void PMCTLResetSystem ( void  )

Issue a system reset.

This function issues a system reset. This will cause the device to reboot. After rebooting, PMCTLGetResetReason() will return PMCTL_RESET_SYSTEM.

Returns
None

References __disable_irq().

§ PMCTLSetVoltageRegulator()

__STATIC_INLINE void PMCTLSetVoltageRegulator ( uint32_t  regulator)

Set the VDDR regulator.

This function sets the VDDR regulator to use in active, idle, and standby modes.

Parameters
regulatorThe voltage regulator to switch to.
Returns
None

§ PMCTLGetVoltageRegulator()

__STATIC_INLINE uint32_t PMCTLGetVoltageRegulator ( void  )

Get the current VDDR regulator.

This function gets the VDDR regulator currently in use.

Returns
Current voltage regulator
  • PMCTL_VOLTAGE_REGULATOR_DCDC
  • PMCTL_VOLTAGE_REGULATOR_GLDO