CC23x0r2DriverLibrary

Function that provides FPU type. More...

Collaboration diagram for FPU Functions:

Functions

__STATIC_INLINE uint32_t SCB_GetFPUType (void)
 get FPU type More...
 

Detailed Description

Function that provides FPU type.

Function Documentation

§ SCB_GetFPUType()

__STATIC_INLINE uint32_t SCB_GetFPUType ( void  )

get FPU type

returns the FPU type

Returns
  • 0: No FPU
  • 1: Single precision FPU
  • 2: Double + Single precision FPU

References __NVIC_PRIO_BITS, __STATIC_INLINE, NVIC_SetPriority, SysTick, SysTick_CTRL_CLKSOURCE_Msk, SysTick_CTRL_ENABLE_Msk, SysTick_CTRL_TICKINT_Msk, SysTick_IRQn, and SysTick_LOAD_RELOAD_Msk.